Data Fields
tUSBDCDCDevice Struct Reference

#include <usbdcdc.h>

Data Fields

const uint16_t ui16VID
 The vendor ID that this device is to present in the device descriptor. More...
 
const uint16_t ui16PID
 The product ID that this device is to present in the device descriptor. More...
 
const uint16_t ui16MaxPowermA
 The maximum power consumption of the device, expressed in milliamps. More...
 
const uint8_t ui8PwrAttributes
 
const tUSBCallback pfnControlCallback
 
void * pvControlCBData
 
const tUSBCallback pfnRxCallback
 
void * pvRxCBData
 
const tUSBCallback pfnTxCallback
 
void * pvTxCBData
 
const uint8_t *const * ppui8StringDescriptors
 
const uint32_t ui32NumStringDescriptors
 
tCDCSerInstance sPrivateData
 

Detailed Description

The structure used by the application to define operating parameters for the CDC device.

Field Documentation

§ ui16VID

const uint16_t tUSBDCDCDevice::ui16VID

The vendor ID that this device is to present in the device descriptor.

Referenced by USBDCDCInit().

§ ui16PID

const uint16_t tUSBDCDCDevice::ui16PID

The product ID that this device is to present in the device descriptor.

Referenced by USBDCDCInit().

§ ui16MaxPowermA

const uint16_t tUSBDCDCDevice::ui16MaxPowermA

The maximum power consumption of the device, expressed in milliamps.

Referenced by USBDCDCInit().

§ ui8PwrAttributes

const uint8_t tUSBDCDCDevice::ui8PwrAttributes

Indicates whether the device is self- or bus-powered and whether or not it supports remote wakeup. Valid values are USB_CONF_ATTR_SELF_PWR or USB_CONF_ATTR_BUS_PWR, optionally ORed with USB_CONF_ATTR_RWAKE.

Referenced by USBDCDCInit().

§ pfnControlCallback

const tUSBCallback tUSBDCDCDevice::pfnControlCallback

A pointer to the callback function which will be called to notify the application of all asynchronous control events related to the operation of the device.

Referenced by USBDCDCCompositeInit().

§ pvControlCBData

void* tUSBDCDCDevice::pvControlCBData

A client-supplied pointer which will be sent as the first parameter in all calls made to the control channel callback, pfnControlCallback.

Referenced by USBDCDCSetControlCBData().

§ pfnRxCallback

const tUSBCallback tUSBDCDCDevice::pfnRxCallback

A pointer to the callback function which will be called to notify the application of events related to the device's data receive channel.

Referenced by USBDCDCCompositeInit().

§ pvRxCBData

void* tUSBDCDCDevice::pvRxCBData

A client-supplied pointer which will be sent as the first parameter in all calls made to the receive channel callback, pfnRxCallback.

Referenced by USBDCDCSetRxCBData().

§ pfnTxCallback

const tUSBCallback tUSBDCDCDevice::pfnTxCallback

A pointer to the callback function which will be called to notify the application of events related to the device's data transmit channel.

Referenced by USBDCDCCompositeInit().

§ pvTxCBData

void* tUSBDCDCDevice::pvTxCBData

A client-supplied pointer which will be sent as the first parameter in all calls made to the transmit channel callback, pfnTxCallback.

Referenced by USBDCDCSetTxCBData().

§ ppui8StringDescriptors

const uint8_t* const* tUSBDCDCDevice::ppui8StringDescriptors

A pointer to the string descriptor array for this device. This array must contain the following string descriptor pointers in this order. Language descriptor, Manufacturer name string (language 1), Product name string (language 1), Serial number string (language 1), Control interface description string (language 1), Configuration description string (language 1).

If supporting more than 1 language, the strings for indices 1 through 5 must be repeated for each of the other languages defined in the language descriptor.

§ ui32NumStringDescriptors

const uint32_t tUSBDCDCDevice::ui32NumStringDescriptors

The number of descriptors provided in the ppStringDescriptors array. This must be 1 + (5 * number of supported languages).

§ sPrivateData

tCDCSerInstance tUSBDCDCDevice::sPrivateData

The private instance data for this device. This memory must remain accessible for as long as the CDC device is in use and must not be modified by any code outside the CDC class driver.

Referenced by ProcessDataFromHost(), ProcessDataToHost(), ProcessNotificationToHost(), USBDCDCCompositeInit(), and USBDCDCInit().


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated