![]() |
![]() |
#include <usbdaudio.h>
Data Fields | |
const uint16_t | ui16VID |
The vendor ID that this device is to present in the device descriptor. More... | |
const uint16_t | ui16PID |
The product ID that this device is to present in the device descriptor. More... | |
const char | pcVendor [8] |
8 byte vendor string. More... | |
const char | pcProduct [16] |
16 byte vendor string. More... | |
const char | pcVersion [4] |
4 byte vendor string. More... | |
const uint16_t | ui16MaxPowermA |
The maximum power consumption of the device, expressed in mA. More... | |
const uint8_t | ui8PwrAttributes |
const tUSBCallback | pfnCallback |
const uint8_t *const * | ppui8StringDescriptors |
const uint32_t | ui32NumStringDescriptors |
const int16_t | i16VolumeMax |
The maximum volume expressed as an 8.8 signed value. More... | |
const int16_t | i16VolumeMin |
The minimum volume expressed as an 8.8 signed value. More... | |
const int16_t | i16VolumeStep |
The minimum volume step expressed as an 8.8 signed value. More... | |
tAudioInstance | sPrivateData |
The private instance data for the audio device. More... | |
The structure used by the application to define operating parameters for the device audio class.
const uint16_t tUSBDAudioDevice::ui16VID |
The vendor ID that this device is to present in the device descriptor.
const uint16_t tUSBDAudioDevice::ui16PID |
The product ID that this device is to present in the device descriptor.
const char tUSBDAudioDevice::pcVendor[8] |
8 byte vendor string.
const char tUSBDAudioDevice::pcProduct[16] |
16 byte vendor string.
const char tUSBDAudioDevice::pcVersion[4] |
4 byte vendor string.
const uint16_t tUSBDAudioDevice::ui16MaxPowermA |
The maximum power consumption of the device, expressed in mA.
const uint8_t tUSBDAudioDevice::ui8PwrAttributes |
Indicates whether the device is self or bus-powered and whether or not it supports remote wake up. Valid values are USB_CONF_ATTR_SELF_PWR or USB_CONF_ATTR_BUS_PWR, optionally ORed with USB_CONF_ATTR_RWAKE.
const tUSBCallback tUSBDAudioDevice::pfnCallback |
A pointer to the callback function which will be called to notify the application of events relating to the operation of the audio device.
const uint8_t* const* tUSBDAudioDevice::ppui8StringDescriptors |
A pointer to the string descriptor array for this device. This array must contain the following string descriptor pointers in this order. Language descriptor, Manufacturer name string (language 1), Product name string (language 1), Serial number string (language 1), Audio Interface description string (language 1), Configuration description string (language 1).
If supporting more than 1 language, the descriptor block (except for string descriptor 0) must be repeated for each language defined in the language descriptor.
Referenced by USBDAudioCompositeInit(), and USBDAudioInit().
const uint32_t tUSBDAudioDevice::ui32NumStringDescriptors |
The number of descriptors provided in the ppStringDescriptors array. This must be 1 + ((5 + (number of strings)) * (number of languages)).
const int16_t tUSBDAudioDevice::i16VolumeMax |
The maximum volume expressed as an 8.8 signed value.
const int16_t tUSBDAudioDevice::i16VolumeMin |
The minimum volume expressed as an 8.8 signed value.
const int16_t tUSBDAudioDevice::i16VolumeStep |
The minimum volume step expressed as an 8.8 signed value.
tAudioInstance tUSBDAudioDevice::sPrivateData |
The private instance data for the audio device.
Referenced by USBAudioBufferOut(), and USBDAudioCompositeInit().