![]() |
![]() |
#include <usblib.h>
Data Fields | |
| uint8_t | ui8NumSections |
| const tConfigSection *const * | psSections |
This is the top level structure defining a USB device configuration descriptor. A configuration descriptor contains a collection of device- specific descriptors in addition to the basic config, interface and endpoint descriptors. To allow flexibility in constructing the configuration, the descriptor is described in terms of a list of data blocks. The first block must contain the configuration descriptor itself and the following blocks are appended to this in order to produce the full descriptor sent to the host in response to a GetDescriptor request for the configuration descriptor.
| uint8_t tConfigHeader::ui8NumSections |
The number of sections comprising the full descriptor for this configuration.
Referenced by BuildCompositeDescriptor(), USBDCDConfigDescGet(), USBDCDConfigDescGetNum(), and USBDCDConfigDescGetSize().
| const tConfigSection* const* tConfigHeader::psSections |
A pointer to an array of ui8NumSections section pointers which must be concatenated to form the configuration descriptor.
Referenced by BuildCompositeDescriptor(), USBDCDConfigDescGet(), USBDCDConfigDescGetNum(), USBDCDConfigDescGetSize(), and USBDCDConfigGetNumAlternateInterfaces().