![]() |
![]() |
SPIMSP432E4DMA Object. More...
#include <SPIMSP432E4DMA.h>
Data Fields | |
HwiP_Handle | hwiHandle |
SemaphoreP_Handle | transferComplete |
SPI_CallbackFxn | transferCallbackFxn |
SPI_Transaction * | transaction |
UDMAMSP432E4_Handle | dmaHandle |
size_t | amtDataXferred |
size_t | currentXferAmt |
uint32_t | bitRate |
uint32_t | dataSize |
uint32_t | transferTimeout |
SPI_Mode | spiMode |
SPI_TransferMode | transferMode |
bool | cancelInProgress |
bool | isOpen |
uint8_t | format |
SPIMSP432E4DMA Object.
The application must not access any member variables of this structure!
HwiP_Handle SPIMSP432E4DMA_Object::hwiHandle |
SemaphoreP_Handle SPIMSP432E4DMA_Object::transferComplete |
SPI_CallbackFxn SPIMSP432E4DMA_Object::transferCallbackFxn |
SPI_Transaction* SPIMSP432E4DMA_Object::transaction |
UDMAMSP432E4_Handle SPIMSP432E4DMA_Object::dmaHandle |
size_t SPIMSP432E4DMA_Object::amtDataXferred |
size_t SPIMSP432E4DMA_Object::currentXferAmt |
uint32_t SPIMSP432E4DMA_Object::bitRate |
uint32_t SPIMSP432E4DMA_Object::dataSize |
uint32_t SPIMSP432E4DMA_Object::transferTimeout |
SPI_Mode SPIMSP432E4DMA_Object::spiMode |
SPI_TransferMode SPIMSP432E4DMA_Object::transferMode |
bool SPIMSP432E4DMA_Object::cancelInProgress |
bool SPIMSP432E4DMA_Object::isOpen |
uint8_t SPIMSP432E4DMA_Object::format |