![]() |
![]() |
Macros | |
#define | ECDH_STATUS_SUCCESS (0) |
Successful status code. More... | |
#define | ECDH_STATUS_ERROR (-1) |
Generic error status code. More... | |
#define | ECDH_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by ECDH_control() for undefined command codes. More... | |
#define | ECDH_STATUS_RESOURCE_UNAVAILABLE (-3) |
An error status code returned if the hardware or software resource is currently unavailable. More... | |
#define | ECDH_STATUS_RESULT_POINT_AT_INFINITY (-4) |
The result of the operation is the point at infinity. More... | |
#define | ECDH_STATUS_RESULT_PRIVATE_KEY_LARGER_THAN_ORDER (-5) |
The private key passed in is larger than the order of the curve. More... | |
#define | ECDH_STATUS_RESULT_PUBLIC_KEY_NOT_ON_CURVE (-6) |
The public key of the other party does not lie upon the curve. More... | |
ECDH_STATUS_* macros are general status codes returned by ECC functions
#define ECDH_STATUS_SUCCESS (0) |
Successful status code.
Function return ECDH_STATUS_SUCCESS if the control code was executed successfully.
#define ECDH_STATUS_ERROR (-1) |
Generic error status code.
Functions return ECDH_STATUS_ERROR if the control code was not executed successfully.
#define ECDH_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by ECDH_control() for undefined command codes.
ECDH_control() returns ECDH_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.
#define ECDH_STATUS_RESOURCE_UNAVAILABLE (-3) |
An error status code returned if the hardware or software resource is currently unavailable.
ECC driver implementations may have hardware or software limitations on how many clients can simultaneously perform operations. This status code is returned if the mutual exclusion mechanism signals that an operation cannot currently be performed.
#define ECDH_STATUS_RESULT_POINT_AT_INFINITY (-4) |
The result of the operation is the point at infinity.
The operation yielded the point at infinity on this curve. This point is not permitted for further use in ECC operations.
#define ECDH_STATUS_RESULT_PRIVATE_KEY_LARGER_THAN_ORDER (-5) |
The private key passed in is larger than the order of the curve.
Private keys must be integers in the interval [1, n - 1], where n is the order of the curve.
#define ECDH_STATUS_RESULT_PUBLIC_KEY_NOT_ON_CURVE (-6) |
The public key of the other party does not lie upon the curve.
The public key received from the other party does not lie upon the agreed upon curve.