Sockets related commands and configuration.
More...
|
| #define | SLNETUTIL_IPV4_VAL(add_3, add_2, add_1, add_0) ((((uint32_t)add_3 << 24) & 0xFF000000) | (((uint32_t)add_2 << 16) & 0xFF0000) | (((uint32_t)add_1 << 8) & 0xFF00) | ((uint32_t)add_0 & 0xFF) ) |
| |
|
| int32_t | SlNetutil_init (int32_t flags) |
| | Initialize the slnetutil module. More...
|
| |
| int32_t | SlNetUtil_getHostByName (uint32_t ifBitmap, char *name, const uint16_t nameLen, uint32_t **ipAddr, uint16_t *ipAddrLen, const uint8_t family) |
| | Get host IP by name
Obtain the IP Address of machine on network, by machine name. More...
|
| |
| uint32_t | SlNetUtil_htonl (uint32_t val) |
| | Reorder the bytes of a 32-bit unsigned value. More...
|
| |
| uint32_t | SlNetUtil_ntohl (uint32_t val) |
| | Reorder the bytes of a 32-bit unsigned value. More...
|
| |
| uint16_t | SlNetUtil_htons (uint16_t val) |
| | Reorder the bytes of a 16-bit unsigned value. More...
|
| |
| uint16_t | SlNetUtil_ntohs (uint16_t val) |
| | Reorder the bytes of a 16-bit unsigned value. More...
|
| |
| const char * | SlNetUtil_inetNtop (int16_t addrFamily, const void *binaryAddr, char *strAddr, SlNetSocklen_t strAddrLen) |
| | Converts IP address in binary representation to string representation. More...
|
| |
| int32_t | SlNetUtil_inetPton (int16_t addrFamily, const char *strAddr, void *binaryAddr) |
| | Converts IP address in string representation to binary representation. More...
|
| |
Sockets related commands and configuration.
§ SLNETUTIL_IPV4_VAL
| #define SLNETUTIL_IPV4_VAL |
( |
|
add_3, |
|
|
|
add_2, |
|
|
|
add_1, |
|
|
|
add_0 |
|
) |
| ((((uint32_t)add_3 << 24) & 0xFF000000) | (((uint32_t)add_2 << 16) & 0xFF0000) | (((uint32_t)add_1 << 8) & 0xFF00) | ((uint32_t)add_0 & 0xFF) ) |
§ SlNetutil_init()
| int32_t SlNetutil_init |
( |
int32_t |
flags | ) |
|
Initialize the slnetutil module.
The SlNetutil_init function Initialize the slnetutil module.
- Parameters
-
| [in] | flags | For future usage, The value 0 may be used in order to run the default flags |
- Returns
- Zero on success, or negative error code on failure
- See also
- Note
- Warning
§ SlNetUtil_getHostByName()
| int32_t SlNetUtil_getHostByName |
( |
uint32_t |
ifBitmap, |
|
|
char * |
name, |
|
|
const uint16_t |
nameLen, |
|
|
uint32_t ** |
ipAddr, |
|
|
uint16_t * |
ipAddrLen, |
|
|
const uint8_t |
family |
|
) |
| |
Get host IP by name
Obtain the IP Address of machine on network, by machine name.
- Parameters
-
| [in] | ifBitmap | Specifies the interfaces which the the host ip needs to be retrieved from according tothe priority until one of them will return an answer.
Value 0 is used in order to choose automatic interfaces selection according to the priority interface list. Value can be combination of interfaces by OR'ing multiple interfaces bit identifiers (SLNETIFC_IDENT_ defined in slnetif.h) Note: interface identifier bit must be configured prior to this socket creation using SlNetIf_add function. |
| [in] | name | Host name |
| [in] | nameLen | Name length |
| [out] | ipAddr | This parameter is filled in with an array of host IP addresses. In case that host name is not resolved, out_ip_addr is zero. |
| [in,out] | ipAddrLen | Holds the size of the ipAddr array, when function successful, the ipAddrLen parameter will be updated with the number of the IP addresses found. |
| [in] | family | Protocol family |
- Returns
- Zero on success, or negative on failure.
SLNETUTIL_POOL_IS_EMPTY may be return in case there are no resources in the system
In this case try again later or increase MAX_CONCURRENT_ACTIONS Possible DNS error codes:
- SLNETUTIL_DNS_QUERY_NO_RESPONSE
- SLNETUTIL_DNS_NO_SERVER
- SLNETUTIL_DNS_QUERY_FAILED
- SLNETUTIL_DNS_MALFORMED_PACKET
- SLNETUTIL_DNS_MISMATCHED_RESPONSE
- See also
- Note
- Only one SlNetUtil_getHostByName can be handled at a time.
Calling this API while the same command is called from another thread, may result in one of the two scenarios:
- The command will wait (internal) until the previous command finish, and then be executed.
- There are not enough resources and POOL_IS_EMPTY error will return.
In this case, MAX_CONCURRENT_ACTIONS can be increased (result in memory increase) or try again later to issue the command.
- Warning
- In case an IP address in a string format is set as input, without any prefix (e.g. "1.2.3.4") the device will not try to access the DNS and it will return the input address on the 'out_ip_addr' field
- Example
- Getting host by name:
uint16_t DestinationIPLen = 1;
uint32_t DestinationIP[1];
uint32_t AddrSize;
int16_t SockId;
SlSockAddrIn_t Addr;
Addr.sin_port = SlNetSock_htons(80);
Addr.sin_addr.s_addr = SlNetSock_htonl(DestinationIP[0]);
AddrSize = sizeof(SlSockAddrIn_t);
§ SlNetUtil_htonl()
| uint32_t SlNetUtil_htonl |
( |
uint32_t |
val | ) |
|
§ SlNetUtil_ntohl()
| uint32_t SlNetUtil_ntohl |
( |
uint32_t |
val | ) |
|
§ SlNetUtil_htons()
| uint16_t SlNetUtil_htons |
( |
uint16_t |
val | ) |
|
Reorder the bytes of a 16-bit unsigned value.
This functions is used to reorder the bytes of a 16-bit unsigned value from host order to network order.
- Parameters
-
| [in] | val | Variable in host order |
- Returns
- Return the variable in network order
- See also
- SlNetSock_bind SlNetSock_connect SlNetSock_recvFrom SlNetSock_accept
- Note
- Warning
§ SlNetUtil_ntohs()
| uint16_t SlNetUtil_ntohs |
( |
uint16_t |
val | ) |
|
Reorder the bytes of a 16-bit unsigned value.
This functions is used to reorder the bytes of a 16-bit unsigned value from network order to host order.
- Parameters
-
| [in] | val | Variable in network order |
- Returns
- Return the variable in host order
- See also
- SlNetSock_bind SlNetSock_connect SlNetSock_recvFrom SlNetSock_accept
- Note
- Warning
§ SlNetUtil_inetNtop()
| const char* SlNetUtil_inetNtop |
( |
int16_t |
addrFamily, |
|
|
const void * |
binaryAddr, |
|
|
char * |
strAddr, |
|
|
SlNetSocklen_t |
strAddrLen |
|
) |
| |
Converts IP address in binary representation to string representation.
This functions is used to converts IP address in binary representation to IP address in string representation.
- Parameters
-
| [in] | addrFamily | Specifies the address family of the created socket For example:
- SLNETSOCK_AF_INET for network address IPv4
- SLNETSOCK_AF_INET6 for network address IPv6
|
| [in] | binaryAddr | Pointer to an IP address structure indicating the address in binary representation |
| [out] | strAddr | Pointer to the address string representation for IPv4 or IPv6 according to the address family |
| [in] | strAddrLen | Specifies the length of the StrAddress_dst, the maximum length of the address in string representation for IPv4 or IPv6 according to the address family |
- Returns
- strAddr on success, or NULL on failure
- See also
- Note
- Warning
- Example
-
§ SlNetUtil_inetPton()
| int32_t SlNetUtil_inetPton |
( |
int16_t |
addrFamily, |
|
|
const char * |
strAddr, |
|
|
void * |
binaryAddr |
|
) |
| |
Converts IP address in string representation to binary representation.
This functions is used to converts IP address in string representation to IP address in binary representation.
- Parameters
-
| [in] | addrFamily | Specifies the address family of the created socket For example:
- SLNETSOCK_AF_INET for network address IPv4
- SLNETSOCK_AF_INET6 for network address IPv6
|
| [out] | strAddr | Specifies the IP address in string representation for IPv4 or IPv6 according to the address family |
| [in] | binaryAddr | Pointer to an address structure that will be filled by the IP address in Binary representation |
- Returns
- 1 on success, -1 on failure, or 0 if the input isn't a valid IP address
- See also
- Note
- Warning
- Example
-