All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Modules Pages
Macros | Functions
sysexc.h File Reference
#include <stdint.h>
#include <stdbool.h>

Go to the source code of this file.

Macros

#define SYSEXC_INT_FP_IXC   0x00000020
 
#define SYSEXC_INT_FP_OFC   0x00000010
 
#define SYSEXC_INT_FP_UFC   0x00000008
 
#define SYSEXC_INT_FP_IOC   0x00000004
 
#define SYSEXC_INT_FP_DZC   0x00000002
 
#define SYSEXC_INT_FP_IDC   0x00000001
 

Functions

void SysExcIntRegister (void(*pfnHandler)(void))
 
void SysExcIntUnregister (void)
 
void SysExcIntEnable (uint32_t ui32IntFlags)
 
void SysExcIntDisable (uint32_t ui32IntFlags)
 
uint32_t SysExcIntStatus (bool bMasked)
 
void SysExcIntClear (uint32_t ui32IntFlags)
 

Macro Definition Documentation

§ SYSEXC_INT_FP_IXC

#define SYSEXC_INT_FP_IXC   0x00000020

§ SYSEXC_INT_FP_OFC

#define SYSEXC_INT_FP_OFC   0x00000010

§ SYSEXC_INT_FP_UFC

#define SYSEXC_INT_FP_UFC   0x00000008

§ SYSEXC_INT_FP_IOC

#define SYSEXC_INT_FP_IOC   0x00000004

§ SYSEXC_INT_FP_DZC

#define SYSEXC_INT_FP_DZC   0x00000002

§ SYSEXC_INT_FP_IDC

#define SYSEXC_INT_FP_IDC   0x00000001
Copyright 2017, Texas Instruments Incorporated