All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Modules Pages
Functions
Watchdog_api

Functions

bool WatchdogRunning (uint32_t ui32Base)
 
void WatchdogEnable (uint32_t ui32Base)
 
void WatchdogResetEnable (uint32_t ui32Base)
 
void WatchdogResetDisable (uint32_t ui32Base)
 
void WatchdogLock (uint32_t ui32Base)
 
void WatchdogUnlock (uint32_t ui32Base)
 
bool WatchdogLockState (uint32_t ui32Base)
 
void WatchdogReloadSet (uint32_t ui32Base, uint32_t ui32LoadVal)
 
uint32_t WatchdogReloadGet (uint32_t ui32Base)
 
uint32_t WatchdogValueGet (uint32_t ui32Base)
 
void WatchdogIntRegister (uint32_t ui32Base, void(*pfnHandler)(void))
 
void WatchdogIntUnregister (uint32_t ui32Base)
 
void WatchdogIntEnable (uint32_t ui32Base)
 
uint32_t WatchdogIntStatus (uint32_t ui32Base, bool bMasked)
 
void WatchdogIntClear (uint32_t ui32Base)
 
void WatchdogIntTypeSet (uint32_t ui32Base, uint32_t ui32Type)
 
void WatchdogStallEnable (uint32_t ui32Base)
 
void WatchdogStallDisable (uint32_t ui32Base)
 

Detailed Description

Function Documentation

§ WatchdogRunning()

bool WatchdogRunning ( uint32_t  ui32Base)

Determines if the watchdog timer is enabled.

Parameters
ui32Baseis the base address of the watchdog timer module.

This function checks to see if the watchdog timer is enabled.

Returns
Returns true if the watchdog timer is enabled and false if it is not.

References ASSERT, HWREG, WDT_CTL_INTEN, and WDT_O_CTL.

§ WatchdogEnable()

void WatchdogEnable ( uint32_t  ui32Base)

Enables the watchdog timer.

Parameters
ui32Baseis the base address of the watchdog timer module.

This function enables the watchdog timer counter and interrupt.

Note
This function has no effect if the watchdog timer has been locked.
Returns
None.

References ASSERT, HWREG, WDT_CTL_INTEN, and WDT_O_CTL.

§ WatchdogResetEnable()

void WatchdogResetEnable ( uint32_t  ui32Base)

Enables the watchdog timer reset.

Parameters
ui32Baseis the base address of the watchdog timer module.

This function enables the capability of the watchdog timer to issue a reset to the processor after a second timeout condition.

Note
This function has no effect if the watchdog timer has been locked.
Returns
None.

References ASSERT, HWREG, WDT_CTL_RESEN, and WDT_O_CTL.

§ WatchdogResetDisable()

void WatchdogResetDisable ( uint32_t  ui32Base)

Disables the watchdog timer reset.

Parameters
ui32Baseis the base address of the watchdog timer module.

This function disables the capability of the watchdog timer to issue a reset to the processor after a second timeout condition.

Note
This function has no effect if the watchdog timer has been locked.
Returns
None.

References ASSERT, HWREG, WDT_CTL_RESEN, and WDT_O_CTL.

§ WatchdogLock()

void WatchdogLock ( uint32_t  ui32Base)

Enables the watchdog timer lock mechanism.

Parameters
ui32Baseis the base address of the watchdog timer module.

This function locks out write access to the watchdog timer registers.

Returns
None.

References ASSERT, HWREG, WDT_LOCK_LOCKED, and WDT_O_LOCK.

§ WatchdogUnlock()

void WatchdogUnlock ( uint32_t  ui32Base)

Disables the watchdog timer lock mechanism.

Parameters
ui32Baseis the base address of the watchdog timer module.

This function enables write access to the watchdog timer registers.

Returns
None.

References ASSERT, HWREG, WDT_LOCK_UNLOCK, and WDT_O_LOCK.

§ WatchdogLockState()

bool WatchdogLockState ( uint32_t  ui32Base)

Gets the state of the watchdog timer lock mechanism.

Parameters
ui32Baseis the base address of the watchdog timer module.

This function returns the lock state of the watchdog timer registers.

Returns
Returns true if the watchdog timer registers are locked, and false if they are not locked.

References ASSERT, HWREG, WDT_LOCK_LOCKED, and WDT_O_LOCK.

§ WatchdogReloadSet()

void WatchdogReloadSet ( uint32_t  ui32Base,
uint32_t  ui32LoadVal 
)

Sets the watchdog timer reload value.

Parameters
ui32Baseis the base address of the watchdog timer module.
ui32LoadValis the load value for the watchdog timer.

This function configures the value to load into the watchdog timer when the count reaches zero for the first time; if the watchdog timer is running when this function is called, then the value is immediately loaded into the watchdog timer counter. If the ui32LoadVal parameter is 0, then an interrupt is immediately generated.

Note
This function has no effect if the watchdog timer has been locked.
Returns
None.

References ASSERT, HWREG, and WDT_O_LOAD.

§ WatchdogReloadGet()

uint32_t WatchdogReloadGet ( uint32_t  ui32Base)

Gets the watchdog timer reload value.

Parameters
ui32Baseis the base address of the watchdog timer module.

This function gets the value that is loaded into the watchdog timer when the count reaches zero for the first time.

Returns
None.

References ASSERT, HWREG, and WDT_O_LOAD.

§ WatchdogValueGet()

uint32_t WatchdogValueGet ( uint32_t  ui32Base)

Gets the current watchdog timer value.

Parameters
ui32Baseis the base address of the watchdog timer module.

This function reads the current value of the watchdog timer.

Returns
Returns the current value of the watchdog timer.

References ASSERT, HWREG, and WDT_O_VALUE.

§ WatchdogIntRegister()

void WatchdogIntRegister ( uint32_t  ui32Base,
void(*)(void)  pfnHandler 
)

Registers an interrupt handler for the watchdog timer interrupt.

Parameters
ui32Baseis the base address of the watchdog timer module.
pfnHandleris a pointer to the function to be called when the watchdog timer interrupt occurs.

This function does the actual registering of the interrupt handler. This function also enables the global interrupt in the interrupt controller; the watchdog timer interrupt must be enabled via WatchdogEnable(). It is the interrupt handler's responsibility to clear the interrupt source via WatchdogIntClear().

See also
IntRegister() for important information about registering interrupt handlers.
Note
The Watchdog timer module has the ability to generate an NMI instead of a standard interrupt. This function registers the standard watchdog interrupt handler. To register the NMI watchdog handler, use IntRegister() to register the handler for the FAULT_NMI interrupt.
Returns
None.

References ASSERT, INT_WATCHDOG, IntEnable(), and IntRegister().

§ WatchdogIntUnregister()

void WatchdogIntUnregister ( uint32_t  ui32Base)

Unregisters an interrupt handler for the watchdog timer interrupt.

Parameters
ui32Baseis the base address of the watchdog timer module.

This function does the actual unregistering of the interrupt handler. This function clears the handler to be called when a watchdog timer interrupt occurs. This function also masks off the interrupt in the interrupt controller so that the interrupt handler no longer is called.

See also
IntRegister() for important information about registering interrupt handlers.
Note
The Watchdog timer module has the ability to generate an NMI instead of a standard interrupt. This function unregisters the standard watchdog interrupt handler. To unregister the NMI watchdog handler, use IntUnregister() to unregister the handler for the FAULT_NMI interrupt.
Returns
None.

References ASSERT, INT_WATCHDOG, IntDisable(), and IntUnregister().

§ WatchdogIntEnable()

void WatchdogIntEnable ( uint32_t  ui32Base)

Enables the watchdog timer interrupt.

Parameters
ui32Baseis the base address of the watchdog timer module.

This function enables the watchdog timer interrupt.

Note
This function has no effect if the watchdog timer has been locked.
Returns
None.

References ASSERT, HWREG, WDT_CTL_INTEN, and WDT_O_CTL.

§ WatchdogIntStatus()

uint32_t WatchdogIntStatus ( uint32_t  ui32Base,
bool  bMasked 
)

Gets the current watchdog timer interrupt status.

Parameters
ui32Baseis the base address of the watchdog timer module.
bMaskedis false if the raw interrupt status is required and true if the masked interrupt status is required.

This function returns the interrupt status for the watchdog timer module. Either the raw interrupt status or the status of interrupt that is allowed to reflect to the processor can be returned.

Returns
Returns the current interrupt status, where a 1 indicates that the watchdog interrupt is active, and a 0 indicates that it is not active.

References ASSERT, HWREG, WDT_O_MIS, and WDT_O_RIS.

§ WatchdogIntClear()

void WatchdogIntClear ( uint32_t  ui32Base)

Clears the watchdog timer interrupt.

Parameters
ui32Baseis the base address of the watchdog timer module.

The watchdog timer interrupt source is cleared, so that it no longer asserts.

Note
Because there is a write buffer in the Cortex-M processor, it may take several clock cycles before the interrupt source is actually cleared. Therefore, it is recommended that the interrupt source be cleared early in the interrupt handler (as opposed to the very last action) to avoid returning from the interrupt handler before the interrupt source is actually cleared. Failure to do so may result in the interrupt handler being immediately reentered (because the interrupt controller still sees the interrupt source asserted). This function has no effect if the watchdog timer has been locked.
Returns
None.

References ASSERT, HWREG, WDT_O_ICR, and WDT_RIS_WDTRIS.

§ WatchdogIntTypeSet()

void WatchdogIntTypeSet ( uint32_t  ui32Base,
uint32_t  ui32Type 
)

Sets the type of interrupt generated by the watchdog.

Parameters
ui32Baseis the base address of the watchdog timer module.
ui32Typeis the type of interrupt to generate.

This function sets the type of interrupt that is generated if the watchdog timer expires. ui32Type can be either WATCHDOG_INT_TYPE_INT to generate a standard interrupt (the default) or WATCHDOG_INT_TYPE_NMI to generate a non-maskable interrupt (NMI).

When configured to generate an NMI, the watchdog interrupt must still be enabled with WatchdogIntEnable(), and it must still be cleared inside the NMI handler with WatchdogIntClear().

Note
This function has no effect if the watchdog timer has been locked.
Returns
None.

References ASSERT, HWREG, WATCHDOG_INT_TYPE_INT, WATCHDOG_INT_TYPE_NMI, WDT_CTL_INTTYPE, and WDT_O_CTL.

§ WatchdogStallEnable()

void WatchdogStallEnable ( uint32_t  ui32Base)

Enables stalling of the watchdog timer during debug events.

Parameters
ui32Baseis the base address of the watchdog timer module.

This function allows the watchdog timer to stop counting when the processor is stopped by the debugger. By doing so, the watchdog is prevented from expiring (typically almost immediately from a human time perspective) and resetting the system (if reset is enabled). The watchdog instead expires after the appropriate number of processor cycles have been executed while debugging (or at the appropriate time after the processor has been restarted).

Note
This function has no effect if the watchdog timer has been locked.
Returns
None.

References ASSERT, HWREG, WDT_O_TEST, and WDT_TEST_STALL.

§ WatchdogStallDisable()

void WatchdogStallDisable ( uint32_t  ui32Base)

Disables stalling of the watchdog timer during debug events.

Parameters
ui32Baseis the base address of the watchdog timer module.

This function disables the debug mode stall of the watchdog timer. By doing so, the watchdog timer continues to count regardless of the processor debug state.

Note
This function has no effect if the watchdog timer has been locked.
Returns
None.

References ASSERT, HWREG, WDT_O_TEST, and WDT_TEST_STALL.

Copyright 2017, Texas Instruments Incorporated