All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Modules Pages
Data Structures | Macros | Functions
Udma_api

Data Structures

struct  tDMAControlTable
 

Macros

#define uDMATaskStructEntry(ui32TransferCount, ui32ItemSize, ui32SrcIncrement, pvSrcAddr, ui32DstIncrement, pvDstAddr, ui32ArbSize, ui32Mode)
 

Functions

void uDMAEnable (void)
 
void uDMADisable (void)
 
uint32_t uDMAErrorStatusGet (void)
 
void uDMAErrorStatusClear (void)
 
void uDMAChannelEnable (uint32_t ui32ChannelNum)
 
void uDMAChannelDisable (uint32_t ui32ChannelNum)
 
bool uDMAChannelIsEnabled (uint32_t ui32ChannelNum)
 
void uDMAControlBaseSet (void *psControlTable)
 
void * uDMAControlBaseGet (void)
 
void * uDMAControlAlternateBaseGet (void)
 
void uDMAChannelRequest (uint32_t ui32ChannelNum)
 
void uDMAChannelAttributeEnable (uint32_t ui32ChannelNum, uint32_t ui32Attr)
 
void uDMAChannelAttributeDisable (uint32_t ui32ChannelNum, uint32_t ui32Attr)
 
uint32_t uDMAChannelAttributeGet (uint32_t ui32ChannelNum)
 
void uDMAChannelControlSet (uint32_t ui32ChannelStructIndex, uint32_t ui32Control)
 
void uDMAChannelTransferSet (uint32_t ui32ChannelStructIndex, uint32_t ui32Mode, void *pvSrcAddr, void *pvDstAddr, uint32_t ui32TransferSize)
 
void uDMAChannelScatterGatherSet (uint32_t ui32ChannelNum, uint32_t ui32TaskCount, void *pvTaskList, uint32_t ui32IsPeriphSG)
 
uint32_t uDMAChannelSizeGet (uint32_t ui32ChannelStructIndex)
 
uint32_t uDMAChannelModeGet (uint32_t ui32ChannelStructIndex)
 
void uDMAIntRegister (uint32_t ui32IntChannel, void(*pfnHandler)(void))
 
void uDMAIntUnregister (uint32_t ui32IntChannel)
 
void uDMAChannelAssign (uint32_t ui32Mapping)
 

Detailed Description

Macro Definition Documentation

§ uDMATaskStructEntry

#define uDMATaskStructEntry (   ui32TransferCount,
  ui32ItemSize,
  ui32SrcIncrement,
  pvSrcAddr,
  ui32DstIncrement,
  pvDstAddr,
  ui32ArbSize,
  ui32Mode 
)
Value:
{ \
(((ui32SrcIncrement) == UDMA_SRC_INC_NONE) ? (void *)(pvSrcAddr) : \
((void *)(&((uint8_t *)(pvSrcAddr))[((ui32TransferCount) << \
((ui32SrcIncrement) >> 26)) - 1]))), \
(((ui32DstIncrement) == UDMA_DST_INC_NONE) ? (void *)(pvDstAddr) :\
((void *)(&((uint8_t *)(pvDstAddr))[((ui32TransferCount) << \
((ui32DstIncrement) >> 30)) - 1]))), \
(ui32SrcIncrement) | (ui32DstIncrement) | (ui32ItemSize) | \
(ui32ArbSize) | \
(((ui32TransferCount) - 1) << 4) | \
((((ui32Mode) == UDMA_MODE_MEM_SCATTER_GATHER) || \
((ui32Mode) == UDMA_MODE_PER_SCATTER_GATHER)) ? \
(ui32Mode) | UDMA_MODE_ALT_SELECT : (ui32Mode)), 0 \
}
#define UDMA_DST_INC_NONE
Definition: udma.h:228
#define UDMA_MODE_PER_SCATTER_GATHER
Definition: udma.h:216
#define UDMA_SRC_INC_NONE
Definition: udma.h:232
#define UDMA_MODE_MEM_SCATTER_GATHER
Definition: udma.h:214
#define UDMA_MODE_ALT_SELECT
Definition: udma.h:218

A helper macro for building scatter-gather task table entries.

Parameters
ui32TransferCountis the count of items to transfer for this task.
ui32ItemSizeis the bit size of the items to transfer for this task.
ui32SrcIncrementis the bit size increment for source data.
pvSrcAddris the starting address of the data to transfer.
ui32DstIncrementis the bit size increment for destination data.
pvDstAddris the starting address of the destination data.
ui32ArbSizeis the arbitration size to use for the transfer task.
ui32Modeis the transfer mode for this task.

This macro is intended to be used to help populate a table of uDMA tasks for a scatter-gather transfer. This macro will calculate the values for the fields of a task structure entry based on the input parameters.

There are specific requirements for the values of each parameter. No checking is done so it is up to the caller to ensure that correct values are used for the parameters.

The ui32TransferCount parameter is the number of items that will be transferred by this task. It must be in the range 1-1024.

The ui32ItemSize parameter is the bit size of the transfer data. It must be one of UDMA_SIZE_8, UDMA_SIZE_16, or UDMA_SIZE_32.

The ui32SrcIncrement parameter is the increment size for the source data. It must be one of UDMA_SRC_INC_8, UDMA_SRC_INC_16, UDMA_SRC_INC_32, or UDMA_SRC_INC_NONE.

The pvSrcAddr parameter is a void pointer to the beginning of the source data.

The ui32DstIncrement parameter is the increment size for the destination data. It must be one of UDMA_DST_INC_8, UDMA_DST_INC_16, UDMA_DST_INC_32, or UDMA_DST_INC_NONE.

The pvDstAddr parameter is a void pointer to the beginning of the location where the data will be transferred.

The ui32ArbSize parameter is the arbitration size for the transfer, and must be one of UDMA_ARB_1, UDMA_ARB_2, UDMA_ARB_4, and so on up to UDMA_ARB_1024. This is used to select the arbitration size in powers of 2, from 1 to 1024.

The ui32Mode parameter is the mode to use for this transfer task. It must be one of UDMA_MODE_BASIC, UDMA_MODE_AUTO, UDMA_MODE_MEM_SCATTER_GATHER, or UDMA_MODE_PER_SCATTER_GATHER. Note that normally all tasks will be one of the scatter-gather modes while the last task is a task list will be AUTO or BASIC.

This macro is intended to be used to initialize individual entries of a structure of tDMAControlTable type, like this:

//!     tDMAControlTable MyTaskList[] =
//!     {
//!         uDMATaskStructEntry(Task1Count, UDMA_SIZE_8,
//!                             UDMA_SRC_INC_8, MySourceBuf,
//!                             UDMA_DST_INC_8, MyDestBuf,
//!                             UDMA_ARB_8, UDMA_MODE_MEM_SCATTER_GATHER),
//!         uDMATaskStructEntry(Task2Count, ...),
//!     }
//! 
\return Nothing; this is not a function.  

Function Documentation

§ uDMAEnable()

void uDMAEnable ( void  )

Enables the uDMA controller for use.

This function enables the uDMA controller. The uDMA controller must be enabled before it can be configured and used.

Returns
None.

References HWREG, UDMA_CFG, and UDMA_CFG_MASTEN.

§ uDMADisable()

void uDMADisable ( void  )

Disables the uDMA controller for use.

This function disables the uDMA controller. Once disabled, the uDMA controller cannot operate until re-enabled with uDMAEnable().

Returns
None.

References HWREG, and UDMA_CFG.

§ uDMAErrorStatusGet()

uint32_t uDMAErrorStatusGet ( void  )

Gets the uDMA error status.

This function returns the uDMA error status. It should be called from within the uDMA error interrupt handler to determine if a uDMA error occurred.

Returns
Returns non-zero if a uDMA error is pending.

References HWREG, and UDMA_ERRCLR.

§ uDMAErrorStatusClear()

void uDMAErrorStatusClear ( void  )

Clears the uDMA error interrupt.

This function clears a pending uDMA error interrupt. This function should be called from within the uDMA error interrupt handler to clear the interrupt.

Returns
None.

References HWREG, and UDMA_ERRCLR.

§ uDMAChannelEnable()

void uDMAChannelEnable ( uint32_t  ui32ChannelNum)

Enables a uDMA channel for operation.

Parameters
ui32ChannelNumis the channel number to enable.

This function enables a specific uDMA channel for use. This function must be used to enable a channel before it can be used to perform a uDMA transfer.

When a uDMA transfer is completed, the channel is automatically disabled by the uDMA controller. Therefore, this function should be called prior to starting up any new transfer.

Returns
None.

References ASSERT, HWREG, and UDMA_ENASET.

§ uDMAChannelDisable()

void uDMAChannelDisable ( uint32_t  ui32ChannelNum)

Disables a uDMA channel for operation.

Parameters
ui32ChannelNumis the channel number to disable.

This function disables a specific uDMA channel. Once disabled, a channel cannot respond to uDMA transfer requests until re-enabled via uDMAChannelEnable().

Returns
None.

References ASSERT, HWREG, and UDMA_ENACLR.

§ uDMAChannelIsEnabled()

bool uDMAChannelIsEnabled ( uint32_t  ui32ChannelNum)

Checks if a uDMA channel is enabled for operation.

Parameters
ui32ChannelNumis the channel number to check.

This function checks to see if a specific uDMA channel is enabled. This function can be used to check the status of a transfer, as the channel is automatically disabled at the end of a transfer.

Returns
Returns true if the channel is enabled, false if disabled.

References ASSERT, HWREG, and UDMA_ENASET.

§ uDMAControlBaseSet()

void uDMAControlBaseSet ( void *  psControlTable)

Sets the base address for the channel control table.

Parameters
psControlTableis a pointer to the 1024-byte-aligned base address of the uDMA channel control table.

This function configures the base address of the channel control table. This table resides in system memory and holds control information for each uDMA channel. The table must be aligned on a 1024-byte boundary. The base address must be configured before any of the channel functions can be used.

The size of the channel control table depends on the number of uDMA channels and the transfer modes that are used. Refer to the technical reference manual and the data sheet for more information about the channel control table.

Returns
None.

References ASSERT, HWREG, and UDMA_CTLBASE.

§ uDMAControlBaseGet()

void* uDMAControlBaseGet ( void  )

Gets the base address for the channel control table.

This function gets the base address of the channel control table. This table resides in system memory and holds control information for each uDMA channel.

Returns
Returns a pointer to the base address of the channel control table.

References HWREG, and UDMA_CTLBASE.

§ uDMAControlAlternateBaseGet()

void* uDMAControlAlternateBaseGet ( void  )

Gets the base address for the channel control table alternate structures.

This function gets the base address of the second half of the channel control table that holds the alternate control structures for each channel.

Returns
Returns a pointer to the base address of the second half of the channel control table.

References HWREG, and UDMA_ALTBASE.

§ uDMAChannelRequest()

void uDMAChannelRequest ( uint32_t  ui32ChannelNum)

Requests a uDMA channel to start a transfer.

Parameters
ui32ChannelNumis the channel number on which to request a uDMA transfer.

This function allows software to request a uDMA channel to begin a transfer. This function could be used for performing a memory-to-memory transfer, or if for some reason a transfer needs to be initiated by software instead of the peripheral associated with that channel.

Note
If the channel is UDMA_CHANNEL_SW and interrupts are used, then the completion is signaled on the uDMA dedicated interrupt. If a peripheral channel is used, then the completion is signaled on the peripheral's interrupt.
Returns
None.

References ASSERT, HWREG, and UDMA_SWREQ.

§ uDMAChannelAttributeEnable()

void uDMAChannelAttributeEnable ( uint32_t  ui32ChannelNum,
uint32_t  ui32Attr 
)

Enables attributes of a uDMA channel.

Parameters
ui32ChannelNumis the channel to configure.
ui32Attris a combination of attributes for the channel.

This function is used to enable attributes of a uDMA channel.

The ui32Attr parameter is the logical OR of any of the following:

  • UDMA_ATTR_USEBURST is used to restrict transfers to use only burst mode.
  • UDMA_ATTR_ALTSELECT is used to select the alternate control structure for this channel (it is very unlikely that this flag should be used).
  • UDMA_ATTR_HIGH_PRIORITY is used to set this channel to high priority.
  • UDMA_ATTR_REQMASK is used to mask the hardware request signal from the peripheral for this channel.
Returns
None.

References ASSERT, HWREG, UDMA_ALTSET, UDMA_ATTR_ALTSELECT, UDMA_ATTR_HIGH_PRIORITY, UDMA_ATTR_REQMASK, UDMA_ATTR_USEBURST, UDMA_PRIOSET, UDMA_REQMASKSET, and UDMA_USEBURSTSET.

§ uDMAChannelAttributeDisable()

void uDMAChannelAttributeDisable ( uint32_t  ui32ChannelNum,
uint32_t  ui32Attr 
)

Disables attributes of a uDMA channel.

Parameters
ui32ChannelNumis the channel to configure.
ui32Attris a combination of attributes for the channel.

This function is used to disable attributes of a uDMA channel.

The ui32Attr parameter is the logical OR of any of the following:

  • UDMA_ATTR_USEBURST is used to restrict transfers to use only burst mode.
  • UDMA_ATTR_ALTSELECT is used to select the alternate control structure for this channel.
  • UDMA_ATTR_HIGH_PRIORITY is used to set this channel to high priority.
  • UDMA_ATTR_REQMASK is used to mask the hardware request signal from the peripheral for this channel.
Returns
None.

References ASSERT, HWREG, UDMA_ALTCLR, UDMA_ATTR_ALTSELECT, UDMA_ATTR_HIGH_PRIORITY, UDMA_ATTR_REQMASK, UDMA_ATTR_USEBURST, UDMA_PRIOCLR, UDMA_REQMASKCLR, and UDMA_USEBURSTCLR.

§ uDMAChannelAttributeGet()

uint32_t uDMAChannelAttributeGet ( uint32_t  ui32ChannelNum)

Gets the enabled attributes of a uDMA channel.

Parameters
ui32ChannelNumis the channel to configure.

This function returns a combination of flags representing the attributes of the uDMA channel.

Returns
Returns the logical OR of the attributes of the uDMA channel, which can be any of the following:
  • UDMA_ATTR_USEBURST is used to restrict transfers to use only burst mode.
  • UDMA_ATTR_ALTSELECT is used to select the alternate control structure for this channel.
  • UDMA_ATTR_HIGH_PRIORITY is used to set this channel to high priority.
  • UDMA_ATTR_REQMASK is used to mask the hardware request signal from the peripheral for this channel.

References ASSERT, HWREG, UDMA_ALTSET, UDMA_ATTR_ALTSELECT, UDMA_ATTR_HIGH_PRIORITY, UDMA_ATTR_REQMASK, UDMA_ATTR_USEBURST, UDMA_PRIOSET, UDMA_REQMASKSET, and UDMA_USEBURSTSET.

§ uDMAChannelControlSet()

void uDMAChannelControlSet ( uint32_t  ui32ChannelStructIndex,
uint32_t  ui32Control 
)

Sets the control parameters for a uDMA channel control structure.

Parameters
ui32ChannelStructIndexis the logical OR of the uDMA channel number with UDMA_PRI_SELECT or UDMA_ALT_SELECT.
ui32Controlis logical OR of several control values to set the control parameters for the channel.

This function is used to set control parameters for a uDMA transfer. These parameters are typically not changed often.

The ui32ChannelStructIndex parameter should be the logical OR of the channel number with one of UDMA_PRI_SELECT or UDMA_ALT_SELECT to choose whether the primary or alternate data structure is used.

The ui32Control parameter is the logical OR of five values: the data size, the source address increment, the destination address increment, the arbitration size, and the use burst flag. The choices available for each of these values is described below.

Choose the data size from one of UDMA_SIZE_8, UDMA_SIZE_16, or UDMA_SIZE_32 to select a data size of 8, 16, or 32 bits.

Choose the source address increment from one of UDMA_SRC_INC_8, UDMA_SRC_INC_16, UDMA_SRC_INC_32, or UDMA_SRC_INC_NONE to select an address increment of 8-bit bytes, 16-bit half-words, 32-bit words, or to select non-incrementing.

Choose the destination address increment from one of UDMA_DST_INC_8, UDMA_DST_INC_16, UDMA_DST_INC_32, or UDMA_DST_INC_NONE to select an address increment of 8-bit bytes, 16-bit half-words, 32-bit words, or to select non-incrementing.

The arbitration size determines how many items are transferred before the uDMA controller re-arbitrates for the bus. Choose the arbitration size from one of UDMA_ARB_1, UDMA_ARB_2, UDMA_ARB_4, UDMA_ARB_8, through UDMA_ARB_1024 to select the arbitration size from 1 to 1024 items, in powers of 2.

The value UDMA_NEXT_USEBURST is used to force the channel to only respond to burst requests at the tail end of a scatter-gather transfer.

Note
The address increment cannot be smaller than the data size.
Returns
None.

References ASSERT, HWREG, UDMA_CHCTL_ARBSIZE_M, UDMA_CHCTL_DSTINC_M, UDMA_CHCTL_DSTSIZE_M, UDMA_CHCTL_NXTUSEBURST, UDMA_CHCTL_SRCINC_M, UDMA_CHCTL_SRCSIZE_M, UDMA_CTLBASE, and tDMAControlTable::ui32Control.

§ uDMAChannelTransferSet()

void uDMAChannelTransferSet ( uint32_t  ui32ChannelStructIndex,
uint32_t  ui32Mode,
void *  pvSrcAddr,
void *  pvDstAddr,
uint32_t  ui32TransferSize 
)

Sets the transfer parameters for a uDMA channel control structure.

Parameters
ui32ChannelStructIndexis the logical OR of the uDMA channel number with either UDMA_PRI_SELECT or UDMA_ALT_SELECT.
ui32Modeis the type of uDMA transfer.
pvSrcAddris the source address for the transfer.
pvDstAddris the destination address for the transfer.
ui32TransferSizeis the number of data items to transfer.

This function is used to configure the parameters for a uDMA transfer. These parameters are not typically changed often. The function uDMAChannelControlSet() MUST be called at least once for this channel prior to calling this function.

The ui32ChannelStructIndex parameter should be the logical OR of the channel number with one of UDMA_PRI_SELECT or UDMA_ALT_SELECT to choose whether the primary or alternate data structure is used.

The ui32Mode parameter should be one of the following values:

  • UDMA_MODE_STOP stops the uDMA transfer. The controller sets the mode to this value at the end of a transfer.
  • UDMA_MODE_BASIC to perform a basic transfer based on request.
  • UDMA_MODE_AUTO to perform a transfer that always completes once started even if the request is removed.
  • UDMA_MODE_PINGPONG to set up a transfer that switches between the primary and alternate control structures for the channel. This mode allows use of ping-pong buffering for uDMA transfers.
  • UDMA_MODE_MEM_SCATTER_GATHER to set up a memory scatter-gather transfer.
  • UDMA_MODE_PER_SCATTER_GATHER to set up a peripheral scatter-gather transfer.

The pvSrcAddr and pvDstAddr parameters are pointers to the first location of the data to be transferred. These addresses should be aligned according to the item size. The compiler takes care of this alignment if the pointers are pointing to storage of the appropriate data type.

The ui32TransferSize parameter is the number of data items, not the number of bytes.

The two scatter-gather modes, memory and peripheral, are actually different depending on whether the primary or alternate control structure is selected. This function looks for the UDMA_PRI_SELECT and UDMA_ALT_SELECT flag along with the channel number and sets the scatter-gather mode as appropriate for the primary or alternate control structure.

The channel must also be enabled using uDMAChannelEnable() after calling this function. The transfer does not begin until the channel has been configured and enabled. Note that the channel is automatically disabled after the transfer is completed, meaning that uDMAChannelEnable() must be called again after setting up the next transfer.

Note
Great care must be taken to not modify a channel control structure that is in use or else the results are unpredictable, including the possibility of undesired data transfers to or from memory or peripherals. For BASIC and AUTO modes, it is safe to make changes when the channel is disabled, or the uDMAChannelModeGet() returns UDMA_MODE_STOP. For PINGPONG or one of the SCATTER_GATHER modes, it is safe to modify the primary or alternate control structure only when the other is being used. The uDMAChannelModeGet() function returns UDMA_MODE_STOP when a channel control structure is inactive and safe to modify.
Returns
None.

References ASSERT, HWREG, tDMAControlTable::pvDstEndAddr, tDMAControlTable::pvSrcEndAddr, UDMA_ALT_SELECT, UDMA_CHCTL_DSTINC_M, UDMA_CHCTL_SRCINC_M, UDMA_CHCTL_XFERMODE_M, UDMA_CHCTL_XFERSIZE_M, UDMA_CTLBASE, UDMA_DST_INC_NONE, UDMA_MODE_ALT_SELECT, UDMA_MODE_MEM_SCATTER_GATHER, UDMA_MODE_PER_SCATTER_GATHER, UDMA_SRC_INC_NONE, and tDMAControlTable::ui32Control.

§ uDMAChannelScatterGatherSet()

void uDMAChannelScatterGatherSet ( uint32_t  ui32ChannelNum,
uint32_t  ui32TaskCount,
void *  pvTaskList,
uint32_t  ui32IsPeriphSG 
)

Configures a uDMA channel for scatter-gather mode.

Parameters
ui32ChannelNumis the uDMA channel number.
ui32TaskCountis the number of scatter-gather tasks to execute.
pvTaskListis a pointer to the beginning of the scatter-gather task list.
ui32IsPeriphSGis a flag to indicate it is a peripheral scatter-gather transfer (else it is memory scatter-gather transfer)

This function is used to configure a channel for scatter-gather mode. The caller must have already set up a task list and must pass a pointer to the start of the task list as the pvTaskList parameter. The ui32TaskCount parameter is the count of tasks in the task list, not the size of the task list. The flag bIsPeriphSG should be used to indicate if scatter-gather should be configured for peripheral or memory operation.

See also
uDMATaskStructEntry
Returns
None.

References ASSERT, HWREG, tDMAControlTable::pvDstEndAddr, tDMAControlTable::pvSrcEndAddr, UDMA_ALT_SELECT, UDMA_ALTCLR, UDMA_CHCTL_ARBSIZE_4, UDMA_CHCTL_DSTINC_32, UDMA_CHCTL_DSTSIZE_32, UDMA_CHCTL_SRCINC_32, UDMA_CHCTL_SRCSIZE_32, UDMA_CHCTL_XFERMODE_MEM_SG, UDMA_CHCTL_XFERMODE_PER_SG, UDMA_CHCTL_XFERSIZE_S, UDMA_CTLBASE, tDMAControlTable::ui32Control, and tDMAControlTable::ui32Spare.

§ uDMAChannelSizeGet()

uint32_t uDMAChannelSizeGet ( uint32_t  ui32ChannelStructIndex)

Gets the current transfer size for a uDMA channel control structure.

Parameters
ui32ChannelStructIndexis the logical OR of the uDMA channel number with either UDMA_PRI_SELECT or UDMA_ALT_SELECT.

This function is used to get the uDMA transfer size for a channel. The transfer size is the number of items to transfer, where the size of an item might be 8, 16, or 32 bits. If a partial transfer has already occurred, then the number of remaining items is returned. If the transfer is complete, then 0 is returned.

Returns
Returns the number of items remaining to transfer.

References ASSERT, HWREG, UDMA_CHCTL_XFERMODE_M, UDMA_CHCTL_XFERSIZE_M, UDMA_CTLBASE, and tDMAControlTable::ui32Control.

§ uDMAChannelModeGet()

uint32_t uDMAChannelModeGet ( uint32_t  ui32ChannelStructIndex)

Gets the transfer mode for a uDMA channel control structure.

Parameters
ui32ChannelStructIndexis the logical OR of the uDMA channel number with either UDMA_PRI_SELECT or UDMA_ALT_SELECT.

This function is used to get the transfer mode for the uDMA channel and to query the status of a transfer on a channel. When the transfer is complete the mode is UDMA_MODE_STOP.

Returns
Returns the transfer mode of the specified channel and control structure, which is one of the following values: UDMA_MODE_STOP, UDMA_MODE_BASIC, UDMA_MODE_AUTO, UDMA_MODE_PINGPONG, UDMA_MODE_MEM_SCATTER_GATHER, or UDMA_MODE_PER_SCATTER_GATHER.

References ASSERT, HWREG, UDMA_CHCTL_XFERMODE_M, UDMA_CTLBASE, UDMA_MODE_ALT_SELECT, UDMA_MODE_MEM_SCATTER_GATHER, UDMA_MODE_PER_SCATTER_GATHER, and tDMAControlTable::ui32Control.

§ uDMAIntRegister()

void uDMAIntRegister ( uint32_t  ui32IntChannel,
void(*)(void)  pfnHandler 
)

Registers an interrupt handler for the uDMA controller.

Parameters
ui32IntChannelidentifies which uDMA interrupt is to be registered.
pfnHandleris a pointer to the function to be called when the interrupt is activated.

This function registers and enables the handler to be called when the uDMA controller generates an interrupt. The ui32IntChannel parameter should be one of the following:

  • INT_UDMA to register an interrupt handler to process interrupts from the uDMA software channel (UDMA_CHANNEL_SW)
  • INT_UDMAERR to register an interrupt handler to process uDMA error interrupts
See also
IntRegister() for important information about registering interrupt handlers.
Note
The interrupt handler for the uDMA is for transfer completion when the channel UDMA_CHANNEL_SW is used and for error interrupts. The interrupts for each peripheral channel are handled through the individual peripheral interrupt handlers.
Returns
None.

References ASSERT, IntEnable(), and IntRegister().

§ uDMAIntUnregister()

void uDMAIntUnregister ( uint32_t  ui32IntChannel)

Unregisters an interrupt handler for the uDMA controller.

Parameters
ui32IntChannelidentifies which uDMA interrupt to unregister.

This function disables and unregisters the handler to be called for the specified uDMA interrupt. The ui32IntChannel parameter should be one of INT_UDMA or INT_UDMAERR as documented for the function uDMAIntRegister().

See also
IntRegister() for important information about registering interrupt handlers.
Returns
None.

References IntDisable(), and IntUnregister().

§ uDMAChannelAssign()

void uDMAChannelAssign ( uint32_t  ui32Mapping)

Assigns a peripheral mapping for a uDMA channel.

Parameters
ui32Mappingis a macro specifying the peripheral assignment for a channel.

This function assigns a peripheral mapping to a uDMA channel. It is used to select which peripheral is used for a uDMA channel. The parameter ui32Mapping should be one of the macros named UDMA_CHn_tttt from the header file udma.h. For example, to assign uDMA channel 0 to the UART2 RX channel, the parameter should be the macro UDMA_CH0_UART2RX.

Please consult the data sheet for a table showing all the possible peripheral assignments for the uDMA channels.

Returns
None.

References ASSERT, HWREG, and UDMA_CHMAP0.

Copyright 2017, Texas Instruments Incorporated