All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Modules Pages
Macros | Enumerations | Functions
flash.h File Reference
#include <stdint.h>
#include <stdbool.h>

Go to the source code of this file.

Macros

#define FLASH_INT_PROGRAM   0x00000002
 
#define FLASH_INT_ACCESS   0x00000001
 
#define FLASH_INT_EEPROM   0x00000004
 
#define FLASH_INT_VOLTAGE_ERR   0x00000200
 
#define FLASH_INT_DATA_ERR   0x00000400
 
#define FLASH_INT_ERASE_ERR   0x00000800
 
#define FLASH_INT_PROGRAM_ERR   0x00002000
 

Enumerations

enum  tFlashProtection { FlashReadWrite, FlashReadOnly, FlashExecuteOnly }
 

Functions

int32_t FlashErase (uint32_t ui32Address)
 
int32_t FlashProgram (uint32_t *pui32Data, uint32_t ui32Address, uint32_t ui32Count)
 
tFlashProtection FlashProtectGet (uint32_t ui32Address)
 
int32_t FlashProtectSet (uint32_t ui32Address, tFlashProtection eProtect)
 
int32_t FlashProtectSave (void)
 
int32_t FlashUserGet (uint32_t *pui32User0, uint32_t *pui32User1)
 
int32_t FlashUserSet (uint32_t ui32User0, uint32_t ui32User1)
 
int32_t FlashAllUserRegisterGet (uint32_t *pui32User0, uint32_t *pui32User1, uint32_t *pui32User2, uint32_t *pui32User3)
 
int32_t FlashAllUserRegisterSet (uint32_t ui32User0, uint32_t ui32User1, uint32_t ui32User2, uint32_t ui32User3)
 
int32_t FlashUserSave (void)
 
int32_t FlashAllUserRegisterSave (void)
 
void FlashIntRegister (void(*pfnHandler)(void))
 
void FlashIntUnregister (void)
 
void FlashIntEnable (uint32_t ui32IntFlags)
 
void FlashIntDisable (uint32_t ui32IntFlags)
 
uint32_t FlashIntStatus (bool bMasked)
 
void FlashIntClear (uint32_t ui32IntFlags)
 

Macro Definition Documentation

§ FLASH_INT_PROGRAM

#define FLASH_INT_PROGRAM   0x00000002

§ FLASH_INT_ACCESS

#define FLASH_INT_ACCESS   0x00000001

§ FLASH_INT_EEPROM

#define FLASH_INT_EEPROM   0x00000004

§ FLASH_INT_VOLTAGE_ERR

#define FLASH_INT_VOLTAGE_ERR   0x00000200

§ FLASH_INT_DATA_ERR

#define FLASH_INT_DATA_ERR   0x00000400

§ FLASH_INT_ERASE_ERR

#define FLASH_INT_ERASE_ERR   0x00000800

§ FLASH_INT_PROGRAM_ERR

#define FLASH_INT_PROGRAM_ERR   0x00002000

Enumeration Type Documentation

§ tFlashProtection

Enumerator
FlashReadWrite 
FlashReadOnly 
FlashExecuteOnly 
Copyright 2017, Texas Instruments Incorporated