![]() |
![]() |
TimerMSP432 Object. More...
#include <TimerMSP432.h>
Data Fields | |
HwiP_Handle | hwiHandle |
SemaphoreP_Handle | timerSem |
Power_NotifyObj | perfChangeNotify |
uint32_t | perfConstraintMask |
Timer_CallBackFxn | callBack |
Timer_Mode | mode |
Timer_PeriodUnits | units |
uint32_t | rawPeriod |
uint32_t | period |
bool | isRunning |
TimerMSP432 Object.
The application must not access any member variables of this structure!
HwiP_Handle TimerMSP432_Object::hwiHandle |
SemaphoreP_Handle TimerMSP432_Object::timerSem |
Power_NotifyObj TimerMSP432_Object::perfChangeNotify |
uint32_t TimerMSP432_Object::perfConstraintMask |
Timer_CallBackFxn TimerMSP432_Object::callBack |
Timer_Mode TimerMSP432_Object::mode |
Timer_PeriodUnits TimerMSP432_Object::units |
uint32_t TimerMSP432_Object::rawPeriod |
uint32_t TimerMSP432_Object::period |
bool TimerMSP432_Object::isRunning |