![]() |
![]() |
![]() |
Macros | |
#define | Watchdog_STATUS_SUCCESS (0) |
Successful status code returned by Watchdog_control(). More... | |
#define | Watchdog_STATUS_ERROR (-1) |
Generic error status code returned by Watchdog_control(). More... | |
#define | Watchdog_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by Watchdog_control() for undefined command codes. More... | |
#define | Watchdog_STATUS_UNSUPPORTED (-3) |
An error status code returned by Watchdog_setReload() for drivers which do not support the aforementioned API. More... | |
Watchdog_STATUS_* macros are general status codes returned by Watchdog_control()
WatchdogMSP432_STATUS_* macros are command codes only defined in the WatchdogMSP432.h driver implementation and need to:
#define Watchdog_STATUS_SUCCESS (0) |
Successful status code returned by Watchdog_control().
Watchdog_control() returns Watchdog_STATUS_SUCCESS if the control code was executed successfully.
#define Watchdog_STATUS_ERROR (-1) |
Generic error status code returned by Watchdog_control().
Watchdog_control() returns Watchdog_STATUS_ERROR if the control code was not executed successfully.
#define Watchdog_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by Watchdog_control() for undefined command codes.
Watchdog_control() returns Watchdog_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.
#define Watchdog_STATUS_UNSUPPORTED (-3) |
An error status code returned by Watchdog_setReload() for drivers which do not support the aforementioned API.
Watchdog_setReload() returns Watchdog_STATUS_UNSUPPORTED if the driver implementation does not support the aforementioned API.