![]() |
![]() |
LZ4 API Guide
1.00.01.00
|
Compression parameters for a LZ4 frame. More...
#include <lz4.h>
Data Fields | |
const void * | src |
Pointer to the source data buffer to compress. More... | |
void * | dst |
Pointer to the destination data buffer to store compressed data. More... | |
uint32_t | length |
Length of source data buffer. More... | |
void * | hashTable |
Pointer to memory block with pow2(hashLog2Size) bytes allocated. More... | |
uint16_t | hashLog2Size |
Power of two used to determine the hash table size. More... | |
bool | addBlockChecksum |
bool | addContentChecksum |
bool | addContentSize |
Compression parameters for a LZ4 frame.
const void* LZ4_compressParams::src |
Pointer to the source data buffer to compress.
Referenced by LZ4_compress().
void* LZ4_compressParams::dst |
Pointer to the destination data buffer to store compressed data.
Referenced by LZ4_compress().
uint32_t LZ4_compressParams::length |
Length of source data buffer.
void* LZ4_compressParams::hashTable |
Pointer to memory block with pow2(hashLog2Size) bytes allocated.
uint16_t LZ4_compressParams::hashLog2Size |
Power of two used to determine the hash table size.
bool LZ4_compressParams::addBlockChecksum |
Add checksum to each compressed block. Decreases compression performance. Valid values are:
bool LZ4_compressParams::addContentChecksum |
Add checksum of original source data buffer. Decreases compression performance. Valid values are:
bool LZ4_compressParams::addContentSize |
Add total content size to LZ4 frame. Increases total frame size by 8 bytes. Valid values are: