54 #include <ti/devices/msp432p4xx/inc/msp.h> 
   62 #define PMAP_ENABLE_RECONFIGURATION     PMAP_CTL_PRECFG 
   63 #define PMAP_DISABLE_RECONFIGURATION    0x00 
   71 #define PMAP_P1MAP ((uint32_t)P1MAP - PMAP_BASE) 
   72 #define PMAP_P2MAP ((uint32_t)P2MAP - PMAP_BASE) 
   73 #define PMAP_P3MAP ((uint32_t)P3MAP - PMAP_BASE) 
   74 #define PMAP_P4MAP ((uint32_t)P4MAP - PMAP_BASE) 
   75 #define PMAP_P5MAP ((uint32_t)P5MAP - PMAP_BASE) 
   76 #define PMAP_P6MAP ((uint32_t)P6MAP - PMAP_BASE) 
   77 #define PMAP_P7MAP ((uint32_t)P7MAP - PMAP_BASE) 
  103         uint8_t numberOfPorts, uint8_t portMapReconfigure);
 
  106 #define PMAP_configurePortsMultipleInstance(a,b,c,d,e) PMAP_configurePorts(b,c,d,e) 
void PMAP_configurePorts(const uint8_t *portMapping, uint8_t pxMAPy, uint8_t numberOfPorts, uint8_t portMapReconfigure)
Definition: pmap.c:36