|  |  | 
#include <stdint.h>#include <ti/devices/msp432p4xx/driverlib/lcd_f.h>#include <ti/devices/msp432p4xx/driverlib/interrupt.h>| Functions | |
| void | LCD_F_initModule (LCD_F_Config *initParams) | 
| Initializes the LCD_F Module.  More... | |
| void | LCD_F_turnOn (void) | 
| Turns on the LCD_F module.  More... | |
| void | LCD_F_turnOff (void) | 
| Turns the LCD_F off.  More... | |
| void | LCD_F_clearAllMemory (void) | 
| Clears all LCD_F memory registers.  More... | |
| void | LCD_F_clearAllBlinkingMemory (void) | 
| Clears all LCD_F blinking memory registers.  More... | |
| void | LCD_F_selectDisplayMemory (uint_fast16_t displayMemory) | 
| Selects display memory.  More... | |
| void | LCD_F_setBlinkingControl (uint_fast16_t clockPrescalar, uint_fast16_t divider, uint_fast16_t mode) | 
| Sets the blinking control register.  More... | |
| void | LCD_F_setAnimationControl (uint_fast16_t clockPrescalar, uint_fast16_t divider, uint_fast16_t frames) | 
| Sets the animation control register.  More... | |
| void | LCD_F_enableAnimation (void) | 
| Enables animation on the LCD_F controller.  More... | |
| void | LCD_F_disableAnimation (void) | 
| Enables animation on the LCD_F controller.  More... | |
| void | LCD_F_clearAllAnimationMemory (void) | 
| Clears all LCD_F animation memory registers.  More... | |
| void | LCD_F_setPinAsLCDFunction (uint_fast8_t pin) | 
| Sets the LCD_F pins as LCD function pin.  More... | |
| void | LCD_F_setPinAsPortFunction (uint_fast8_t pin) | 
| Sets the LCD_F pins as port function pin.  More... | |
| void | LCD_F_setPinsAsLCDFunction (uint_fast8_t startPin, uint8_t endPin) | 
| Sets the LCD_F pins as LCD function pin.  More... | |
| void | LCD_F_setPinAsCOM (uint8_t pin, uint_fast8_t com) | 
| Sets the LCD_F pin as a common line.  More... | |
| void | LCD_F_setPinAsSEG (uint_fast8_t pin) | 
| Sets the LCD_F pin as a segment line.  More... | |
| void | LCD_F_selectBias (uint_fast16_t bias) | 
| Selects the bias level.  More... | |
| void | LCD_F_setVLCDSource (uint_fast16_t v2v3v4Source, uint_fast16_t v5Source) | 
| Sets the voltage source for V2/V3/V4 and V5.  More... | |
| void | LCD_F_clearInterrupt (uint32_t mask) | 
| Clears the LCD_F selected interrupt flags.  More... | |
| uint32_t | LCD_F_getInterruptStatus (void) | 
| Returns the status of the selected interrupt flags.  More... | |
| uint32_t | LCD_F_getEnabledInterruptStatus (void) | 
| Returns the status of the selected interrupt flags masked with the currently enabled interrupts.  More... | |
| void | LCD_F_enableInterrupt (uint32_t mask) | 
| Enables the LCD_F selected interrupts.  More... | |
| void | LCD_F_disableInterrupt (uint32_t mask) | 
| Disables the LCD_F selected interrupts.  More... | |
| void | LCD_F_registerInterrupt (void(*intHandler)(void)) | 
| void | LCD_F_unregisterInterrupt (void) |