55 #include <ti/devices/msp432p4xx/inc/msp.h> 
   62 #define FPU_HALF_IEEE           0x00000000 
   63 #define FPU_HALF_ALTERNATE      0x04000000 
   70 #define FPU_NAN_PROPAGATE       0x00000000 
   71 #define FPU_NAN_DEFAULT         0x02000000 
   78 #define FPU_FLUSH_TO_ZERO_DIS   0x00000000 
   79 #define FPU_FLUSH_TO_ZERO_EN    0x01000000 
   86 #define FPU_ROUND_NEAREST       0x00000000 
   87 #define FPU_ROUND_POS_INF       0x00400000 
   88 #define FPU_ROUND_NEG_INF       0x00800000 
   89 #define FPU_ROUND_ZERO          0x00c00000 
void FPU_enableStacking(void)
Definition: fpu.c:51
void FPU_disableStacking(void)
Definition: fpu.c:70
void FPU_enableModule(void)
Definition: fpu.c:34
void FPU_setHalfPrecisionMode(uint32_t mode)
Definition: fpu.c:79
void FPU_setRoundingMode(uint32_t mode)
Definition: fpu.c:103
void FPU_setFlushToZeroMode(uint32_t mode)
Definition: fpu.c:95
void FPU_setNaNMode(uint32_t mode)
Definition: fpu.c:87
void FPU_enableLazyStacking(void)
Definition: fpu.c:61
void FPU_disableModule(void)
Definition: fpu.c:43