Data Fields
UART_Config_ Struct Reference

UART Global configuration. More...

#include <UART.h>

Collaboration diagram for UART_Config_:
Collaboration graph
[legend]

Data Fields

UART_FxnTable const * fxnTablePtr
 
void * object
 
void const * hwAttrs
 

Detailed Description

UART Global configuration.

The UART_Config structure contains a set of pointers used to characterize the UART driver implementation.

This structure needs to be defined before calling UART_init() and it must not be changed thereafter.

See also
UART_init()

Field Documentation

§ fxnTablePtr

UART_FxnTable const* UART_Config_::fxnTablePtr

Pointer to a table of driver-specific implementations of UART APIs

§ object

void* UART_Config_::object

Pointer to a driver specific data object

§ hwAttrs

void const* UART_Config_::hwAttrs

Pointer to a driver specific hardware attributes structure


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale