TimerMSP432 Hardware Attributes. More...
#include <TimerMSP432.h>
Data Fields | |
uint32_t | timerBaseAddress |
uint32_t | clockSource |
uint32_t | intNum |
uint32_t | intPriority |
TimerMSP432 Hardware Attributes.
Timer hardware attributes that tell the TimerMSP432 driver specific hardware configurations and interrupt priority settings.
The Timer32 only supports MCLK as a clock source. As a result, the clockSource field has no event for Timer32 instances.
A sample structure is shown below:
uint32_t TimerMSP432_HWAttrs::timerBaseAddress |
The base address of the timer peripheral.
uint32_t TimerMSP432_HWAttrs::clockSource |
Specifies the clock source for the timer peripheral.
uint32_t TimerMSP432_HWAttrs::intNum |
The hardware interrupt number for the timer peripheral.
uint32_t TimerMSP432_HWAttrs::intPriority |
The interrupt priority.