PWMTimerMSP432_Status.
More...
#include <PWMTimerMSP432.h>
PWMTimerMSP432_Status.
The application must not access any member variables of this structure!
§ perfChangeNotify
§ periodUnits
§ perfConstraintMask
uint32_t PWMTimerMSP432_Status::perfConstraintMask |
§ clockSource
uint32_t PWMTimerMSP432_Status::clockSource |
§ duties
uint32_t PWMTimerMSP432_Status::duties[PWMTimerMSP432_NUM_PWM_OUTPUTS] |
§ periodCounts
uint32_t PWMTimerMSP432_Status::periodCounts |
§ period
uint32_t PWMTimerMSP432_Status::period |
§ prescalar
uint8_t PWMTimerMSP432_Status::prescalar |
§ activeOutputsMask
uint8_t PWMTimerMSP432_Status::activeOutputsMask |
§ openMask
uint8_t PWMTimerMSP432_Status::openMask |
The documentation for this struct was generated from the following file: