Data Fields
Capture_Config_ Struct Reference

Capture Global configuration. More...

#include <Capture.h>

Collaboration diagram for Capture_Config_:
Collaboration graph
[legend]

Data Fields

Capture_FxnTable const * fxnTablePtr
 
void * object
 
void const * hwAttrs
 

Detailed Description

Capture Global configuration.

The Capture_Config structure contains a set of pointers used to characterize the capture driver implementation.

This structure needs to be defined before calling Capture_init() and it must not be changed thereafter.

See also
Capture_init()

Field Documentation

§ fxnTablePtr

Capture_FxnTable const* Capture_Config_::fxnTablePtr

Pointer to a table of driver-specific implementations of capture APIs.

§ object

void* Capture_Config_::object

Pointer to a driver specific data object.

§ hwAttrs

void const* Capture_Config_::hwAttrs

Pointer to a driver specific hardware attributes structure.


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale