72 #ifndef ti_drivers_watchdog_WatchdogMSP432__include 73 #define ti_drivers_watchdog_WatchdogMSP432__include 80 #include <ti/drivers/dpl/HwiP.h> uint8_t clockSource
Definition: WatchdogMSP432.h:150
uint8_t intPriority
Definition: WatchdogMSP432.h:149
bool isOpen
Definition: WatchdogMSP432.h:162
HwiP_Handle hwiHandle
Definition: WatchdogMSP432.h:161
Watchdog hardware attributes for MSP432 These fields are used by driverlib APIs and therefore must be...
Definition: WatchdogMSP432.h:146
Watchdog driver interface.
uint8_t clockDivider
Definition: WatchdogMSP432.h:151
const Watchdog_FxnTable WatchdogMSP432_fxnTable
Watchdog function table for MSP432.
uint32_t baseAddr
Definition: WatchdogMSP432.h:147
uint8_t intNum
Definition: WatchdogMSP432.h:148
Watchdog_ResetMode resetMode
Definition: WatchdogMSP432.h:160
The definition of a Watchdog function table that contains the required set of functions to control a ...
Definition: Watchdog.h:362
Watchdog_ResetMode
Watchdog reset mode settings.
Definition: Watchdog.h:276
Watchdog Object for MSP432.
Definition: WatchdogMSP432.h:159