#include <lcd_f.h>
uint32_t LCD_F_initParam::clockSource |
Selects the clock that will be used by the LCD_F_E.
Valid values are:
- LCD_F_CLOCKSOURCE_XTCLK [Default]
- LCD_F_CLOCKSOURCE_ACLK [Default]
- LCD_F_CLOCKSOURCE_VLOCLK
- LCD_F_CLOCKSOURCE_LFXT
Referenced by LCD_F_initModule().
uint32_t LCD_F_initParam::clockDivider |
Selects the divider for LCD frequency.
Valid values are:
- LCD_F_CLOCKDIVIDER_1 [Default]
- LCD_F_CLOCKDIVIDER_2
- LCD_F_CLOCKDIVIDER_3
- LCD_F_CLOCKDIVIDER_4
- LCD_F_CLOCKDIVIDER_5
- LCD_F_CLOCKDIVIDER_6
- LCD_F_CLOCKDIVIDER_7
- LCD_F_CLOCKDIVIDER_8
- LCD_F_CLOCKDIVIDER_9
- LCD_F_CLOCKDIVIDER_10
- LCD_F_CLOCKDIVIDER_11
- LCD_F_CLOCKDIVIDER_12
- LCD_F_CLOCKDIVIDER_13
- LCD_F_CLOCKDIVIDER_14
- LCD_F_CLOCKDIVIDER_15
- LCD_F_CLOCKDIVIDER_16
- LCD_F_CLOCKDIVIDER_17
- LCD_F_CLOCKDIVIDER_18
- LCD_F_CLOCKDIVIDER_19
- LCD_F_CLOCKDIVIDER_20
- LCD_F_CLOCKDIVIDER_21
- LCD_F_CLOCKDIVIDER_22
- LCD_F_CLOCKDIVIDER_23
- LCD_F_CLOCKDIVIDER_24
- LCD_F_CLOCKDIVIDER_25
- LCD_F_CLOCKDIVIDER_26
- LCD_F_CLOCKDIVIDER_27
- LCD_F_CLOCKDIVIDER_28
- LCD_F_CLOCKDIVIDER_29
- LCD_F_CLOCKDIVIDER_30
- LCD_F_CLOCKDIVIDER_31
- LCD_F_CLOCKDIVIDER_32
Referenced by LCD_F_initModule().
uint32_t LCD_F_initParam::clockPrescaler |
Selects the prescaler
Valid values are:
- LCD_F_CLOCKPRESCALER_1 [Default]
- LCD_F_CLOCKPRESCALER_2
- LCD_F_CLOCKPRESCALER_4
- LCD_F_CLOCKPRESCALER_8
- LCD_F_CLOCKPRESCALER_16
- LCD_F_CLOCKPRESCALER_32
Referenced by LCD_F_initModule().
uint32_t LCD_F_initParam::muxRate |
Selects LCD_F_E mux rate.
Valid values are:
- LCD_F_STATIC [Default]
- LCD_F_2_MUX
- LCD_F_3_MUX
- LCD_F_4_MUX
- LCD_F_5_MUX
- LCD_F_6_MUX
- LCD_F_7_MUX
- LCD_F_8_MUX
Referenced by LCD_F_initModule().
uint32_t LCD_F_initParam::waveforms |
Selects LCD waveform mode.
Valid values are:
- LCD_F_STANDARD_WAVEFORMS [Default]
- LCD_F_LOW_POWER_WAVEFORMS
Referenced by LCD_F_initModule().
uint32_t LCD_F_initParam::segments |
Sets LCD segment on/off.
Valid values are:
- LCD_F_SEGMENTS_DISABLED [Default]
- LCD_F_SEGMENTS_ENABLED
Referenced by LCD_F_initModule().
The documentation for this struct was generated from the following file: