Macros | Functions
ADC14

Analog to Digital Converter with a maximum of 14-bit resolution. More...

Macros

#define ADC_CLOCKSOURCE_ADCOSC   (ADC14_CTL0_SSEL_0)
 
#define ADC_CLOCKSOURCE_SYSOSC   (ADC14_CTL0_SSEL_1)
 
#define ADC_CLOCKSOURCE_ACLK   (ADC14_CTL0_SSEL_2)
 
#define ADC_CLOCKSOURCE_MCLK   (ADC14_CTL0_SSEL_3)
 
#define ADC_CLOCKSOURCE_SMCLK   (ADC14_CTL0_SSEL_4)
 
#define ADC_CLOCKSOURCE_HSMCLK   (ADC14_CTL0_SSEL_5)
 
#define ADC_PREDIVIDER_1   (ADC14_CTL0_PDIV_0)
 
#define ADC_PREDIVIDER_4   (ADC14_CTL0_PDIV_1)
 
#define ADC_PREDIVIDER_32   (ADC14_CTL0_PDIV_2)
 
#define ADC_PREDIVIDER_64   (ADC14_CTL0_PDIV_3)
 
#define ADC_DIVIDER_1   (ADC14_CTL0_DIV_0)
 
#define ADC_DIVIDER_2   (ADC14_CTL0_DIV_1)
 
#define ADC_DIVIDER_3   (ADC14_CTL0_DIV_2)
 
#define ADC_DIVIDER_4   (ADC14_CTL0_DIV_3)
 
#define ADC_DIVIDER_5   (ADC14_CTL0_DIV_4)
 
#define ADC_DIVIDER_6   (ADC14_CTL0_DIV_5)
 
#define ADC_DIVIDER_7   (ADC14_CTL0_DIV_6)
 
#define ADC_DIVIDER_8   (ADC14_CTL0_DIV_7)
 
#define ADC_MAPINTCH3   (ADC14_CTL1_CH3MAP)
 
#define ADC_MAPINTCH2   (ADC14_CTL1_CH2MAP)
 
#define ADC_MAPINTCH1   (ADC14_CTL1_CH1MAP)
 
#define ADC_MAPINTCH0   (ADC14_CTL1_CH0MAP)
 
#define ADC_TEMPSENSEMAP   (ADC14_CTL1_TCMAP)
 
#define ADC_BATTMAP   (ADC14_CTL1_BATMAP)
 
#define ADC_NOROUTE   0
 
#define ADC_8BIT   ADC14_CTL1_RES_0
 
#define ADC_10BIT   ADC14_CTL1_RES_1
 
#define ADC_12BIT   ADC14_CTL1_RES_2
 
#define ADC_14BIT   ADC14_CTL1_RES_3
 
#define ADC_TRIGGER_ADCSC   ADC14_CTL0_SHS_0
 
#define ADC_TRIGGER_SOURCE1   ADC14_CTL0_SHS_1
 
#define ADC_TRIGGER_SOURCE2   ADC14_CTL0_SHS_2
 
#define ADC_TRIGGER_SOURCE3   ADC14_CTL0_SHS_3
 
#define ADC_TRIGGER_SOURCE4   ADC14_CTL0_SHS_4
 
#define ADC_TRIGGER_SOURCE5   ADC14_CTL0_SHS_5
 
#define ADC_TRIGGER_SOURCE6   ADC14_CTL0_SHS_6
 
#define ADC_TRIGGER_SOURCE7   ADC14_CTL0_SHS_7
 
#define ADC_PULSE_WIDTH_4   ADC14_CTL0_SHT1_0
 
#define ADC_PULSE_WIDTH_8   ADC14_CTL0_SHT1_1
 
#define ADC_PULSE_WIDTH_16   ADC14_CTL0_SHT1_2
 
#define ADC_PULSE_WIDTH_32   ADC14_CTL0_SHT1_3
 
#define ADC_PULSE_WIDTH_64   ADC14_CTL0_SHT1_4
 
#define ADC_PULSE_WIDTH_96   ADC14_CTL0_SHT1_5
 
#define ADC_PULSE_WIDTH_128   ADC14_CTL0_SHT1_6
 
#define ADC_PULSE_WIDTH_192   ADC14_CTL0_SHT1_7
 
#define ADC_NONDIFFERENTIAL_INPUTS   false
 
#define ADC_DIFFERENTIAL_INPUTS   true
 
#define ADC_MEM0   0x00000001
 
#define ADC_MEM1   0x00000002
 
#define ADC_MEM2   0x00000004
 
#define ADC_MEM3   0x00000008
 
#define ADC_MEM4   0x00000010
 
#define ADC_MEM5   0x00000020
 
#define ADC_MEM6   0x00000040
 
#define ADC_MEM7   0x00000080
 
#define ADC_MEM8   0x00000100
 
#define ADC_MEM9   0x00000200
 
#define ADC_MEM10   0x00000400
 
#define ADC_MEM11   0x00000800
 
#define ADC_MEM12   0x00001000
 
#define ADC_MEM13   0x00002000
 
#define ADC_MEM14   0x00004000
 
#define ADC_MEM15   0x00008000
 
#define ADC_MEM16   0x00010000
 
#define ADC_MEM17   0x00020000
 
#define ADC_MEM18   0x00040000
 
#define ADC_MEM19   0x00080000
 
#define ADC_MEM20   0x00100000
 
#define ADC_MEM21   0x00200000
 
#define ADC_MEM22   0x00400000
 
#define ADC_MEM23   0x00800000
 
#define ADC_MEM24   0x01000000
 
#define ADC_MEM25   0x02000000
 
#define ADC_MEM26   0x04000000
 
#define ADC_MEM27   0x08000000
 
#define ADC_MEM28   0x10000000
 
#define ADC_MEM29   0x20000000
 
#define ADC_MEM30   0x40000000
 
#define ADC_MEM31   0x80000000
 
#define ADC_VREFPOS_AVCC_VREFNEG_VSS   (ADC14_MCTLN_VRSEL_0)
 
#define ADC_VREFPOS_INTBUF_VREFNEG_VSS   (ADC14_MCTLN_VRSEL_1)
 
#define ADC_VREFPOS_EXTPOS_VREFNEG_EXTNEG   (ADC14_MCTLN_VRSEL_14)
 
#define ADC_VREFPOS_EXTBUF_VREFNEG_EXTNEG   (ADC14_MCTLN_VRSEL_15)
 
#define ADC_INPUT_A0   (ADC14_MCTLN_INCH_0)
 
#define ADC_INPUT_A1   (ADC14_MCTLN_INCH_1)
 
#define ADC_INPUT_A2   (ADC14_MCTLN_INCH_2)
 
#define ADC_INPUT_A3   (ADC14_MCTLN_INCH_3)
 
#define ADC_INPUT_A4   (ADC14_MCTLN_INCH_4)
 
#define ADC_INPUT_A5   (ADC14_MCTLN_INCH_5)
 
#define ADC_INPUT_A6   (ADC14_MCTLN_INCH_6)
 
#define ADC_INPUT_A7   (ADC14_MCTLN_INCH_7)
 
#define ADC_INPUT_A8   (ADC14_MCTLN_INCH_8)
 
#define ADC_INPUT_A9   (ADC14_MCTLN_INCH_9)
 
#define ADC_INPUT_A10   (ADC14_MCTLN_INCH_10)
 
#define ADC_INPUT_A11   (ADC14_MCTLN_INCH_11)
 
#define ADC_INPUT_A12   (ADC14_MCTLN_INCH_12)
 
#define ADC_INPUT_A13   (ADC14_MCTLN_INCH_13)
 
#define ADC_INPUT_A14   (ADC14_MCTLN_INCH_14)
 
#define ADC_INPUT_A15   (ADC14_MCTLN_INCH_15)
 
#define ADC_INPUT_A16   (ADC14_MCTLN_INCH_16)
 
#define ADC_INPUT_A17   (ADC14_MCTLN_INCH_17)
 
#define ADC_INPUT_A18   (ADC14_MCTLN_INCH_18)
 
#define ADC_INPUT_A19   (ADC14_MCTLN_INCH_19)
 
#define ADC_INPUT_A20   (ADC14_MCTLN_INCH_20)
 
#define ADC_INPUT_A21   (ADC14_MCTLN_INCH_21)
 
#define ADC_INPUT_A22   (ADC14_MCTLN_INCH_22)
 
#define ADC_INPUT_A23   (ADC14_MCTLN_INCH_23)
 
#define ADC_INPUT_A24   (ADC14_MCTLN_INCH_24)
 
#define ADC_INPUT_A25   (ADC14_MCTLN_INCH_25)
 
#define ADC_INPUT_A26   (ADC14_MCTLN_INCH_26)
 
#define ADC_INPUT_A27   (ADC14_MCTLN_INCH_27)
 
#define ADC_INPUT_A28   (ADC14_MCTLN_INCH_28)
 
#define ADC_INPUT_A29   (ADC14_MCTLN_INCH_29)
 
#define ADC_INPUT_A30   (ADC14_MCTLN_INCH_30)
 
#define ADC_INPUT_A31   (ADC14_MCTLN_INCH_31)
 
#define ADC_COMP_WINDOW0   0x00
 
#define ADC_COMP_WINDOW1   0x01
 
#define ADC_SIGNED_BINARY   0x00
 
#define ADC_UNSIGNED_BINARY   0x01
 
#define ADC_MANUAL_ITERATION   0x00
 
#define ADC_AUTOMATIC_ITERATION   ADC14_CTL0_MSC
 
#define ADC_UNRESTRICTED_POWER_MODE   ADC14_CTL1_PWRMD_0
 
#define ADC_ULTRA_LOW_POWER_MODE   ADC14_CTL1_PWRMD_2
 
#define ADC_INT0   ADC14_IER0_IE0
 
#define ADC_INT1   ADC14_IER0_IE1
 
#define ADC_INT2   ADC14_IER0_IE2
 
#define ADC_INT3   ADC14_IER0_IE3
 
#define ADC_INT4   ADC14_IER0_IE4
 
#define ADC_INT5   ADC14_IER0_IE5
 
#define ADC_INT6   ADC14_IER0_IE6
 
#define ADC_INT7   ADC14_IER0_IE7
 
#define ADC_INT8   ADC14_IER0_IE8
 
#define ADC_INT9   ADC14_IER0_IE9
 
#define ADC_INT10   ADC14_IER0_IE10
 
#define ADC_INT11   ADC14_IER0_IE11
 
#define ADC_INT12   ADC14_IER0_IE12
 
#define ADC_INT13   ADC14_IER0_IE13
 
#define ADC_INT14   ADC14_IER0_IE14
 
#define ADC_INT15   ADC14_IER0_IE15
 
#define ADC_INT16   ADC14_IER0_IE16
 
#define ADC_INT17   ADC14_IER0_IE17
 
#define ADC_INT18   ADC14_IER0_IE18
 
#define ADC_INT19   ADC14_IER0_IE19
 
#define ADC_INT20   ADC14_IER0_IE20
 
#define ADC_INT21   ADC14_IER0_IE21
 
#define ADC_INT22   ADC14_IER0_IE22
 
#define ADC_INT23   ADC14_IER0_IE23
 
#define ADC_INT24   ADC14_IER0_IE24
 
#define ADC_INT25   ADC14_IER0_IE25
 
#define ADC_INT26   ADC14_IER0_IE26
 
#define ADC_INT27   ADC14_IER0_IE27
 
#define ADC_INT28   ADC14_IER0_IE28
 
#define ADC_INT29   ADC14_IER0_IE29
 
#define ADC_INT30   ADC14_IER0_IE30
 
#define ADC_INT31   ADC14_IER0_IE31
 
#define ADC_IN_INT   0x0000000200000000
 
#define ADC_LO_INT   0x0000000400000000
 
#define ADC_HI_INT   0x0000000800000000
 
#define ADC_OV_INT   0x0000001000000000
 
#define ADC_TOV_INT   0x0000002000000000
 
#define ADC_RDY_INT   0x0000004000000000
 
#define ADC_INVALID_MEM   32
 
#define ADC14_enableModuleMultipleInstance(a)   ADC14_enableModule()
 
#define ADC14_disableModuleMultipleInstance(a)   ADC14_disableModule()
 
#define ADC14_initModuleMultipleInstance(a, b, c, d, e)   ADC14_initModule(b,c,d,e)
 
#define ADC14_setResolutionMultipleInstance(a, b)   ADC14_setResolution(b)
 
#define ADC14_getResolutionMultipleInstance(a)   ADC14_getResolution()
 
#define ADC14_setSampleHoldTriggerMultipleInstance(a, b, c)   ADC14_setSampleHoldTrigger(b,c)
 
#define ADC14_setSampleHoldTimeMultipleInstance(a, b, c)   ADC14_setSampleHoldTime(b,c)
 
#define ADC14_configureMultiSequenceModeMultipleInstance(a, b, c, d)   ADC14_configureMultiSequenceMode(b,c,d)
 
#define ADC14_configureSingleSampleModeMultipleInstance(a, b, c)   ADC14_configureSingleSampleMode(b,c)
 
#define ADC14_enableConversionMultipleInstance(a, b)   ADC14_enableConversion(b)
 
#define ADC14_disableConversionMultipleInstance(a)   ADC14_disableConversion()
 
#define ADC14_toggleConversionTriggerMultipleInstance(a)   ADC14_toggleConversionTrigger()
 
#define ADC14_isBusyMultipleInstance(a)   ADC14_isBusy()
 
#define ADC14_configureConversionMemoryMultipleInstance(a, b, c, d, e)   ADC14_configureConversionMemory(b,c,d,e)
 
#define ADC14_enableComparatorWindowMultipleInstance(a, b, c)   ADC14_enableComparatorWindow(b,c)
 
#define ADC14_disableComparatorWindowMultipleInstance(a, b)   ADC14_disableComparatorWindow(b)
 
#define ADC14_setComparatorWindowValueMultipleInstance(a, b, c, d)   ADC14_setComparatorWindowValue(b,c,d)
 
#define ADC14_setResultFormatMultipleInstance(a, b)   ADC14_setResultFormat(b)
 
#define ADC14_getResultMultipleInstance(a, b)   ADC14_getResult(b)
 
#define ADC14_getMultiSequenceResultMultipleInstance(a, b)   ADC14_getMultiSequenceResult(b)
 
#define ADC14_getResultArrayMultipleInstance(a, b, c, d)   ADC14_getResultArray(b,c,d)
 
#define ADC14_enableReferenceBurstMultipleInstance(a)   ADC14_enableReferenceBurst()
 
#define ADC14_disableReferenceBurstMultipleInstance(a)   ADC14_disableReferenceBurst()
 
#define ADC14_setPowerModeMultipleInstance(a, b)   ADC14_setPowerMode(b)
 
#define ADC14_enableSampleTimerMultipleInstance(a, b)   ADC14_enableSampleTimer(b)
 
#define ADC14_disableSampleTimerMultipleInstance(a)   ADC14_disableSampleTimer()
 
#define ADC14_enableInterruptMultipleInstance(a, b)   ADC14_enableInterrupt(b)
 
#define ADC14_disableInterruptMultipleInstance(a, b)   ADC14_disableInterrupt(b)
 
#define ADC14_getInterruptStatusMultipleInstance(a)   ADC14_getInterruptStatus()
 
#define ADC14_getEnabledInterruptStatusMultipleInstance(a)   ADC14_getEnabledInterruptStatus()
 
#define ADC14_clearInterruptFlagMultipleInstance(a, b)   ADC14_clearInterruptFlag(b)
 
#define ADC14_registerInterruptMultipleInstance(a, b)   ADC14_registerInterrupt(b)
 
#define ADC14_unregisterInterruptMultipleInstance(a)   ADC14_unregisterInterrupt()
 

Functions

void ADC14_enableModule (void)
 
bool ADC14_disableModule (void)
 
bool ADC14_initModule (uint32_t clockSource, uint32_t clockPredivider, uint32_t clockDivider, uint32_t internalChannelMask)
 
void ADC14_setResolution (uint32_t resolution)
 
uint_fast32_t ADC14_getResolution (void)
 
bool ADC14_setSampleHoldTrigger (uint32_t source, bool invertSignal)
 
bool ADC14_setSampleHoldTime (uint32_t firstPulseWidth, uint32_t secondPulseWidth)
 
bool ADC14_configureMultiSequenceMode (uint32_t memoryStart, uint32_t memoryEnd, bool repeatMode)
 
bool ADC14_configureSingleSampleMode (uint32_t memoryDestination, bool repeatMode)
 
bool ADC14_enableConversion (void)
 
void ADC14_disableConversion (void)
 
bool ADC14_toggleConversionTrigger (void)
 
bool ADC14_isBusy (void)
 
bool ADC14_configureConversionMemory (uint32_t memorySelect, uint32_t refSelect, uint32_t channelSelect, bool differntialMode)
 
bool ADC14_enableComparatorWindow (uint32_t memorySelect, uint32_t windowSelect)
 
bool ADC14_disableComparatorWindow (uint32_t memorySelect)
 
bool ADC14_setComparatorWindowValue (uint32_t window, int16_t low, int16_t high)
 
bool ADC14_setResultFormat (uint32_t resultFormat)
 
uint_fast16_t ADC14_getResult (uint32_t memorySelect)
 
void ADC14_getMultiSequenceResult (uint16_t *res)
 
void ADC14_getResultArray (uint32_t memoryStart, uint32_t memoryEnd, uint16_t *res)
 
bool ADC14_enableReferenceBurst (void)
 
bool ADC14_disableReferenceBurst (void)
 
bool ADC14_setPowerMode (uint32_t powerMode)
 
bool ADC14_enableSampleTimer (uint32_t multiSampleConvert)
 
bool ADC14_disableSampleTimer (void)
 
void ADC14_enableInterrupt (uint_fast64_t mask)
 
void ADC14_disableInterrupt (uint_fast64_t mask)
 
uint_fast64_t ADC14_getInterruptStatus (void)
 
uint_fast64_t ADC14_getEnabledInterruptStatus (void)
 
void ADC14_clearInterruptFlag (uint_fast64_t mask)
 
void ADC14_registerInterrupt (void(*intHandler)(void))
 
void ADC14_unregisterInterrupt (void)
 

Detailed Description

Analog to Digital Converter with a maximum of 14-bit resolution.


Module Operation


The ADC14 module for Driver Library is designed to allow the user to make simple analog to digital conversions as well make complex and simultaneous conversions across multiple channels.


Conversion Modes


With Single Conversion Mode, the user will sample only a single ADC channel which will be stored in a single ADC memory location. This is the most basic ADC sample/convert mode and allows for very simple measurements on a single channel. To configure single sample mode, only a single destination is configured for the sample/conversion result. The following is a code snippet for configuring/initializing the ADC module in single conversion mode as well as kicking off the start of conversion/sampling.

When using single sample mode, only one memory location will be written for a conversion/sample cycle. To access the result of this conversion, the ADC14_getResult API is used with the corresponding memory location specified. This is usually done within the interrupt service routine of the ADC module.

The ADC14 APIs also support the setup/configuration of multiple conversion mode. With multiple conversion mode, multiple ADC channels are sampled and stored in multiple ADC memory addresses in a single sweep. This is particularly useful when the user wants to take a sample of multiple channels over a period of time (also known as scan mode). The ADC14_getMultiSequenceResult function is used to populate the given array pointer with the result over a wide memory arrange (setup with ADC14_configureMultiSequenceMode ).


Repeat Modes


When configuring the ADC module to use multiple or single sample/conversion mode, a boolean argument is provided to signal whether the DriverLib ADC module should work in "repeat" mode. With repeat mode, once a conversion/sample is completed and read by the API, a new conversion happens until the user manually stops conversion using the ADC14_toggleConversionTrigger command. Repeat mode is useful when the user wants to continuously sample an ADC channel over an extended period of time.

When repeat mode is specified to be false, whenever a conversion/sample is finished and read from the result register, the module will stop conversion until called by the ADC14_toggleConversionTrigger function.


Conversion of Results


When reading a result of an ADC14 conversion, it is important to note that the result will be relevant to the current resolution of the ADC14 device. For example, say the ADC14 module is setup with a 14-bit resolution and a positive reference of 2.5v (and a negative of 0v). In this case, if the conversion result of 16383 would signify a value of 2.5v (if in unsigned) mode. A snippet of code that converts the conversion result in the ADC register to a real life value can be seen in the following:

It is important to note that when using floating point arithmetic, it is important to enable the devices FPU (if available) to save CPU cycles and energy consumption.


Programming Example


The DriverLib package contains a variety of different code examples that demonstrate the usage of the ADC14 module. These code examples are accessible under the examples/ folder of the SDK release as well as through TI Resource Explorer if using Code Composer Studio. These code examples provide a comprehensive list of use cases as well as practical applications involving each module.

Below is a very brief code example showing how to configure the ADC14 module in single sample mode. For a set of more detailed code examples, please refer to the code examples in the examples/ directory of the SDK release:

Macro Definition Documentation

#define ADC_CLOCKSOURCE_ADCOSC   (ADC14_CTL0_SSEL_0)

Referenced by ADC14_initModule().

#define ADC_CLOCKSOURCE_SYSOSC   (ADC14_CTL0_SSEL_1)

Referenced by ADC14_initModule().

#define ADC_CLOCKSOURCE_ACLK   (ADC14_CTL0_SSEL_2)

Referenced by ADC14_initModule().

#define ADC_CLOCKSOURCE_MCLK   (ADC14_CTL0_SSEL_3)

Referenced by ADC14_initModule().

#define ADC_CLOCKSOURCE_SMCLK   (ADC14_CTL0_SSEL_4)

Referenced by ADC14_initModule().

#define ADC_CLOCKSOURCE_HSMCLK   (ADC14_CTL0_SSEL_5)

Referenced by ADC14_initModule().

#define ADC_PREDIVIDER_1   (ADC14_CTL0_PDIV_0)

Referenced by ADC14_initModule().

#define ADC_PREDIVIDER_4   (ADC14_CTL0_PDIV_1)

Referenced by ADC14_initModule().

#define ADC_PREDIVIDER_32   (ADC14_CTL0_PDIV_2)

Referenced by ADC14_initModule().

#define ADC_PREDIVIDER_64   (ADC14_CTL0_PDIV_3)

Referenced by ADC14_initModule().

#define ADC_DIVIDER_1   (ADC14_CTL0_DIV_0)

Referenced by ADC14_initModule().

#define ADC_DIVIDER_2   (ADC14_CTL0_DIV_1)

Referenced by ADC14_initModule().

#define ADC_DIVIDER_3   (ADC14_CTL0_DIV_2)

Referenced by ADC14_initModule().

#define ADC_DIVIDER_4   (ADC14_CTL0_DIV_3)

Referenced by ADC14_initModule().

#define ADC_DIVIDER_5   (ADC14_CTL0_DIV_4)

Referenced by ADC14_initModule().

#define ADC_DIVIDER_6   (ADC14_CTL0_DIV_5)

Referenced by ADC14_initModule().

#define ADC_DIVIDER_7   (ADC14_CTL0_DIV_6)

Referenced by ADC14_initModule().

#define ADC_DIVIDER_8   (ADC14_CTL0_DIV_7)

Referenced by ADC14_initModule().

#define ADC_MAPINTCH3   (ADC14_CTL1_CH3MAP)

Referenced by ADC14_initModule().

#define ADC_MAPINTCH2   (ADC14_CTL1_CH2MAP)

Referenced by ADC14_initModule().

#define ADC_MAPINTCH1   (ADC14_CTL1_CH1MAP)

Referenced by ADC14_initModule().

#define ADC_MAPINTCH0   (ADC14_CTL1_CH0MAP)

Referenced by ADC14_initModule().

#define ADC_TEMPSENSEMAP   (ADC14_CTL1_TCMAP)

Referenced by ADC14_initModule().

#define ADC_BATTMAP   (ADC14_CTL1_BATMAP)

Referenced by ADC14_initModule().

#define ADC_NOROUTE   0
#define ADC_8BIT   ADC14_CTL1_RES_0

Referenced by ADC14_setResolution().

#define ADC_10BIT   ADC14_CTL1_RES_1

Referenced by ADC14_setResolution().

#define ADC_12BIT   ADC14_CTL1_RES_2

Referenced by ADC14_setResolution().

#define ADC_14BIT   ADC14_CTL1_RES_3

Referenced by ADC14_setResolution().

#define ADC_TRIGGER_ADCSC   ADC14_CTL0_SHS_0
#define ADC_TRIGGER_SOURCE1   ADC14_CTL0_SHS_1
#define ADC_TRIGGER_SOURCE2   ADC14_CTL0_SHS_2
#define ADC_TRIGGER_SOURCE3   ADC14_CTL0_SHS_3
#define ADC_TRIGGER_SOURCE4   ADC14_CTL0_SHS_4
#define ADC_TRIGGER_SOURCE5   ADC14_CTL0_SHS_5
#define ADC_TRIGGER_SOURCE6   ADC14_CTL0_SHS_6
#define ADC_TRIGGER_SOURCE7   ADC14_CTL0_SHS_7
#define ADC_PULSE_WIDTH_4   ADC14_CTL0_SHT1_0

Referenced by ADC14_setSampleHoldTime().

#define ADC_PULSE_WIDTH_8   ADC14_CTL0_SHT1_1

Referenced by ADC14_setSampleHoldTime().

#define ADC_PULSE_WIDTH_16   ADC14_CTL0_SHT1_2

Referenced by ADC14_setSampleHoldTime().

#define ADC_PULSE_WIDTH_32   ADC14_CTL0_SHT1_3

Referenced by ADC14_setSampleHoldTime().

#define ADC_PULSE_WIDTH_64   ADC14_CTL0_SHT1_4

Referenced by ADC14_setSampleHoldTime().

#define ADC_PULSE_WIDTH_96   ADC14_CTL0_SHT1_5

Referenced by ADC14_setSampleHoldTime().

#define ADC_PULSE_WIDTH_128   ADC14_CTL0_SHT1_6

Referenced by ADC14_setSampleHoldTime().

#define ADC_PULSE_WIDTH_192   ADC14_CTL0_SHT1_7

Referenced by ADC14_setSampleHoldTime().

#define ADC_NONDIFFERENTIAL_INPUTS   false
#define ADC_DIFFERENTIAL_INPUTS   true
#define ADC_MEM0   0x00000001
#define ADC_MEM1   0x00000002
#define ADC_MEM2   0x00000004
#define ADC_MEM3   0x00000008
#define ADC_MEM4   0x00000010
#define ADC_MEM5   0x00000020
#define ADC_MEM6   0x00000040
#define ADC_MEM7   0x00000080
#define ADC_MEM8   0x00000100
#define ADC_MEM9   0x00000200
#define ADC_MEM10   0x00000400
#define ADC_MEM11   0x00000800
#define ADC_MEM12   0x00001000
#define ADC_MEM13   0x00002000
#define ADC_MEM14   0x00004000
#define ADC_MEM15   0x00008000
#define ADC_MEM16   0x00010000
#define ADC_MEM17   0x00020000
#define ADC_MEM18   0x00040000
#define ADC_MEM19   0x00080000
#define ADC_MEM20   0x00100000
#define ADC_MEM21   0x00200000
#define ADC_MEM22   0x00400000
#define ADC_MEM23   0x00800000
#define ADC_MEM24   0x01000000
#define ADC_MEM25   0x02000000
#define ADC_MEM26   0x04000000
#define ADC_MEM27   0x08000000
#define ADC_MEM28   0x10000000
#define ADC_MEM29   0x20000000
#define ADC_MEM30   0x40000000
#define ADC_MEM31   0x80000000
#define ADC_VREFPOS_AVCC_VREFNEG_VSS   (ADC14_MCTLN_VRSEL_0)
#define ADC_VREFPOS_INTBUF_VREFNEG_VSS   (ADC14_MCTLN_VRSEL_1)
#define ADC_VREFPOS_EXTPOS_VREFNEG_EXTNEG   (ADC14_MCTLN_VRSEL_14)
#define ADC_VREFPOS_EXTBUF_VREFNEG_EXTNEG   (ADC14_MCTLN_VRSEL_15)
#define ADC_INPUT_A0   (ADC14_MCTLN_INCH_0)
#define ADC_INPUT_A1   (ADC14_MCTLN_INCH_1)
#define ADC_INPUT_A2   (ADC14_MCTLN_INCH_2)
#define ADC_INPUT_A3   (ADC14_MCTLN_INCH_3)
#define ADC_INPUT_A4   (ADC14_MCTLN_INCH_4)
#define ADC_INPUT_A5   (ADC14_MCTLN_INCH_5)
#define ADC_INPUT_A6   (ADC14_MCTLN_INCH_6)
#define ADC_INPUT_A7   (ADC14_MCTLN_INCH_7)
#define ADC_INPUT_A8   (ADC14_MCTLN_INCH_8)
#define ADC_INPUT_A9   (ADC14_MCTLN_INCH_9)
#define ADC_INPUT_A10   (ADC14_MCTLN_INCH_10)
#define ADC_INPUT_A11   (ADC14_MCTLN_INCH_11)
#define ADC_INPUT_A12   (ADC14_MCTLN_INCH_12)
#define ADC_INPUT_A13   (ADC14_MCTLN_INCH_13)
#define ADC_INPUT_A14   (ADC14_MCTLN_INCH_14)
#define ADC_INPUT_A15   (ADC14_MCTLN_INCH_15)
#define ADC_INPUT_A16   (ADC14_MCTLN_INCH_16)
#define ADC_INPUT_A17   (ADC14_MCTLN_INCH_17)
#define ADC_INPUT_A18   (ADC14_MCTLN_INCH_18)
#define ADC_INPUT_A19   (ADC14_MCTLN_INCH_19)
#define ADC_INPUT_A20   (ADC14_MCTLN_INCH_20)
#define ADC_INPUT_A21   (ADC14_MCTLN_INCH_21)
#define ADC_INPUT_A22   (ADC14_MCTLN_INCH_22)
#define ADC_INPUT_A23   (ADC14_MCTLN_INCH_23)
#define ADC_INPUT_A24   (ADC14_MCTLN_INCH_24)
#define ADC_INPUT_A25   (ADC14_MCTLN_INCH_25)
#define ADC_INPUT_A26   (ADC14_MCTLN_INCH_26)
#define ADC_INPUT_A27   (ADC14_MCTLN_INCH_27)
#define ADC_INPUT_A28   (ADC14_MCTLN_INCH_28)
#define ADC_INPUT_A29   (ADC14_MCTLN_INCH_29)
#define ADC_INPUT_A30   (ADC14_MCTLN_INCH_30)
#define ADC_INPUT_A31   (ADC14_MCTLN_INCH_31)
#define ADC_COMP_WINDOW0   0x00
#define ADC_COMP_WINDOW1   0x01
#define ADC_SIGNED_BINARY   0x00

Referenced by ADC14_setResultFormat().

#define ADC_UNSIGNED_BINARY   0x01

Referenced by ADC14_setResultFormat().

#define ADC_MANUAL_ITERATION   0x00

Referenced by ADC14_enableSampleTimer().

#define ADC_AUTOMATIC_ITERATION   ADC14_CTL0_MSC
#define ADC_UNRESTRICTED_POWER_MODE   ADC14_CTL1_PWRMD_0

Referenced by ADC14_setPowerMode().

#define ADC_ULTRA_LOW_POWER_MODE   ADC14_CTL1_PWRMD_2

Referenced by ADC14_setPowerMode().

#define ADC_INT0   ADC14_IER0_IE0
#define ADC_INT1   ADC14_IER0_IE1
#define ADC_INT2   ADC14_IER0_IE2
#define ADC_INT3   ADC14_IER0_IE3
#define ADC_INT4   ADC14_IER0_IE4
#define ADC_INT5   ADC14_IER0_IE5
#define ADC_INT6   ADC14_IER0_IE6
#define ADC_INT7   ADC14_IER0_IE7
#define ADC_INT8   ADC14_IER0_IE8
#define ADC_INT9   ADC14_IER0_IE9
#define ADC_INT10   ADC14_IER0_IE10
#define ADC_INT11   ADC14_IER0_IE11
#define ADC_INT12   ADC14_IER0_IE12
#define ADC_INT13   ADC14_IER0_IE13
#define ADC_INT14   ADC14_IER0_IE14
#define ADC_INT15   ADC14_IER0_IE15
#define ADC_INT16   ADC14_IER0_IE16
#define ADC_INT17   ADC14_IER0_IE17
#define ADC_INT18   ADC14_IER0_IE18
#define ADC_INT19   ADC14_IER0_IE19
#define ADC_INT20   ADC14_IER0_IE20
#define ADC_INT21   ADC14_IER0_IE21
#define ADC_INT22   ADC14_IER0_IE22
#define ADC_INT23   ADC14_IER0_IE23
#define ADC_INT24   ADC14_IER0_IE24
#define ADC_INT25   ADC14_IER0_IE25
#define ADC_INT26   ADC14_IER0_IE26
#define ADC_INT27   ADC14_IER0_IE27
#define ADC_INT28   ADC14_IER0_IE28
#define ADC_INT29   ADC14_IER0_IE29
#define ADC_INT30   ADC14_IER0_IE30
#define ADC_INT31   ADC14_IER0_IE31
#define ADC_IN_INT   0x0000000200000000
#define ADC_LO_INT   0x0000000400000000
#define ADC_HI_INT   0x0000000800000000
#define ADC_OV_INT   0x0000001000000000
#define ADC_TOV_INT   0x0000002000000000
#define ADC_RDY_INT   0x0000004000000000
#define ADC_INVALID_MEM   32
#define ADC14_enableModuleMultipleInstance (   a)    ADC14_enableModule()
#define ADC14_disableModuleMultipleInstance (   a)    ADC14_disableModule()
#define ADC14_initModuleMultipleInstance (   a,
  b,
  c,
  d,
 
)    ADC14_initModule(b,c,d,e)
#define ADC14_setResolutionMultipleInstance (   a,
 
)    ADC14_setResolution(b)
#define ADC14_getResolutionMultipleInstance (   a)    ADC14_getResolution()
#define ADC14_setSampleHoldTriggerMultipleInstance (   a,
  b,
 
)    ADC14_setSampleHoldTrigger(b,c)
#define ADC14_setSampleHoldTimeMultipleInstance (   a,
  b,
 
)    ADC14_setSampleHoldTime(b,c)
#define ADC14_configureMultiSequenceModeMultipleInstance (   a,
  b,
  c,
 
)    ADC14_configureMultiSequenceMode(b,c,d)
#define ADC14_configureSingleSampleModeMultipleInstance (   a,
  b,
 
)    ADC14_configureSingleSampleMode(b,c)
#define ADC14_enableConversionMultipleInstance (   a,
 
)    ADC14_enableConversion(b)
#define ADC14_disableConversionMultipleInstance (   a)    ADC14_disableConversion()
#define ADC14_toggleConversionTriggerMultipleInstance (   a)    ADC14_toggleConversionTrigger()
#define ADC14_isBusyMultipleInstance (   a)    ADC14_isBusy()
#define ADC14_configureConversionMemoryMultipleInstance (   a,
  b,
  c,
  d,
 
)    ADC14_configureConversionMemory(b,c,d,e)
#define ADC14_enableComparatorWindowMultipleInstance (   a,
  b,
 
)    ADC14_enableComparatorWindow(b,c)
#define ADC14_disableComparatorWindowMultipleInstance (   a,
 
)    ADC14_disableComparatorWindow(b)
#define ADC14_setComparatorWindowValueMultipleInstance (   a,
  b,
  c,
 
)    ADC14_setComparatorWindowValue(b,c,d)
#define ADC14_setResultFormatMultipleInstance (   a,
 
)    ADC14_setResultFormat(b)
#define ADC14_getResultMultipleInstance (   a,
 
)    ADC14_getResult(b)
#define ADC14_getMultiSequenceResultMultipleInstance (   a,
 
)    ADC14_getMultiSequenceResult(b)
#define ADC14_getResultArrayMultipleInstance (   a,
  b,
  c,
 
)    ADC14_getResultArray(b,c,d)
#define ADC14_enableReferenceBurstMultipleInstance (   a)    ADC14_enableReferenceBurst()
#define ADC14_disableReferenceBurstMultipleInstance (   a)    ADC14_disableReferenceBurst()
#define ADC14_setPowerModeMultipleInstance (   a,
 
)    ADC14_setPowerMode(b)
#define ADC14_enableSampleTimerMultipleInstance (   a,
 
)    ADC14_enableSampleTimer(b)
#define ADC14_disableSampleTimerMultipleInstance (   a)    ADC14_disableSampleTimer()
#define ADC14_enableInterruptMultipleInstance (   a,
 
)    ADC14_enableInterrupt(b)
#define ADC14_disableInterruptMultipleInstance (   a,
 
)    ADC14_disableInterrupt(b)
#define ADC14_getInterruptStatusMultipleInstance (   a)    ADC14_getInterruptStatus()
#define ADC14_getEnabledInterruptStatusMultipleInstance (   a)    ADC14_getEnabledInterruptStatus()
#define ADC14_clearInterruptFlagMultipleInstance (   a,
 
)    ADC14_clearInterruptFlag(b)
#define ADC14_registerInterruptMultipleInstance (   a,
 
)    ADC14_registerInterrupt(b)
#define ADC14_unregisterInterruptMultipleInstance (   a)    ADC14_unregisterInterrupt()

Function Documentation

void ADC14_enableModule ( void  )

Enables the ADC block.

This will enable operation of the ADC block.

Returns
none.
bool ADC14_disableModule ( void  )

Disables the ADC block.

This will disable operation of the ADC block.

Returns
false if user is trying to disable during active conversion
bool ADC14_initModule ( uint32_t  clockSource,
uint32_t  clockPredivider,
uint32_t  clockDivider,
uint32_t  internalChannelMask 
)

Initializes the ADC module and sets up the clock system divider/pre-divider. This initialization function will also configure the internal/external signal mapping.

Note
A call to this function while active ADC conversion is happening is an invalid case and will result in a false value being returned.
Parameters
clockSourceThe clock source to use for the ADC module.
  • ADC_CLOCKSOURCE_ADCOSC [DEFAULT]
  • ADC_CLOCKSOURCE_SYSOSC
  • ADC_CLOCKSOURCE_ACLK
  • ADC_CLOCKSOURCE_MCLK
  • ADC_CLOCKSOURCE_SMCLK
  • ADC_CLOCKSOURCE_HSMCLK
clockPredividerDivides the given clock source before feeding it into the main clock divider. Valid values are:
  • ADC_PREDIVIDER_1 [DEFAULT]
  • ADC_PREDIVIDER_4
  • ADC_PREDIVIDER_32
  • ADC_PREDIVIDER_64
clockDividerDivides the pre-divided clock source Valid values are
  • ADC_DIVIDER_1 [Default value]
  • ADC_DIVIDER_2
  • ADC_DIVIDER_3
  • ADC_DIVIDER_4
  • ADC_DIVIDER_5
  • ADC_DIVIDER_6
  • ADC_DIVIDER_7
  • ADC_DIVIDER_8
internalChannelMaskConfigures the internal/external pin mappings for the ADC modules. This setting determines if the given ADC channel or component is mapped to an external pin (default), or routed to an internal component. This parameter is a bit mask where a logical high value will switch the component to the internal routing. For a list of internal routings, please refer to the device specific data sheet. Valid values are a logical OR of the following values:
  • ADC_MAPINTCH3
  • ADC_MAPINTCH2
  • ADC_MAPINTCH1
  • ADC_MAPINTCH0
  • ADC_TEMPSENSEMAP
  • ADC_BATTMAP

  • ADC_NOROUTE If internalChannelMask is not desired, pass ADC_NOROUTE in lieu of this parameter.
Returns
false if the initialization fails due to an in progress conversion

References ADC_BATTMAP, ADC_CLOCKSOURCE_ACLK, ADC_CLOCKSOURCE_ADCOSC, ADC_CLOCKSOURCE_HSMCLK, ADC_CLOCKSOURCE_MCLK, ADC_CLOCKSOURCE_SMCLK, ADC_CLOCKSOURCE_SYSOSC, ADC_DIVIDER_1, ADC_DIVIDER_2, ADC_DIVIDER_3, ADC_DIVIDER_4, ADC_DIVIDER_5, ADC_DIVIDER_6, ADC_DIVIDER_7, ADC_DIVIDER_8, ADC_MAPINTCH0, ADC_MAPINTCH1, ADC_MAPINTCH2, ADC_MAPINTCH3, ADC_PREDIVIDER_1, ADC_PREDIVIDER_32, ADC_PREDIVIDER_4, ADC_PREDIVIDER_64, ADC_TEMPSENSEMAP, and ASSERT.

void ADC14_setResolution ( uint32_t  resolution)

Sets the resolution of the ADC module. The default resolution is 12-bit, however for power consumption concerns this can be limited to a lower resolution

Parameters
resolutionResolution of the ADC module
  • ADC_8BIT (10 clock cycle conversion time)
  • ADC_10BIT (12 clock cycle conversion time)
  • ADC_12BIT (14 clock cycle conversion time)
  • ADC_14BIT (16 clock cycle conversion time)[DEFAULT]
Returns
none

References ADC_10BIT, ADC_12BIT, ADC_14BIT, ADC_8BIT, and ASSERT.

uint_fast32_t ADC14_getResolution ( void  )

Gets the resolution of the ADC module.

Returns
Resolution of the ADC module
  • ADC_8BIT (10 clock cycle conversion time)
  • ADC_10BIT (12 clock cycle conversion time)
  • ADC_12BIT (14 clock cycle conversion time)
  • ADC_14BIT (16 clock cycle conversion time)
bool ADC14_setSampleHoldTrigger ( uint32_t  source,
bool  invertSignal 
)

Sets the source for the trigger of the ADC module. By default, this value is configured to a software source (the ADCSC bit), however depending on the specific device the trigger can be set to different sources (for example, a timer output). These sources vary from part to part and the user should refer to the device specific datasheet.

Parameters
sourceTrigger source for sampling. Possible values include:
  • ADC_TRIGGER_ADCSC [DEFAULT]
  • ADC_TRIGGER_SOURCE1
  • ADC_TRIGGER_SOURCE2
  • ADC_TRIGGER_SOURCE3
  • ADC_TRIGGER_SOURCE4
  • ADC_TRIGGER_SOURCE5
  • ADC_TRIGGER_SOURCE6
  • ADC_TRIGGER_SOURCE7
invertSignalWhen set to true, will invert the trigger signal to a falling edge. When false, will use a rising edge.
Returns
false if setting fails due to an in progress conversion

References ADC_TRIGGER_ADCSC, ADC_TRIGGER_SOURCE1, ADC_TRIGGER_SOURCE2, ADC_TRIGGER_SOURCE3, ADC_TRIGGER_SOURCE4, ADC_TRIGGER_SOURCE5, ADC_TRIGGER_SOURCE6, ADC_TRIGGER_SOURCE7, and ASSERT.

bool ADC14_setSampleHoldTime ( uint32_t  firstPulseWidth,
uint32_t  secondPulseWidth 
)

Sets the sample/hold time for the specified memory register range. The duration of time required for a sample differs depending on the user's hardware configuration.

There are two values in the ADCC module. The first value controls ADC memory locations ADC_MEMORY_0 through ADC_MEMORY_7 and ADC_MEMORY_24 through ADC_MEMORY_31, while the second value controls memory locations ADC_MEMORY_8 through ADC_MEMORY_23.

Parameters
firstPulseWidthPulse width of the first pulse in ADCCLK cycles Possible values must be one of the following:
  • ADC_PULSE_WIDTH_4 [DEFAULT]
  • ADC_PULSE_WIDTH_8
  • ADC_PULSE_WIDTH_16
  • ADC_PULSE_WIDTH_32
  • ADC_PULSE_WIDTH_64
  • ADC_PULSE_WIDTH_96
  • ADC_PULSE_WIDTH_128
  • ADC_PULSE_WIDTH_192
secondPulseWidthPulse width of the second pulse in ADCCLK cycles. Possible values must be one of the following:
  • ADC_PULSE_WIDTH_4 [DEFAULT]
  • ADC_PULSE_WIDTH_8
  • ADC_PULSE_WIDTH_16
  • ADC_PULSE_WIDTH_32
  • ADC_PULSE_WIDTH_64
  • ADC_PULSE_WIDTH_96
  • ADC_PULSE_WIDTH_128
  • ADC_PULSE_WIDTH_192
Returns
false if setting fails due to an in progress conversion

References ADC_PULSE_WIDTH_128, ADC_PULSE_WIDTH_16, ADC_PULSE_WIDTH_192, ADC_PULSE_WIDTH_32, ADC_PULSE_WIDTH_4, ADC_PULSE_WIDTH_64, ADC_PULSE_WIDTH_8, ADC_PULSE_WIDTH_96, and ASSERT.

bool ADC14_configureMultiSequenceMode ( uint32_t  memoryStart,
uint32_t  memoryEnd,
bool  repeatMode 
)

Configures the ADC module to use a multiple memory sample scheme. This means that multiple samples will consecutively take place and be stored in multiple memory locations. The first sample/conversion will be placed in memoryStart, while the last sample will be stored in memoryEnd. Each memory location should be configured individually using the ADC14_configureConversionMemory function.

The ADC module can be started in "repeat" mode which will cause the ADC module to resume sampling once the initial sample/conversion set is executed. For multi-sample mode, this means that the sampling of the entire memory provided.

Parameters
memoryStartMemory location to store first sample/conversion value. Possible values include:
  • ADC_MEM0 through ADC_MEM31
memoryEndMemory location to store last sample. Possible values include:
  • ADC_MEM0 through ADC_MEM31
repeatModeSpecifies whether or not to repeat the conversion/sample cycle after the first round of sample/conversions. Valid values are true or false.
Returns
false if setting fails due to an in progress conversion

References ADC_INVALID_MEM, and ASSERT.

bool ADC14_configureSingleSampleMode ( uint32_t  memoryDestination,
bool  repeatMode 
)

Configures the ADC module to use a a single ADC memory location for sampling/conversion. This is used when only one channel might be needed for conversion, or where using a multiple sampling scheme is not important.

The ADC module can be started in "repeat" mode which will cause the ADC module to resume sampling once the initial sample/conversion set is executed. In single sample mode, this will cause the ADC module to continuously sample into the memory destination provided.

Parameters
memoryDestinationMemory location to store sample/conversion value. Possible values include:
  • ADC_MEM0 through ADC_MEM31
repeatModeSpecifies whether or not to repeat the conversion/sample cycle after the first round of sample/conversions
Returns
false if setting fails due to an in progress conversion

References ASSERT.

bool ADC14_enableConversion ( void  )

Enables conversion of ADC data. Note that this only enables conversion. To trigger the conversion, you will have to call the ADC14_toggleConversionTrigger or use the source trigger configured in ADC14_setSampleHoldTrigger.

Returns
false if setting fails due to an in progress conversion
void ADC14_disableConversion ( void  )

Halts conversion conversion of the ADC module. Note that the software bit for triggering conversions will also be cleared with this function.

If multi-sequence conversion mode was enabled, the position of the last completed conversion can be retrieved using ADCLastConversionMemoryGet

Returns
none
bool ADC14_toggleConversionTrigger ( void  )

Toggles the trigger for conversion of the ADC module by toggling the trigger software bit. Note that this will cause the ADC to start conversion regardless if the software bit was set as the trigger using ADC14_setSampleHoldTrigger.

Returns
false if setting fails due to an in progress conversion
bool ADC14_isBusy ( void  )

Returns a boolean value that tells if a conversion/sample is in progress

Returns
true if conversion is active, false otherwise
bool ADC14_configureConversionMemory ( uint32_t  memorySelect,
uint32_t  refSelect,
uint32_t  channelSelect,
bool  differntialMode 
)

Configures an individual memory location for the ADC module.

Parameters
memorySelectis the individual ADC memory location to configure. If multiple memory locations want to be configured with the same configuration, this value can be logically ORed together with other values.
  • ADC_MEM0 through ADC_MEM31
refSelectis the voltage reference to use for the selected memory spot. Possible values include:
  • ADC_VREFPOS_AVCC_VREFNEG_VSS [DEFAULT]
  • ADC_VREFPOS_INTBUF_VREFNEG_VSS
  • ADC_VREFPOS_EXTPOS_VREFNEG_EXTNEG
  • ADC_VREFPOS_EXTBUF_VREFNEG_EXTNEG
channelSelectselects the channel to be used for ADC sampling. Note if differential mode is enabled, the value sampled will be equal to the difference between the corresponding even/odd memory locations. Possible values are:
  • ADC_INPUT_A0 through ADC_INPUT_A31
differntialModeselects if the channel selected by the channelSelect will be configured in differential mode. If this parameter is given as true, the configured channel will be paired with its neighbor in differential mode. for example, if channel A0 or A1 is selected, the channel configured will be the difference between A0 and A1. If A2 or A3 are selected, the channel configured will be the difference between A2 and A3 (and so on). Users can enter true or false, or one of the following values:
  • ADC_NONDIFFERENTIAL_INPUTS
  • ADC_DIFFERENTIAL_INPUTS
Returns
false if setting fails due to an in progress conversion

References ADC_INVALID_MEM.

bool ADC14_enableComparatorWindow ( uint32_t  memorySelect,
uint32_t  windowSelect 
)

Enables the specified mask of memory channels to use the specified comparator window. THe ADCC module has two different comparator windows that can be set with this function.

Parameters
memorySelectis the mask of memory locations to enable the comparator window for. This can be a bitwise OR of the following values:
  • ADC_MEM0 through ADC_MEM31
windowSelectMemory location to store sample/conversion value. Possible values include: ADCOMP_WINDOW0 [DEFAULT] ADCOMP_WINDOW1
Returns
false if setting fails due to an in progress conversion

References ADC_COMP_WINDOW0, ADC_COMP_WINDOW1, and ADC_INVALID_MEM.

bool ADC14_disableComparatorWindow ( uint32_t  memorySelect)

Disables the comparator window on the specified memory channels

Parameters
memorySelectis the mask of memory locations to disable the comparator window for. This can be a bitwise OR of the following values:
  • ADC_MEM0 through ADC_MEM31
Returns
false if setting fails due to an in progress conversion
bool ADC14_setComparatorWindowValue ( uint32_t  window,
int16_t  low,
int16_t  high 
)

Sets the lower and upper limits of the specified window comparator. Note that this function will truncate values based of the resolution/data format configured. If the ADC is operating in 10-bit mode, and a 12-bit value is passed into this function the most significant 2 bits will be truncated.

The parameters provided to this function for the upper and lower threshold depend on the current resolution for the ADC. For example, if configured in 12-bit mode, a 12-bit resolution is the maximum that can be provided for the window. If in 2's complement mode, Bit 15 is used as the MSB.

Parameters
windowMemory location to store sample/conversion value. Possible values include: ADC_COMP_WINDOW0 [DEFAULT] ADC_COMP_WINDOW1
lowis the lower limit of the window comparator
highis the upper limit of the window comparator
Returns
false if setting fails due to an in progress conversion

References ADC_COMP_WINDOW0, ADC_COMP_WINDOW1, and ASSERT.

bool ADC14_setResultFormat ( uint32_t  resultFormat)

Switches between a binary unsigned data format and a signed 2's complement data format.

Parameters
resultFormatFormat for result to conversion results. Possible values include: ADC_UNSIGNED_BINARY [DEFAULT] ADC_SIGNED_BINARY
Returns
false if setting fails due to an in progress conversion

References ADC_SIGNED_BINARY, ADC_UNSIGNED_BINARY, and ASSERT.

uint_fast16_t ADC14_getResult ( uint32_t  memorySelect)

Returns the conversion result for the specified memory channel in the format assigned by the ADC14_setResultFormat (unsigned binary by default) function.

Parameters
memorySelectis the memory location to get the conversion result. Valid values are:
  • ADC_MEM0 through ADC_MEM31
Returns
conversion result of specified memory channel

References ADC_INVALID_MEM.

void ADC14_getMultiSequenceResult ( uint16_t *  res)

Returns the conversion results of the currently configured multi-sequence conversion. If a multi-sequence conversion has not happened, this value is unreliable. Note that it is up to the user to verify the integrity of and proper size of the array being passed. If there are 16 multi-sequence results, and an array with only 4 elements allocated is passed, invalid memory settings will occur

Parameters
resconversion result of the last multi-sequence sample in an array of unsigned 16-bit integers
Returns
None
void ADC14_getResultArray ( uint32_t  memoryStart,
uint32_t  memoryEnd,
uint16_t *  res 
)

Returns the conversion results of the specified ADC memory locations. Note that it is up to the user to verify the integrity of and proper size of the array being passed. If there are 16 multi-sequence results, and an array with only 4 elements allocated is passed, invalid memory settings will occur. This function is inclusive.

Parameters
memoryStartis the memory location to get the conversion result. Valid values are:
  • ADC_MEM0 through ADC_MEM31
memoryEndis the memory location to get the conversion result. Valid values are:
  • ADC_MEM0 through ADC_MEM31
resconversion result of the last multi-sequence sample in an array of unsigned 16-bit integers
Returns
None

References ADC_INVALID_MEM, and ASSERT.

bool ADC14_enableReferenceBurst ( void  )

Enables the "on-demand" activity of the voltage reference register. If this setting is enabled, the internal voltage reference buffer will only be updated during a sample or conversion cycle. This is used to optimize power consumption.

Returns
false if setting fails due to an in progress conversion
bool ADC14_disableReferenceBurst ( void  )

Disables the "on-demand" activity of the voltage reference register.

Returns
false if setting fails due to an in progress conversion
bool ADC14_setPowerMode ( uint32_t  powerMode)

Sets the power mode of the ADC module. A more aggressive power mode will restrict the number of samples per second for sampling while optimizing power consumption. Ideally, if power consumption is a concern, this value should be set to the most restrictive setting that satisfies your sampling requirement.

Parameters
adcPowerModeis the power mode to set. Valid values are:
  • ADC_UNRESTRICTED_POWER_MODE (no restriction)
  • ADC_LOW_POWER_MODE (500ksps restriction)
  • ADC_ULTRA_LOW_POWER_MODE (200ksps restriction)
  • ADC_EXTREME_LOW_POWER_MODE (50ksps restriction)
Returns
false if setting fails due to an in progress conversion

References ADC_ULTRA_LOW_POWER_MODE, ADC_UNRESTRICTED_POWER_MODE, and ASSERT.

bool ADC14_enableSampleTimer ( uint32_t  multiSampleConvert)

Enables SAMPCON to be sourced from the sampling timer and to configures multi sample and conversion mode.

Parameters
multiSampleConvert- Switches between manual and automatic iteration when using the sample timer. Valid values are:
  • ADC_MANUAL_ITERATION The user will have to manually set the SHI signal ( usually by ADC14_toggleConversionTrigger ) at the end of each sample/conversion cycle.
  • ADC_AUTOMATIC_ITERATION After one sample/convert is finished, the ADC module will automatically continue on to the next sample
Returns
false if the initialization fails due to an in progress conversion

References ADC_MANUAL_ITERATION.

bool ADC14_disableSampleTimer ( void  )

Disables SAMPCON from being sourced from the sample timer.

Returns
false if the initialization fails due to an in progress conversion
void ADC14_enableInterrupt ( uint_fast64_t  mask)

Enables the indicated ADCC interrupt sources. The ADC_INT0 through ADC_INT31 parameters correspond to a completion event of the corresponding memory location. For example, when the ADC_MEM0 location finishes a conversion cycle, the ADC_INT0 interrupt will be set.

Parameters
maskis the bit mask of interrupts to enable. Valid values are a bitwise OR of the following values:
  • ADC_INT0 through ADC_INT31
  • ADC_IN_INT - Interrupt enable for a conversion in the result register is either greater than the ADCLO or lower than the ADCHI threshold.
  • ADC_LO_INT - Interrupt enable for the falling short of the lower limit interrupt of the window comparator for the result register.
  • ADC_HI_INT - Interrupt enable for the exceeding the upper limit of the window comparator for the result register.
  • ADC_OV_INT - Interrupt enable for a conversion that is about to save to a memory buffer that has not been read out yet.
  • ADC_TOV_INT -Interrupt enable for a conversion that is about to start before the previous conversion has been completed.
  • ADC_RDY_INT -Interrupt enable for the local buffered reference ready signal.
Returns
NONE
void ADC14_disableInterrupt ( uint_fast64_t  mask)

Disables the indicated ADCC interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor. The ADC_INT0 through ADC_INT31 parameters correspond to a completion event of the corresponding memory location. For example, when the ADC_MEM0 location finishes a conversion cycle, the ADC_INT0 interrupt will be set.

Parameters
maskis the bit mask of interrupts to disable. Valid values are a bitwise OR of the following values:
  • ADC_INT0 through ADC_INT31
  • ADC_IN_INT - Interrupt enable for a conversion in the result register is either greater than the ADCLO or lower than the ADCHI threshold.
  • ADC_LO_INT - Interrupt enable for the falling short of the lower limit interrupt of the window comparator for the result register.
  • ADC_HI_INT - Interrupt enable for the exceeding the upper limit of the window comparator for the result register.
  • ADC_OV_INT - Interrupt enable for a conversion that is about to save to a memory buffer that has not been read out yet.
  • ADC_TOV_INT -Interrupt enable for a conversion that is about to start before the previous conversion has been completed.
  • ADC_RDY_INT -Interrupt enable for the local buffered reference ready signal.
Returns
NONE
uint_fast64_t ADC14_getInterruptStatus ( void  )

Returns the status of a the ADC interrupt register. The ADC_INT0 through ADC_INT31 parameters correspond to a completion event of the corresponding memory location. For example, when the ADC_MEM0 location finishes a conversion cycle, the ADC_INT0 interrupt will be set.

Returns
The interrupt status. Value is a bitwise OR of the following values:
  • ADC_INT0 through ADC_INT31
  • ADC_IN_INT - Interrupt enable for a conversion in the result register is either greater than the ADCLO or lower than the ADCHI threshold.
  • ADC_LO_INT - Interrupt enable for the falling short of the lower limit interrupt of the window comparator for the result register.
  • ADC_HI_INT - Interrupt enable for the exceeding the upper limit of the window comparator for the result register.
  • ADC_OV_INT - Interrupt enable for a conversion that is about to save to a memory buffer that has not been read out yet.
  • ADC_TOV_INT -Interrupt enable for a conversion that is about to start before the previous conversion has been completed.
  • ADC_RDY_INT -Interrupt enable for the local buffered reference ready signal.

Referenced by ADC14_getEnabledInterruptStatus().

uint_fast64_t ADC14_getEnabledInterruptStatus ( void  )

Returns the status of a the ADC interrupt register masked with the enabled interrupts. This function is useful to call in ISRs to get a list of pending interrupts that are actually enabled and could have caused the ISR. The ADC_INT0 through ADC_INT31 parameters correspond to a completion event of the corresponding memory location. For example, when the ADC_MEM0 location finishes a conversion cycle, the ADC_INT0

Returns
The interrupt status. Value is a bitwise OR of the following values:
  • ADC_INT0 through ADC_INT31
  • ADC_IN_INT - Interrupt enable for a conversion in the result register is either greater than the ADCLO or lower than the ADCHI threshold.
  • ADC_LO_INT - Interrupt enable for the falling short of the lower limit interrupt of the window comparator for the result register.
  • ADC_HI_INT - Interrupt enable for the exceeding the upper limit of the window comparator for the result register.
  • ADC_OV_INT - Interrupt enable for a conversion that is about to save to a memory buffer that has not been read out yet.
  • ADC_TOV_INT -Interrupt enable for a conversion that is about to start before the previous conversion has been completed.
  • ADC_RDY_INT -Interrupt enable for the local buffered reference ready signal.

References ADC14_getInterruptStatus().

void ADC14_clearInterruptFlag ( uint_fast64_t  mask)

Clears the indicated ADCC interrupt sources.

Parameters
maskis the bit mask of interrupts to clear. The ADC_INT0 through ADC_INT31 parameters correspond to a completion event of the corresponding memory location. For example, when the ADC_MEM0 location finishes a conversion cycle, the ADC_INT0 interrupt will be set. Valid values are a bitwise OR of the following values:
  • ADC_INT0 through ADC_INT31
  • ADC_IN_INT - Interrupt enable for a conversion in the result register is either greater than the ADCLO or lower than the ADCHI threshold.
  • ADC_LO_INT - Interrupt enable for the falling short of the lower limit interrupt of the window comparator for the result register.
  • ADC_HI_INT - Interrupt enable for the exceeding the upper limit of the window comparator for the result register.
  • ADC_OV_INT - Interrupt enable for a conversion that is about to save to a memory buffer that has not been read out yet.
  • ADC_TOV_INT -Interrupt enable for a conversion that is about to start before the previous conversion has been completed.
  • ADC_RDY_INT -Interrupt enable for the local buffered reference ready signal.
Returns
NONE
void ADC14_registerInterrupt ( void(*)(void)  intHandler)

Registers an interrupt handler for the ADC interrupt.

Parameters
intHandleris a pointer to the function to be called when the ADC interrupt occurs.

This function registers the handler to be called when an ADC interrupt occurs. This function enables the global interrupt in the interrupt controller; specific ADC14 interrupts must be enabled via ADC14_enableInterrupt(). It is the interrupt handler's responsibility to clear the interrupt source via ADC14_clearInterruptFlag().

See Also
Interrupt_registerInterrupt() for important information about registering interrupt handlers.
Returns
None.

References INT_ADC14, Interrupt_enableInterrupt(), and Interrupt_registerInterrupt().

void ADC14_unregisterInterrupt ( void  )

Unregisters the interrupt handler for the ADCC module.

This function unregisters the handler to be called when an ADCC interrupt occurs. This function also masks off the interrupt in the interrupt controller so that the interrupt handler no longer is called.

See Also
Interrupt_registerInterrupt() for important information about registering interrupt handlers.
Returns
None.

References INT_ADC14, Interrupt_disableInterrupt(), and Interrupt_unregisterInterrupt().


Copyright 2019, Texas Instruments Incorporated