![]() |
![]() |
The definition of a timer function table that contains the required set of functions to control a specific timer driver implementation. More...
#include <Timer.h>

Data Fields | |
| Timer_CloseFxn | closeFxn |
| Timer_ControlFxn | controlFxn |
| Timer_GetCountFxn | getCountFxn |
| Timer_InitFxn | initFxn |
| Timer_OpenFxn | openFxn |
| Timer_StartFxn | startFxn |
| Timer_StopFxn | stopFxn |
The definition of a timer function table that contains the required set of functions to control a specific timer driver implementation.
| Timer_CloseFxn Timer_FxnTable::closeFxn |
Function to close the specified peripheral.
| Timer_ControlFxn Timer_FxnTable::controlFxn |
Function to implementation specific control function.
| Timer_GetCountFxn Timer_FxnTable::getCountFxn |
Function to get the count of the specified peripheral.
| Timer_InitFxn Timer_FxnTable::initFxn |
Function to initialize the given data object.
| Timer_OpenFxn Timer_FxnTable::openFxn |
Function to open the specified peripheral.
| Timer_StartFxn Timer_FxnTable::startFxn |
Function to start the specified peripheral.
| Timer_StopFxn Timer_FxnTable::stopFxn |
Function to stop the specified peripheral.