SimpleLink Graphics Library  4.11.00.04
Data Structures | Typedefs | Functions | Variables
button.h File Reference
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  Graphics_Button
 This structure defines the characteristics of a Button. More...
 

Typedefs

typedef struct Graphics_Button Graphics_Button
 This structure defines the characteristics of a Button. More...
 

Functions

void Graphics_drawButton (const Graphics_Context *context, const Graphics_Button *button)
 
bool Graphics_isButtonSelected (const Graphics_Button *button, uint16_t x, uint16_t y)
 
void Graphics_drawSelectedButton (const Graphics_Context *context, const Graphics_Button *button)
 
void Graphics_drawReleasedButton (const Graphics_Context *context, const Graphics_Button *button)
 

Variables

Graphics_Context g_sContext
 

Typedef Documentation

§ Graphics_Button

This structure defines the characteristics of a Button.

Variable Documentation

§ g_sContext

Graphics_Context g_sContext
Copyright 2018, Texas Instruments Incorporated