Data Fields
CaptureMSP432_Object_ Struct Reference

CaptureMSP432 Object. More...

#include <CaptureMSP432.h>

Collaboration diagram for CaptureMSP432_Object_:
Collaboration graph
[legend]

Data Fields

HwiP_Handle hwiHandle
 
Capture_CallBackFxn callBack
 
Capture_PeriodUnits periodUnits
 
uint32_t previousCount
 
uint32_t ccrRegister
 
bool isRunning
 

Detailed Description

CaptureMSP432 Object.

The application must not access any member variables of this structure!

Field Documentation

§ hwiHandle

HwiP_Handle CaptureMSP432_Object_::hwiHandle

§ callBack

Capture_CallBackFxn CaptureMSP432_Object_::callBack

§ periodUnits

Capture_PeriodUnits CaptureMSP432_Object_::periodUnits

§ previousCount

uint32_t CaptureMSP432_Object_::previousCount

§ ccrRegister

uint32_t CaptureMSP432_Object_::ccrRegister

§ isRunning

bool CaptureMSP432_Object_::isRunning

The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale