![]() |
![]() |
ADC driver implementation for a MSP432 analog-to-digital converter.
============================================================================
Refer to ADCBuf.h for a complete description of APIs & example of use
#include <stdint.h>
#include <stdbool.h>
#include <ti/devices/DeviceFamily.h>
#include <ti/devices/msp432p4xx/driverlib/sysctl_a.h>
#include <ti/drivers/ADCBuf.h>
#include <ti/drivers/dpl/HwiP.h>
#include <ti/drivers/dpl/SemaphoreP.h>
#include <ti/drivers/Power.h>
#include <ti/drivers/dma/UDMAMSP432.h>
#include <ti/devices/msp432p4xx/driverlib/adc14.h>
Go to the source code of this file.
Data Structures | |
struct | ADCBufMSP432_ParamsExtension |
MSP432 specfic extension to ADCBuf_Params. More... | |
struct | ADCBufMSP432_Channels |
ADCMSP432 Channel setting These fields define channel-specific settings: GPIO and reference voltage. These settings happen when ADCBuf_convert() is called. More... | |
struct | ADCBufMSP432_HWAttrs |
ADCBufMSP432 Hardware attributes These fields are populated by PinMux tool but user is allowed to change for different channels setting. More... | |
struct | ADCBufMSP432_Object |
ADCBufMSP432 Object. More... | |
Macros | |
#define | ADCBufMSP432_CMD_ENTER_ADC_ULTRA_LOW_POWER_MODE ADCBuf_CMD_RESERVED + 1 |
This control function enters ADC in low power mode. More... | |
#define | ADCBufMSP432_CMD_EXIT_ADC_ULTRA_LOW_POWER_MODE ADCBuf_CMD_RESERVED + 2 |
This control function exits ADC from low power mode. More... | |
#define | ADCBufMSP432_P4_0_A13 ((13 << 10) | 0x0340) /* ch 13, port 4, pin 0 */ |
#define | ADCBufMSP432_P4_1_A12 ((12 << 10) | 0x0341) /* ch 12, port 4, pin 1 */ |
#define | ADCBufMSP432_P4_2_A11 ((11 << 10) | 0x0342) /* ch 11, port 4, pin 2 */ |
#define | ADCBufMSP432_P4_3_A10 ((10 << 10) | 0x0343) /* ch 10, port 4, pin 3 */ |
#define | ADCBufMSP432_P4_4_A9 ((9 << 10) | 0x0344) /* ch 9, port 4, pin 4 */ |
#define | ADCBufMSP432_P4_5_A8 ((8 << 10) | 0x0345) /* ch 8, port 4, pin 5 */ |
#define | ADCBufMSP432_P4_6_A7 ((7 << 10) | 0x0346) /* ch 7, port 4, pin 6 */ |
#define | ADCBufMSP432_P4_7_A6 ((6 << 10) | 0x0347) /* ch 6, port 4, pin 7 */ |
#define | ADCBufMSP432_P5_0_A5 ((5 << 10) | 0x0350) /* ch 5, port 5, pin 0 */ |
#define | ADCBufMSP432_P5_1_A4 ((4 << 10) | 0x0351) /* ch 4, port 5, pin 1 */ |
#define | ADCBufMSP432_P5_2_A3 ((3 << 10) | 0x0352) /* ch 3, port 5, pin 2 */ |
#define | ADCBufMSP432_P5_3_A2 ((2 << 10) | 0x0353) /* ch 2, port 5, pin 3 */ |
#define | ADCBufMSP432_P5_4_A1 ((1 << 10) | 0x0354) /* ch 1, port 5, pin 4 */ |
#define | ADCBufMSP432_P5_5_A0 ((0 << 10) | 0x0355) /* ch 0, port 5, pin 5 */ |
#define | ADCBufMSP432_P6_0_A15 ((15 << 10) | 0x0360) /* ch 15, port 6, pin 0 */ |
#define | ADCBufMSP432_P6_1_A14 ((14 << 10) | 0x0361) /* ch 14, port 6, pin 1 */ |
#define | ADCBufMSP432_P8_2_A23 ((23 << 10) | 0x0382) /* ch 23, port 8, pin 2 */ |
#define | ADCBufMSP432_P8_3_A22 ((22 << 10) | 0x0383) /* ch 22, port 8, pin 3 */ |
#define | ADCBufMSP432_P8_4_A21 ((21 << 10) | 0x0384) /* ch 21, port 8, pin 4 */ |
#define | ADCBufMSP432_P8_5_A20 ((20 << 10) | 0x0385) /* ch 20, port 8, pin 5 */ |
#define | ADCBufMSP432_P8_6_A19 ((19 << 10) | 0x0386) /* ch 19, port 8, pin 6 */ |
#define | ADCBufMSP432_P8_7_A18 ((18 << 10) | 0x0387) /* ch 18, port 8, pin 7 */ |
#define | ADCBufMSP432_P9_0_A17 ((17 << 10) | 0x0390) /* ch 17, port 9, pin 0 */ |
#define | ADCBufMSP432_P9_1_A16 ((16 << 10) | 0x0391) /* ch 16, port 9, pin 1 */ |
#define | ADCBufMSP432_PIN_NONE 0 |
#define | ADCBufMSP432_INTERNAL_SOURCE_PIN 0 |
Typedefs | |
typedef enum ADCBufMSP432_ReferenceSource | ADCBufMSP432_ReferenceSource |
ADCMSP432 reference source These fields are used by ADCBufMSP432_HWAttrs to specify the reference voltage for each channel. More... | |
typedef enum ADCBufMSP432_SamplingDuration | ADCBufMSP432_SamplingDuration |
ADCMSP432 sampling duration These fields define the MSP432 ADC sampling duration (sample and hold time) in the pulse width unit. User can specify the differnt sampling duration in the ADCBufMSP432_ParamsExtension when opening the ADC. More... | |
typedef enum ADCBufMSP432_TimerReferenceSource | ADCBufMSP432_TimerReferenceSource |
ADCMSP432 timer trigger source These fields are used by ADCBufMSP432_HWAttrs to specify the Timer Capture for each channel. More... | |
typedef enum ADCBufMSP432_ClockSource | ADCBufMSP432_ClockSource |
ADCMSP432 clock source These fields are used by ADCBufMSP432_HWAttrs to specify the clock source for the ADC module. More... | |
typedef enum ADCBufMSP432_TriggerSource | ADCBufMSP432_TriggerSource |
ADCMSP432 trigger source These fields are used by ADCBufMSP432_HWAttrs to specify the trigger source for the ADC. More... | |
typedef enum ADCBufMSP432_DifferentialMode | ADCBufMSP432_DifferentialMode |
ADCMSP432 Differential Mode These fields are used by ADCBufMSP432_HWAttrs to specify if ADC differential sampling mode is selected. More... | |
typedef enum ADCBufMSP432_InternalSourceMode | ADCBufMSP432_InternalSourceMode |
ADCMSP432 Internal Source Mode These fields are used by ADCBufMSP432_HWAttrs to specify if a internal source mode is selected, i.e. temperature sensore or battery monitor modes. More... | |
typedef struct ADCBufMSP432_ParamsExtension | ADCBufMSP432_ParamsExtension |
MSP432 specfic extension to ADCBuf_Params. More... | |
typedef struct ADCBufMSP432_Channels | ADCBufMSP432_Channels |
ADCMSP432 Channel setting These fields define channel-specific settings: GPIO and reference voltage. These settings happen when ADCBuf_convert() is called. More... | |
typedef struct ADCBufMSP432_HWAttrs | ADCBufMSP432_HWAttrs |
ADCBufMSP432 Hardware attributes These fields are populated by PinMux tool but user is allowed to change for different channels setting. More... | |
typedef struct ADCBufMSP432_Object | ADCBufMSP432_Object |
ADCBufMSP432 Object. More... | |
Enumerations | |
enum | ADCBufMSP432_ReferenceSource { ADCBufMSP432_VREFPOS_AVCC_VREFNEG_VSS = ADC_VREFPOS_AVCC_VREFNEG_VSS, ADCBufMSP432_VREFPOS_INTBUF_VREFNEG_VSS = ADC_VREFPOS_INTBUF_VREFNEG_VSS, ADCBufMSP432_VREFPOS_EXTPOS_VREFNEG_EXTNEG = ADC_VREFPOS_EXTPOS_VREFNEG_EXTNEG, ADCBufMSP432_VREFPOS_EXTBUF_VREFNEG_EXTNEG = ADC_VREFPOS_EXTBUF_VREFNEG_EXTNEG } |
ADCMSP432 reference source These fields are used by ADCBufMSP432_HWAttrs to specify the reference voltage for each channel. More... | |
enum | ADCBufMSP432_SamplingDuration { ADCBufMSP432_SamplingDuration_PULSE_WIDTH_4 = ADC_PULSE_WIDTH_4, ADCBufMSP432_SamplingDuration_PULSE_WIDTH_8 = ADC_PULSE_WIDTH_8, ADCBufMSP432_SamplingDuration_PULSE_WIDTH_16 = ADC_PULSE_WIDTH_16, ADCBufMSP432_SamplingDuration_PULSE_WIDTH_32 = ADC_PULSE_WIDTH_32, ADCBufMSP432_SamplingDuration_PULSE_WIDTH_64 = ADC_PULSE_WIDTH_64, ADCBufMSP432_SamplingDuration_PULSE_WIDTH_96 = ADC_PULSE_WIDTH_96, ADCBufMSP432_SamplingDuration_PULSE_WIDTH_128 = ADC_PULSE_WIDTH_128, ADCBufMSP432_SamplingDuration_PULSE_WIDTH_192 = ADC_PULSE_WIDTH_192 } |
ADCMSP432 sampling duration These fields define the MSP432 ADC sampling duration (sample and hold time) in the pulse width unit. User can specify the differnt sampling duration in the ADCBufMSP432_ParamsExtension when opening the ADC. More... | |
enum | ADCBufMSP432_TimerReferenceSource { ADCBufMSP432_TIMERA0_CAPTURECOMPARE1 = 0, ADCBufMSP432_TIMERA0_CAPTURECOMPARE2 = 1, ADCBufMSP432_TIMERA1_CAPTURECOMPARE1 = 2, ADCBufMSP432_TIMERA1_CAPTURECOMPARE2 = 3, ADCBufMSP432_TIMERA2_CAPTURECOMPARE1 = 4, ADCBufMSP432_TIMERA2_CAPTURECOMPARE2 = 5, ADCBufMSP432_TIMERA3_CAPTURECOMPARE1 = 6 } |
ADCMSP432 timer trigger source These fields are used by ADCBufMSP432_HWAttrs to specify the Timer Capture for each channel. More... | |
enum | ADCBufMSP432_ClockSource { ADCBufMSP432_ADC_CLOCK = ADC_CLOCKSOURCE_ADCOSC, ADCBufMSP432_SYSOSC_CLOCK = ADC_CLOCKSOURCE_SYSOSC, ADCBufMSP432_ACLK_CLOCK = ADC_CLOCKSOURCE_ACLK, ADCBufMSP432_MCLK_CLOCK = ADC_CLOCKSOURCE_MCLK, ADCBufMSP432_SMCLK_CLOCK = ADC_CLOCKSOURCE_SMCLK, ADCBufMSP432_HSMCLK_CLOCK = ADC_CLOCKSOURCE_HSMCLK } |
ADCMSP432 clock source These fields are used by ADCBufMSP432_HWAttrs to specify the clock source for the ADC module. More... | |
enum | ADCBufMSP432_TriggerSource { ADCBufMSP432_TIMER_TRIGGER = ADC_MANUAL_ITERATION, ADCBufMSP432_SOFTWARE_AUTOMATIC_TRIGGER = ADC_AUTOMATIC_ITERATION } |
ADCMSP432 trigger source These fields are used by ADCBufMSP432_HWAttrs to specify the trigger source for the ADC. More... | |
enum | ADCBufMSP432_DifferentialMode { ADCBufMSP432_SINGLE_ENDED = ADC_NONDIFFERENTIAL_INPUTS, ADCBufMSP432_DIFFERENTIAL = ADC_DIFFERENTIAL_INPUTS } |
ADCMSP432 Differential Mode These fields are used by ADCBufMSP432_HWAttrs to specify if ADC differential sampling mode is selected. More... | |
enum | ADCBufMSP432_InternalSourceMode { ADCBufMSP432_INTERNAL_SOURCE_MODE_OFF = 0, ADCBufMSP432_TEMPERATURE_MODE = ADC_TEMPSENSEMAP, ADCBufMSP432_BATTERY_MONITOR_MODE = ADC_BATTMAP } |
ADCMSP432 Internal Source Mode These fields are used by ADCBufMSP432_HWAttrs to specify if a internal source mode is selected, i.e. temperature sensore or battery monitor modes. More... | |
Variables | |
const ADCBuf_FxnTable | ADCBufMSP432_fxnTable |
#define ADCBufMSP432_CMD_ENTER_ADC_ULTRA_LOW_POWER_MODE ADCBuf_CMD_RESERVED + 1 |
This control function enters ADC in low power mode.
This function changes the ADC clock source to ADC Clock, enables the reference to burst mode, sets the ADC resolution to 8 bits and enables Ultra Low Power Mode of ADC.
#define ADCBufMSP432_CMD_EXIT_ADC_ULTRA_LOW_POWER_MODE ADCBuf_CMD_RESERVED + 2 |
This control function exits ADC from low power mode.
This function changes the ADC clock source to default set by hwAttrib, disables the reference burst mode, sets the ADC resolution to 14 bits and enables Unrestricted Power Mode of ADC.
#define ADCBufMSP432_P4_0_A13 ((13 << 10) | 0x0340) /* ch 13, port 4, pin 0 */ |
#define ADCBufMSP432_P4_1_A12 ((12 << 10) | 0x0341) /* ch 12, port 4, pin 1 */ |
#define ADCBufMSP432_P4_2_A11 ((11 << 10) | 0x0342) /* ch 11, port 4, pin 2 */ |
#define ADCBufMSP432_P4_3_A10 ((10 << 10) | 0x0343) /* ch 10, port 4, pin 3 */ |
#define ADCBufMSP432_P4_4_A9 ((9 << 10) | 0x0344) /* ch 9, port 4, pin 4 */ |
#define ADCBufMSP432_P4_5_A8 ((8 << 10) | 0x0345) /* ch 8, port 4, pin 5 */ |
#define ADCBufMSP432_P4_6_A7 ((7 << 10) | 0x0346) /* ch 7, port 4, pin 6 */ |
#define ADCBufMSP432_P4_7_A6 ((6 << 10) | 0x0347) /* ch 6, port 4, pin 7 */ |
#define ADCBufMSP432_P5_0_A5 ((5 << 10) | 0x0350) /* ch 5, port 5, pin 0 */ |
#define ADCBufMSP432_P5_1_A4 ((4 << 10) | 0x0351) /* ch 4, port 5, pin 1 */ |
#define ADCBufMSP432_P5_2_A3 ((3 << 10) | 0x0352) /* ch 3, port 5, pin 2 */ |
#define ADCBufMSP432_P5_3_A2 ((2 << 10) | 0x0353) /* ch 2, port 5, pin 3 */ |
#define ADCBufMSP432_P5_4_A1 ((1 << 10) | 0x0354) /* ch 1, port 5, pin 4 */ |
#define ADCBufMSP432_P5_5_A0 ((0 << 10) | 0x0355) /* ch 0, port 5, pin 5 */ |
#define ADCBufMSP432_P6_0_A15 ((15 << 10) | 0x0360) /* ch 15, port 6, pin 0 */ |
#define ADCBufMSP432_P6_1_A14 ((14 << 10) | 0x0361) /* ch 14, port 6, pin 1 */ |
#define ADCBufMSP432_P8_2_A23 ((23 << 10) | 0x0382) /* ch 23, port 8, pin 2 */ |
#define ADCBufMSP432_P8_3_A22 ((22 << 10) | 0x0383) /* ch 22, port 8, pin 3 */ |
#define ADCBufMSP432_P8_4_A21 ((21 << 10) | 0x0384) /* ch 21, port 8, pin 4 */ |
#define ADCBufMSP432_P8_5_A20 ((20 << 10) | 0x0385) /* ch 20, port 8, pin 5 */ |
#define ADCBufMSP432_P8_6_A19 ((19 << 10) | 0x0386) /* ch 19, port 8, pin 6 */ |
#define ADCBufMSP432_P8_7_A18 ((18 << 10) | 0x0387) /* ch 18, port 8, pin 7 */ |
#define ADCBufMSP432_P9_0_A17 ((17 << 10) | 0x0390) /* ch 17, port 9, pin 0 */ |
#define ADCBufMSP432_P9_1_A16 ((16 << 10) | 0x0391) /* ch 16, port 9, pin 1 */ |
#define ADCBufMSP432_PIN_NONE 0 |
#define ADCBufMSP432_INTERNAL_SOURCE_PIN 0 |
typedef enum ADCBufMSP432_ReferenceSource ADCBufMSP432_ReferenceSource |
ADCMSP432 reference source These fields are used by ADCBufMSP432_HWAttrs to specify the reference voltage for each channel.
ADCMSP432 sampling duration These fields define the MSP432 ADC sampling duration (sample and hold time) in the pulse width unit. User can specify the differnt sampling duration in the ADCBufMSP432_ParamsExtension when opening the ADC.
ADCMSP432 timer trigger source These fields are used by ADCBufMSP432_HWAttrs to specify the Timer Capture for each channel.
typedef enum ADCBufMSP432_ClockSource ADCBufMSP432_ClockSource |
ADCMSP432 clock source These fields are used by ADCBufMSP432_HWAttrs to specify the clock source for the ADC module.
typedef enum ADCBufMSP432_TriggerSource ADCBufMSP432_TriggerSource |
ADCMSP432 trigger source These fields are used by ADCBufMSP432_HWAttrs to specify the trigger source for the ADC.
ADCMSP432 Differential Mode These fields are used by ADCBufMSP432_HWAttrs to specify if ADC differential sampling mode is selected.
ADCMSP432 Internal Source Mode These fields are used by ADCBufMSP432_HWAttrs to specify if a internal source mode is selected, i.e. temperature sensore or battery monitor modes.
typedef struct ADCBufMSP432_ParamsExtension ADCBufMSP432_ParamsExtension |
MSP432 specfic extension to ADCBuf_Params.
To use non-default MSP432 specific parameters when calling ADCBuf_open(), a pointer to an instance of this struct must be specified in ADCBuf_Params::custom. Alternatively, these values can be set using the control function after calling ADCBuf_open().
typedef struct ADCBufMSP432_Channels ADCBufMSP432_Channels |
ADCMSP432 Channel setting These fields define channel-specific settings: GPIO and reference voltage. These settings happen when ADCBuf_convert() is called.
typedef struct ADCBufMSP432_HWAttrs ADCBufMSP432_HWAttrs |
ADCBufMSP432 Hardware attributes These fields are populated by PinMux tool but user is allowed to change for different channels setting.
A sample structure is shown below:
typedef struct ADCBufMSP432_Object ADCBufMSP432_Object |
ADCBufMSP432 Object.
The application must not access any member variables of this structure!
ADCMSP432 reference source These fields are used by ADCBufMSP432_HWAttrs to specify the reference voltage for each channel.
Enumerator | |
---|---|
ADCBufMSP432_VREFPOS_AVCC_VREFNEG_VSS | |
ADCBufMSP432_VREFPOS_INTBUF_VREFNEG_VSS | |
ADCBufMSP432_VREFPOS_EXTPOS_VREFNEG_EXTNEG | |
ADCBufMSP432_VREFPOS_EXTBUF_VREFNEG_EXTNEG |
ADCMSP432 sampling duration These fields define the MSP432 ADC sampling duration (sample and hold time) in the pulse width unit. User can specify the differnt sampling duration in the ADCBufMSP432_ParamsExtension when opening the ADC.
ADCMSP432 timer trigger source These fields are used by ADCBufMSP432_HWAttrs to specify the Timer Capture for each channel.
ADCMSP432 clock source These fields are used by ADCBufMSP432_HWAttrs to specify the clock source for the ADC module.
Enumerator | |
---|---|
ADCBufMSP432_ADC_CLOCK | |
ADCBufMSP432_SYSOSC_CLOCK | |
ADCBufMSP432_ACLK_CLOCK | |
ADCBufMSP432_MCLK_CLOCK | |
ADCBufMSP432_SMCLK_CLOCK | |
ADCBufMSP432_HSMCLK_CLOCK |
ADCMSP432 trigger source These fields are used by ADCBufMSP432_HWAttrs to specify the trigger source for the ADC.
Enumerator | |
---|---|
ADCBufMSP432_TIMER_TRIGGER | |
ADCBufMSP432_SOFTWARE_AUTOMATIC_TRIGGER |
ADCMSP432 Differential Mode These fields are used by ADCBufMSP432_HWAttrs to specify if ADC differential sampling mode is selected.
Enumerator | |
---|---|
ADCBufMSP432_SINGLE_ENDED | |
ADCBufMSP432_DIFFERENTIAL |
ADCMSP432 Internal Source Mode These fields are used by ADCBufMSP432_HWAttrs to specify if a internal source mode is selected, i.e. temperature sensore or battery monitor modes.
Enumerator | |
---|---|
ADCBufMSP432_INTERNAL_SOURCE_MODE_OFF | |
ADCBufMSP432_TEMPERATURE_MODE | |
ADCBufMSP432_BATTERY_MONITOR_MODE |
const ADCBuf_FxnTable ADCBufMSP432_fxnTable |