![]() |
![]() |
SD driver implementation built on the TI SPI driver.
============================================================================
The SDSPI header file should be included in an application as follows:
Refer to SD.h for a complete description of APIs & example of use.
This SD driver implementation can be used to communicate with SD cards via a SPI peripheral. This driver leverages the TI SPI driver to transfer data to/from the host processor to the SD card. The SD card chip select is also handled by this driver via the TI GPIO driver. Both the SPI driver instance & the GPIO pin (used as chip select) must be specified in the SDSPI hardware attributes.
Note: This driver requires that the 'defaultTxBufValue' field in the SPI driver hardware attributes be set to '0xFF'.
This driver relies on the TI SPI driver to configure the SPI peripheral & perform data transfers. This means that data to be transferred must comply with rules & restrictions set SPI driver (memory alignment & DMA accessibility requirements). Refer to SPI.h & the device specific SPI implementation header files for details.
#include <stdint.h>#include <ti/drivers/dpl/SemaphoreP.h>#include <ti/drivers/SD.h>#include <ti/drivers/SPI.h>
Go to the source code of this file.
Data Structures | |
| struct | SDSPI_HWAttrs_ |
| struct | SDSPI_Object_ |
| SDSPI Object. More... | |
Typedefs | |
| typedef struct SDSPI_HWAttrs_ | SDSPI_HWAttrs |
| typedef struct SDSPI_Object_ | SDSPI_Object |
| SDSPI Object. More... | |
Variables | |
| const SD_FxnTable | SDSPI_fxnTable |
| typedef struct SDSPI_HWAttrs_ SDSPI_HWAttrs |
| typedef struct SDSPI_Object_ SDSPI_Object |
SDSPI Object.
The application must not access any member variables of this structure!
| const SD_FxnTable SDSPI_fxnTable |