LZ4 API Guide
1.00.01.00
|
Compression parameters for a single LZ4 block. More...
#include <lz4.h>
Data Fields | |
const void * | src |
Pointer to the source data buffer to compress. More... | |
void * | dst |
Pointer to the destination data buffer to store compressed data. More... | |
uint32_t | length |
Length of source data buffer. More... | |
void * | hashTable |
Pointer to memory block with pow2(hashLog2Size) bytes allocated. More... | |
uint16_t | hashLog2Size |
Power of two used to determine the hash table size. More... | |
bool | addBlockChecksum |
Compression parameters for a single LZ4 block.
const void* LZ4_compressBlockParams::src |
Pointer to the source data buffer to compress.
Referenced by LZ4_compressBlock().
void* LZ4_compressBlockParams::dst |
Pointer to the destination data buffer to store compressed data.
Referenced by LZ4_compressBlock().
uint32_t LZ4_compressBlockParams::length |
Length of source data buffer.
Referenced by LZ4_compressBlock().
void* LZ4_compressBlockParams::hashTable |
Pointer to memory block with pow2(hashLog2Size) bytes allocated.
Referenced by LZ4_compressBlock().
uint16_t LZ4_compressBlockParams::hashLog2Size |
Power of two used to determine the hash table size.
Referenced by LZ4_compressBlock().
bool LZ4_compressBlockParams::addBlockChecksum |
Add checksum to each compressed block. Decreases compression performance. Valid values are: