Data Fields
UARTMSP432_HWAttrsV1 Struct Reference

UARTMSP432 Hardware attributes. More...

#include <UARTMSP432.h>

Data Fields

unsigned int baseAddr
 
unsigned int intNum
 
unsigned int intPriority
 
uint8_t clockSource
 
uint32_t bitOrder
 
uint8_t numBaudrateEntries
 
UARTMSP432_BaudrateConfig const * baudrateLUT
 
unsigned char * ringBufPtr
 
size_t ringBufSize
 
uint16_t rxPin
 
uint16_t txPin
 
UARTMSP432_ErrorCallback errorFxn
 

Detailed Description

UARTMSP432 Hardware attributes.

These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP432Ware these definitions are found in:

intPriority is the UART peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.dpl interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().

A sample structure is shown below:

unsigned char uartMSP432RingBuffer[2][32];
const UARTMSP432_HWAttrsV1 uartMSP432HWAttrs[MSP_EXP432P401R_UARTCOUNT] = {
{
.baseAddr = EUSCI_A0_BASE,
.intNum = INT_EUSCIA0,
.intPriority = (~0),
.clockSource = EUSCI_A_UART_CLOCKSOURCE_SMCLK,
.bitOrder = EUSCI_A_UART_LSB_FIRST,
.numBaudrateEntries = sizeof(uartMSP432Baudrates) /
.baudrateLUT = uartMSP432Baudrates,
.ringBufPtr = uartMSP432RingBuffer[0],
.ringBufSize = sizeof(uartMSP432RingBuffer[0]),
.errorFxn = NULL
},
{
.baseAddr = EUSCI_A2_BASE,
.intNum = INT_EUSCIA2,
.intPriority = (~0),
.clockSource = EUSCI_A_UART_CLOCKSOURCE_SMCLK,
.bitOrder = EUSCI_A_UART_LSB_FIRST,
.numBaudrateEntries = sizeof(uartMSP432Baudrates) /
.baudrateLUT = uartMSP432Baudrates
.ringBufPtr = uartMSP432RingBuffer[1],
.ringBufSize = sizeof(uartMSP432RingBuffer[1]),
.errorFxn = NULL
}
};

Field Documentation

§ baseAddr

unsigned int UARTMSP432_HWAttrsV1::baseAddr

UART Peripheral's base address

§ intNum

unsigned int UARTMSP432_HWAttrsV1::intNum

UART Peripheral's interrupt vector

§ intPriority

unsigned int UARTMSP432_HWAttrsV1::intPriority

UART Peripheral's interrupt priority

§ clockSource

uint8_t UARTMSP432_HWAttrsV1::clockSource

UART Clock source

§ bitOrder

uint32_t UARTMSP432_HWAttrsV1::bitOrder

UART Bit order

§ numBaudrateEntries

uint8_t UARTMSP432_HWAttrsV1::numBaudrateEntries

Number of UARTMSP432_BaudrateConfig entries

§ baudrateLUT

UARTMSP432_BaudrateConfig const* UARTMSP432_HWAttrsV1::baudrateLUT

Pointer to a table of possible UARTMSP432_BaudrateConfig entries

§ ringBufPtr

unsigned char* UARTMSP432_HWAttrsV1::ringBufPtr

Pointer to a application ring buffer

§ ringBufSize

size_t UARTMSP432_HWAttrsV1::ringBufSize

Size of ringBufPtr

§ rxPin

uint16_t UARTMSP432_HWAttrsV1::rxPin

§ txPin

uint16_t UARTMSP432_HWAttrsV1::txPin

§ errorFxn

UARTMSP432_ErrorCallback UARTMSP432_HWAttrsV1::errorFxn

Application error function to be called on receive errors


The documentation for this struct was generated from the following file:
Copyright 2018, Texas Instruments Incorporated