SDSPI Hardware attributes. More...
#include <SDSPI.h>
SDSPI Hardware attributes.
The SDSPI HWAttrs configuration structure contains the index of the SPI peripheral to be used for data transfers & the index of the GPIO Pin which will act as chip select. This driver uses this information to:
An example configuration structure could look as the following: