SimpleLink Graphics Library  4.10.00.09
Data Structures | Typedefs | Functions | Variables
radioButton.h File Reference
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  Graphics_RadioButton
 This structure defines the characteristics of a RadioButton. More...
 

Typedefs

typedef struct Graphics_RadioButton Graphics_RadioButton
 This structure defines the characteristics of a RadioButton. More...
 

Functions

void Graphics_drawRadioButton (const Graphics_Context *context, const Graphics_RadioButton *radioButton)
 
bool Graphics_isRadioButtonSelected (const Graphics_RadioButton *radioButton, uint16_t x, uint16_t y)
 
void Graphics_drawSelectedRadioButton (const Graphics_Context *context, const Graphics_RadioButton *radioButton)
 
void Graphics_drawReleasedRadioButton (const Graphics_Context *context, const Graphics_RadioButton *radioButton)
 

Variables

Graphics_Context g_sContext
 

Typedef Documentation

§ Graphics_RadioButton

This structure defines the characteristics of a RadioButton.

Variable Documentation

§ g_sContext

Graphics_Context g_sContext
Copyright 2018, Texas Instruments Incorporated