#include <flash_a.h>
uint32_t __sFlashCtl_ProtectionRegister::B0_MAIN_R0 |
uint32_t __sFlashCtl_ProtectionRegister::B0_MAIN_R1 |
uint32_t __sFlashCtl_ProtectionRegister::B0_MAIN_R2 |
uint32_t __sFlashCtl_ProtectionRegister::B0_MAIN_R3 |
uint32_t __sFlashCtl_ProtectionRegister::B0_MAIN_R4 |
uint32_t __sFlashCtl_ProtectionRegister::B0_MAIN_R5 |
uint32_t __sFlashCtl_ProtectionRegister::B0_MAIN_R6 |
uint32_t __sFlashCtl_ProtectionRegister::B0_MAIN_R7 |
uint32_t __sFlashCtl_ProtectionRegister::B1_MAIN_R0 |
uint32_t __sFlashCtl_ProtectionRegister::B1_MAIN_R1 |
uint32_t __sFlashCtl_ProtectionRegister::B1_MAIN_R2 |
uint32_t __sFlashCtl_ProtectionRegister::B1_MAIN_R3 |
uint32_t __sFlashCtl_ProtectionRegister::B1_MAIN_R4 |
uint32_t __sFlashCtl_ProtectionRegister::B1_MAIN_R5 |
uint32_t __sFlashCtl_ProtectionRegister::B1_MAIN_R6 |
uint32_t __sFlashCtl_ProtectionRegister::B1_MAIN_R7 |
uint32_t __sFlashCtl_ProtectionRegister::B0_INFO_R0 |
uint32_t __sFlashCtl_ProtectionRegister::B1_INFO_R0 |
The documentation for this struct was generated from the following file: