![]() |
![]() |
ADCMSP432 Channel setting These fields define channel-specific settings: GPIO and reference voltage. These settings happen when ADCBuf_convert() is called. More...
#include <ADCBufMSP432.h>
Data Fields | |
uint_fast16_t | adcPin |
ADCBufMSP432_ReferenceSource | refSource |
uint32_t | refVoltage |
ADCBufMSP432_DifferentialMode | adcInputMode |
uint_fast16_t | adcDifferentialPin |
ADCBufMSP432_InternalSourceMode | adcInternalSource |
ADCMSP432 Channel setting These fields define channel-specific settings: GPIO and reference voltage. These settings happen when ADCBuf_convert() is called.
uint_fast16_t ADCBufMSP432_Channels::adcPin |
ADC pin, port channel
ADCBufMSP432_ReferenceSource ADCBufMSP432_Channels::refSource |
ADC reference source
uint32_t ADCBufMSP432_Channels::refVoltage |
ADC reference voltage in microVolts (if it is internal, the value should be 1.5 or 2.5)
ADCBufMSP432_DifferentialMode ADCBufMSP432_Channels::adcInputMode |
ADC differential mode option
uint_fast16_t ADCBufMSP432_Channels::adcDifferentialPin |
ADC differential pin, if adcInputMode = 1, specify pin
ADCBufMSP432_InternalSourceMode ADCBufMSP432_Channels::adcInternalSource |
ADC internal source mode select