Data Fields
UDMAMSP432_Transfer Struct Reference

UDMAMSP432 Transfer configuration. More...

#include <UDMAMSP432.h>

Data Fields

uint32_t dmaChannel
 
uint32_t structSelect
 
uint32_t ctlOptions
 
uint32_t transferMode
 
void * dmaTransferSource
 
void * dmaTransferDestination
 
uint32_t transferSize
 

Detailed Description

UDMAMSP432 Transfer configuration.

The UDMAMSP432_Transfer structure contains parameters for initializing a DMA transfer using a given DMA channel number.

This struct is used in UDMAMSP432_setupTransfer().

Field Documentation

§ dmaChannel

uint32_t UDMAMSP432_Transfer::dmaChannel

DMA channel

§ structSelect

uint32_t UDMAMSP432_Transfer::structSelect

§ ctlOptions

uint32_t UDMAMSP432_Transfer::ctlOptions

DMA control options

§ transferMode

uint32_t UDMAMSP432_Transfer::transferMode

DMA transfer mode. Basic or PingPong

§ dmaTransferSource

void* UDMAMSP432_Transfer::dmaTransferSource

Source of DMA transfer

§ dmaTransferDestination

void* UDMAMSP432_Transfer::dmaTransferDestination

Destination of DMA transfer

§ transferSize

uint32_t UDMAMSP432_Transfer::transferSize

Size of DMA transfer


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated