![]() |
![]() |
CaptureMSP432 Object. More...
#include <CaptureMSP432.h>
Data Fields | |
HwiP_Handle | hwiHandle |
Capture_CallBackFxn | callBack |
Capture_PeriodUnits | periodUnits |
uint32_t | previousCount |
uint32_t | ccrRegister |
bool | isRunning |
CaptureMSP432 Object.
The application must not access any member variables of this structure!
HwiP_Handle CaptureMSP432_Object_::hwiHandle |
Capture_CallBackFxn CaptureMSP432_Object_::callBack |
Capture_PeriodUnits CaptureMSP432_Object_::periodUnits |
uint32_t CaptureMSP432_Object_::previousCount |
uint32_t CaptureMSP432_Object_::ccrRegister |
bool CaptureMSP432_Object_::isRunning |