![]() |
![]() |
ADCBufMSP432 Hardware attributes These fields are populated by PinMux tool but user is allowed to change for different channels setting. More...
#include <ADCBufMSP432.h>
Data Fields | |
uint32_t | intPriority |
ADCBufMSP432_Channels * | channelSetting |
ADCBufMSP432_TimerReferenceSource | adcTimerTriggerSource |
uint8_t | useDMA |
uint8_t | dmaIntNum |
ADCBufMSP432_TriggerSource | adcTriggerSource |
uint32_t | timerDutyCycle |
ADCBufMSP432_ClockSource | clockSource |
ADCBufMSP432 Hardware attributes These fields are populated by PinMux tool but user is allowed to change for different channels setting.
A sample structure is shown below:
uint32_t ADCBufMSP432_HWAttrs::intPriority |
ADCBufMSP432_Channels* ADCBufMSP432_HWAttrs::channelSetting |
ADC interrupt priority
ADCBufMSP432_TimerReferenceSource ADCBufMSP432_HWAttrs::adcTimerTriggerSource |
ADC channel specific setting
uint8_t ADCBufMSP432_HWAttrs::useDMA |
ADC Timer Trigger Source
uint8_t ADCBufMSP432_HWAttrs::dmaIntNum |
Select if ADC uses DMA DMA interrupt number
ADCBufMSP432_TriggerSource ADCBufMSP432_HWAttrs::adcTriggerSource |
uint32_t ADCBufMSP432_HWAttrs::timerDutyCycle |
ADC Trigger Source
ADCBufMSP432_ClockSource ADCBufMSP432_HWAttrs::clockSource |
ADC Timer Duty Cycle