![]() |
![]() |
Macros | |
| #define | DISPLAY_STATUS_SUCCESS 0 |
| Successful status code returned by Display_control(). More... | |
| #define | DISPLAY_STATUS_ERROR -1 |
| Generic error status code returned by Display_control(). More... | |
| #define | DISPLAY_STATUS_UNDEFINEDCMD -2 |
| An error status code returned by Display_control() for undefined command codes. More... | |
DISPLAY_STATUS_* macros are general status codes returned by Display_control()
| #define DISPLAY_STATUS_SUCCESS 0 |
Successful status code returned by Display_control().
Display_control() returns DISPLAY_STATUS_SUCCESS if the control code was executed successfully.
| #define DISPLAY_STATUS_ERROR -1 |
Generic error status code returned by Display_control().
Display_control() returns DISPLAY_STATUS_ERROR if the control code was not executed successfully.
| #define DISPLAY_STATUS_UNDEFINEDCMD -2 |
An error status code returned by Display_control() for undefined command codes.
Display_control() returns DISPLAY_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.