SPI driver implementation for a EUSCI peripheral on MSP432 using the micro DMA controller.
============================================================================
The SPI header file should be included in an application as follows:
Refer to SPI.h for a complete description of APIs & example of use.
This SPI driver implementation is designed to operate on a EUCSI controller in SPI mode using a micro DMA controller.
Frame Formats
This SPI controller supports 4 phase & polarity formats. Refer to the device specific data sheets & technical reference manuals for specifics on each format.
SPI Chip Select
The SPI driver can be used in 3-pin or 4-pin mode. When in 4-pin mode the hardware manages a pin as the chip select. In 3-pin mode it is the application's responsibility to assert and de-assert a GPIO pin for chip select purposes.
Chip select type | SPI_MASTER mode | SPI_SLAVE mode |
Hardware chip select | No action is needed by the application to select the peripheral. | See the device documentation on it's chip select requirements. |
Software chip select | The application is responsible to ensure that correct SPI slave is selected before performing a SPI_transfer(). | Up to the application's implementation. |
SPI data frames
The EUSCI controller only supports 8-bit data frames.
dataSize | buffer element size |
8 bits | uint8_t |
DMA operation
DMA use in this driver varies based on the SPI_TransferMode set when the driver instance was opened. If the driver was opened in SPI_MODE_CALLBACK, all transfers make use of the DMA regardless of the amount of data.
If the driver was opened in SPI_MODE_BLOCKING, it verifies the amount of data frames to be transfered exceeds the minDmaTransferSize before performing a transfer using the DMA. minDmaTransferSize (in the SPIMSP432DMA_HWAttrs) allows users to set a minimum amount of data frames a transfer must have to perform a transfer using the DMA. If the amount of data is less than minDmaTransferSize, the driver performs a polling transfer. This feature is provided for situations where there is little data to be transfered & it is more efficient to simply perform a polling transfer instead of configuring the DMA & waiting until the task is unblocked.
DMA Interrupts
The MSP432 DMA controller has 4 interrupt vectors to handle all DMA related IRQ. Due to the "shared" nature of the DMA interrupts, this driver implementation requires each SPI instance to explicitly use a single DMA interrupt. It is up to the application to ensure no two peripherals are configured to respond to a given DMA interrupt at any moment.
DMA transfer size limit
The DMA controller only supports data transfers of up to 1024 data frames, so large amounts of data will be split & transfered accordingly. Each SPI driver instance requires 2 DMA channels (Tx and Rx) to operate.
DMA accessible memory
Ensure that the txBuf and rxBuf (in SPI_Transaction) point to memory that is accessible by the DMA.
Scratch Buffers
A uint8_t scratch buffer is used to allow SPI_transfers where txBuf or rxBuf are NULL. Rather than requiring txBuf or rxBuf to have a dummy buffer of size of the transfer count, a single DMA accessible uint8_t scratch buffer is used. When txBuf is NULL, an internal scratch buffer is initialized to the defaultTxBufValue so the DMA will send some known value.
|
#define | SPIMSP432DMA_P1_0_UCA0STE 0x00000110 /* Primary, port 1, pin 0 */ |
|
#define | SPIMSP432DMA_P1_1_UCA0CLK 0x00000111 /* Primary, port 1, pin 1 */ |
|
#define | SPIMSP432DMA_P1_2_UCA0SOMI 0x00000112 /* Primary, port 1, pin 2 */ |
|
#define | SPIMSP432DMA_P1_3_UCA0SIMO 0x00000113 /* Primary, port 1, pin 3 */ |
|
#define | SPIMSP432DMA_P1_4_UCB0STE 0x00000114 /* Primary, port 1, pin 4 */ |
|
#define | SPIMSP432DMA_P1_5_UCB0CLK 0x00000115 /* Primary, port 1, pin 5 */ |
|
#define | SPIMSP432DMA_P1_6_UCB0SIMO 0x00000116 /* Primary, port 1, pin 6 */ |
|
#define | SPIMSP432DMA_P1_7_UCB0SOMI 0x00000117 /* Primary, port 1, pin 7 */ |
|
#define | SPIMSP432DMA_P2_0_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x20) |
|
#define | SPIMSP432DMA_P2_0_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x20) |
|
#define | SPIMSP432DMA_P2_0_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x20) |
|
#define | SPIMSP432DMA_P2_0_UCA1STE ((PMAP_UCA1STE << 10) | 0x20) |
|
#define | SPIMSP432DMA_P2_0_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x20) |
|
#define | SPIMSP432DMA_P2_0_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x20) |
|
#define | SPIMSP432DMA_P2_0_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x20) |
|
#define | SPIMSP432DMA_P2_0_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x20) |
|
#define | SPIMSP432DMA_P2_0_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x20) |
|
#define | SPIMSP432DMA_P2_0_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x20) |
|
#define | SPIMSP432DMA_P2_0_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x20) |
|
#define | SPIMSP432DMA_P2_0_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x20) |
|
#define | SPIMSP432DMA_P2_0_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x20) |
|
#define | SPIMSP432DMA_P2_0_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x20) |
|
#define | SPIMSP432DMA_P2_0_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x20) |
|
#define | SPIMSP432DMA_P2_0_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x20) |
|
#define | SPIMSP432DMA_P2_0_UCA2STE ((PMAP_UCA2STE << 10) | 0x20) |
|
#define | SPIMSP432DMA_P2_0_UCB2STE ((PMAP_UCB2STE << 10) | 0x20) |
|
#define | SPIMSP432DMA_P2_1_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x21) |
|
#define | SPIMSP432DMA_P2_1_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x21) |
|
#define | SPIMSP432DMA_P2_1_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x21) |
|
#define | SPIMSP432DMA_P2_1_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x21) |
|
#define | SPIMSP432DMA_P2_1_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x21) |
|
#define | SPIMSP432DMA_P2_1_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x21) |
|
#define | SPIMSP432DMA_P2_1_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x21) |
|
#define | SPIMSP432DMA_P2_1_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x21) |
|
#define | SPIMSP432DMA_P2_1_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x21) |
|
#define | SPIMSP432DMA_P2_1_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x21) |
|
#define | SPIMSP432DMA_P2_1_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x21) |
|
#define | SPIMSP432DMA_P2_1_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x21) |
|
#define | SPIMSP432DMA_P2_1_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x21) |
|
#define | SPIMSP432DMA_P2_1_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x21) |
|
#define | SPIMSP432DMA_P2_1_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x21) |
|
#define | SPIMSP432DMA_P2_1_UCA1STE ((PMAP_UCA1STE << 10) | 0x21) |
|
#define | SPIMSP432DMA_P2_1_UCA2STE ((PMAP_UCA2STE << 10) | 0x21) |
|
#define | SPIMSP432DMA_P2_1_UCB2STE ((PMAP_UCB2STE << 10) | 0x21) |
|
#define | SPIMSP432DMA_P2_2_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x22) |
|
#define | SPIMSP432DMA_P2_2_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x22) |
|
#define | SPIMSP432DMA_P2_2_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x22) |
|
#define | SPIMSP432DMA_P2_2_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x22) |
|
#define | SPIMSP432DMA_P2_2_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x22) |
|
#define | SPIMSP432DMA_P2_2_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x22) |
|
#define | SPIMSP432DMA_P2_2_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x22) |
|
#define | SPIMSP432DMA_P2_2_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x22) |
|
#define | SPIMSP432DMA_P2_2_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x22) |
|
#define | SPIMSP432DMA_P2_2_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x22) |
|
#define | SPIMSP432DMA_P2_2_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x22) |
|
#define | SPIMSP432DMA_P2_2_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x22) |
|
#define | SPIMSP432DMA_P2_2_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x22) |
|
#define | SPIMSP432DMA_P2_2_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x22) |
|
#define | SPIMSP432DMA_P2_2_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x22) |
|
#define | SPIMSP432DMA_P2_2_UCA1STE ((PMAP_UCA1STE << 10) | 0x22) |
|
#define | SPIMSP432DMA_P2_2_UCA2STE ((PMAP_UCA2STE << 10) | 0x22) |
|
#define | SPIMSP432DMA_P2_2_UCB2STE ((PMAP_UCB2STE << 10) | 0x22) |
|
#define | SPIMSP432DMA_P2_3_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x23) |
|
#define | SPIMSP432DMA_P2_3_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x23) |
|
#define | SPIMSP432DMA_P2_3_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x23) |
|
#define | SPIMSP432DMA_P2_3_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x23) |
|
#define | SPIMSP432DMA_P2_3_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x23) |
|
#define | SPIMSP432DMA_P2_3_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x23) |
|
#define | SPIMSP432DMA_P2_3_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x23) |
|
#define | SPIMSP432DMA_P2_3_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x23) |
|
#define | SPIMSP432DMA_P2_3_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x23) |
|
#define | SPIMSP432DMA_P2_3_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x23) |
|
#define | SPIMSP432DMA_P2_3_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x23) |
|
#define | SPIMSP432DMA_P2_3_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x23) |
|
#define | SPIMSP432DMA_P2_3_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x23) |
|
#define | SPIMSP432DMA_P2_3_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x23) |
|
#define | SPIMSP432DMA_P2_3_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x23) |
|
#define | SPIMSP432DMA_P2_3_UCA1STE ((PMAP_UCA1STE << 10) | 0x23) |
|
#define | SPIMSP432DMA_P2_3_UCA2STE ((PMAP_UCA2STE << 10) | 0x23) |
|
#define | SPIMSP432DMA_P2_3_UCB2STE ((PMAP_UCB2STE << 10) | 0x23) |
|
#define | SPIMSP432DMA_P2_4_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x24) |
|
#define | SPIMSP432DMA_P2_4_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x24) |
|
#define | SPIMSP432DMA_P2_4_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x24) |
|
#define | SPIMSP432DMA_P2_4_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x24) |
|
#define | SPIMSP432DMA_P2_4_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x24) |
|
#define | SPIMSP432DMA_P2_4_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x24) |
|
#define | SPIMSP432DMA_P2_4_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x24) |
|
#define | SPIMSP432DMA_P2_4_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x24) |
|
#define | SPIMSP432DMA_P2_4_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x24) |
|
#define | SPIMSP432DMA_P2_4_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x24) |
|
#define | SPIMSP432DMA_P2_4_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x24) |
|
#define | SPIMSP432DMA_P2_4_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x24) |
|
#define | SPIMSP432DMA_P2_4_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x24) |
|
#define | SPIMSP432DMA_P2_4_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x24) |
|
#define | SPIMSP432DMA_P2_4_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x24) |
|
#define | SPIMSP432DMA_P2_4_UCA1STE ((PMAP_UCA1STE << 10) | 0x24) |
|
#define | SPIMSP432DMA_P2_4_UCA2STE ((PMAP_UCA2STE << 10) | 0x24) |
|
#define | SPIMSP432DMA_P2_4_UCB2STE ((PMAP_UCB2STE << 10) | 0x24) |
|
#define | SPIMSP432DMA_P2_5_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x25) |
|
#define | SPIMSP432DMA_P2_5_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x25) |
|
#define | SPIMSP432DMA_P2_5_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x25) |
|
#define | SPIMSP432DMA_P2_5_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x25) |
|
#define | SPIMSP432DMA_P2_5_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x25) |
|
#define | SPIMSP432DMA_P2_5_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x25) |
|
#define | SPIMSP432DMA_P2_5_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x25) |
|
#define | SPIMSP432DMA_P2_5_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x25) |
|
#define | SPIMSP432DMA_P2_5_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x25) |
|
#define | SPIMSP432DMA_P2_5_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x25) |
|
#define | SPIMSP432DMA_P2_5_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x25) |
|
#define | SPIMSP432DMA_P2_5_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x25) |
|
#define | SPIMSP432DMA_P2_5_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x25) |
|
#define | SPIMSP432DMA_P2_5_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x25) |
|
#define | SPIMSP432DMA_P2_5_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x25) |
|
#define | SPIMSP432DMA_P2_5_UCA1STE ((PMAP_UCA1STE << 10) | 0x25) |
|
#define | SPIMSP432DMA_P2_5_UCA2STE ((PMAP_UCA2STE << 10) | 0x25) |
|
#define | SPIMSP432DMA_P2_5_UCB2STE ((PMAP_UCB2STE << 10) | 0x25) |
|
#define | SPIMSP432DMA_P2_6_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x26) |
|
#define | SPIMSP432DMA_P2_6_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x26) |
|
#define | SPIMSP432DMA_P2_6_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x26) |
|
#define | SPIMSP432DMA_P2_6_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x26) |
|
#define | SPIMSP432DMA_P2_6_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x26) |
|
#define | SPIMSP432DMA_P2_6_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x26) |
|
#define | SPIMSP432DMA_P2_6_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x26) |
|
#define | SPIMSP432DMA_P2_6_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x26) |
|
#define | SPIMSP432DMA_P2_6_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x26) |
|
#define | SPIMSP432DMA_P2_6_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x26) |
|
#define | SPIMSP432DMA_P2_6_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x26) |
|
#define | SPIMSP432DMA_P2_6_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x26) |
|
#define | SPIMSP432DMA_P2_6_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x26) |
|
#define | SPIMSP432DMA_P2_6_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x26) |
|
#define | SPIMSP432DMA_P2_6_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x26) |
|
#define | SPIMSP432DMA_P2_6_UCA1STE ((PMAP_UCA1STE << 10) | 0x26) |
|
#define | SPIMSP432DMA_P2_6_UCA2STE ((PMAP_UCA2STE << 10) | 0x26) |
|
#define | SPIMSP432DMA_P2_6_UCB2STE ((PMAP_UCB2STE << 10) | 0x26) |
|
#define | SPIMSP432DMA_P2_7_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x27) |
|
#define | SPIMSP432DMA_P2_7_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x27) |
|
#define | SPIMSP432DMA_P2_7_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x27) |
|
#define | SPIMSP432DMA_P2_7_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x27) |
|
#define | SPIMSP432DMA_P2_7_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x27) |
|
#define | SPIMSP432DMA_P2_7_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x27) |
|
#define | SPIMSP432DMA_P2_7_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x27) |
|
#define | SPIMSP432DMA_P2_7_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x27) |
|
#define | SPIMSP432DMA_P2_7_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x27) |
|
#define | SPIMSP432DMA_P2_7_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x27) |
|
#define | SPIMSP432DMA_P2_7_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x27) |
|
#define | SPIMSP432DMA_P2_7_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x27) |
|
#define | SPIMSP432DMA_P2_7_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x27) |
|
#define | SPIMSP432DMA_P2_7_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x27) |
|
#define | SPIMSP432DMA_P2_7_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x27) |
|
#define | SPIMSP432DMA_P2_7_UCA1STE ((PMAP_UCA1STE << 10) | 0x27) |
|
#define | SPIMSP432DMA_P2_7_UCA2STE ((PMAP_UCA2STE << 10) | 0x27) |
|
#define | SPIMSP432DMA_P2_7_UCB2STE ((PMAP_UCB2STE << 10) | 0x27) |
|
#define | SPIMSP432DMA_P3_0_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x30) |
|
#define | SPIMSP432DMA_P3_0_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x30) |
|
#define | SPIMSP432DMA_P3_0_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x30) |
|
#define | SPIMSP432DMA_P3_0_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x30) |
|
#define | SPIMSP432DMA_P3_0_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x30) |
|
#define | SPIMSP432DMA_P3_0_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x30) |
|
#define | SPIMSP432DMA_P3_0_UCA2STE ((PMAP_UCA2STE << 10) | 0x30) |
|
#define | SPIMSP432DMA_P3_0_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x30) |
|
#define | SPIMSP432DMA_P3_0_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x30) |
|
#define | SPIMSP432DMA_P3_0_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x30) |
|
#define | SPIMSP432DMA_P3_0_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x30) |
|
#define | SPIMSP432DMA_P3_0_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x30) |
|
#define | SPIMSP432DMA_P3_0_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x30) |
|
#define | SPIMSP432DMA_P3_0_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x30) |
|
#define | SPIMSP432DMA_P3_0_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x30) |
|
#define | SPIMSP432DMA_P3_0_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x30) |
|
#define | SPIMSP432DMA_P3_0_UCA1STE ((PMAP_UCA1STE << 10) | 0x30) |
|
#define | SPIMSP432DMA_P3_0_UCB2STE ((PMAP_UCB2STE << 10) | 0x30) |
|
#define | SPIMSP432DMA_P3_1_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x31) |
|
#define | SPIMSP432DMA_P3_1_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x31) |
|
#define | SPIMSP432DMA_P3_1_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x31) |
|
#define | SPIMSP432DMA_P3_1_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x31) |
|
#define | SPIMSP432DMA_P3_1_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x31) |
|
#define | SPIMSP432DMA_P3_1_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x31) |
|
#define | SPIMSP432DMA_P3_1_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x31) |
|
#define | SPIMSP432DMA_P3_1_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x31) |
|
#define | SPIMSP432DMA_P3_1_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x31) |
|
#define | SPIMSP432DMA_P3_1_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x31) |
|
#define | SPIMSP432DMA_P3_1_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x31) |
|
#define | SPIMSP432DMA_P3_1_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x31) |
|
#define | SPIMSP432DMA_P3_1_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x31) |
|
#define | SPIMSP432DMA_P3_1_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x31) |
|
#define | SPIMSP432DMA_P3_1_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x31) |
|
#define | SPIMSP432DMA_P3_1_UCA1STE ((PMAP_UCA1STE << 10) | 0x31) |
|
#define | SPIMSP432DMA_P3_1_UCA2STE ((PMAP_UCA2STE << 10) | 0x31) |
|
#define | SPIMSP432DMA_P3_1_UCB2STE ((PMAP_UCB2STE << 10) | 0x31) |
|
#define | SPIMSP432DMA_P3_2_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x32) |
|
#define | SPIMSP432DMA_P3_2_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x32) |
|
#define | SPIMSP432DMA_P3_2_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x32) |
|
#define | SPIMSP432DMA_P3_2_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x32) |
|
#define | SPIMSP432DMA_P3_2_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x32) |
|
#define | SPIMSP432DMA_P3_2_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x32) |
|
#define | SPIMSP432DMA_P3_2_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x32) |
|
#define | SPIMSP432DMA_P3_2_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x32) |
|
#define | SPIMSP432DMA_P3_2_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x32) |
|
#define | SPIMSP432DMA_P3_2_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x32) |
|
#define | SPIMSP432DMA_P3_2_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x32) |
|
#define | SPIMSP432DMA_P3_2_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x32) |
|
#define | SPIMSP432DMA_P3_2_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x32) |
|
#define | SPIMSP432DMA_P3_2_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x32) |
|
#define | SPIMSP432DMA_P3_2_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x32) |
|
#define | SPIMSP432DMA_P3_2_UCA1STE ((PMAP_UCA1STE << 10) | 0x32) |
|
#define | SPIMSP432DMA_P3_2_UCA2STE ((PMAP_UCA2STE << 10) | 0x32) |
|
#define | SPIMSP432DMA_P3_2_UCB2STE ((PMAP_UCB2STE << 10) | 0x32) |
|
#define | SPIMSP432DMA_P3_3_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x33) |
|
#define | SPIMSP432DMA_P3_3_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x33) |
|
#define | SPIMSP432DMA_P3_3_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x33) |
|
#define | SPIMSP432DMA_P3_3_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x33) |
|
#define | SPIMSP432DMA_P3_3_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x33) |
|
#define | SPIMSP432DMA_P3_3_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x33) |
|
#define | SPIMSP432DMA_P3_3_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x33) |
|
#define | SPIMSP432DMA_P3_3_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x33) |
|
#define | SPIMSP432DMA_P3_3_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x33) |
|
#define | SPIMSP432DMA_P3_3_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x33) |
|
#define | SPIMSP432DMA_P3_3_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x33) |
|
#define | SPIMSP432DMA_P3_3_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x33) |
|
#define | SPIMSP432DMA_P3_3_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x33) |
|
#define | SPIMSP432DMA_P3_3_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x33) |
|
#define | SPIMSP432DMA_P3_3_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x33) |
|
#define | SPIMSP432DMA_P3_3_UCA1STE ((PMAP_UCA1STE << 10) | 0x33) |
|
#define | SPIMSP432DMA_P3_3_UCA2STE ((PMAP_UCA2STE << 10) | 0x33) |
|
#define | SPIMSP432DMA_P3_3_UCB2STE ((PMAP_UCB2STE << 10) | 0x33) |
|
#define | SPIMSP432DMA_P3_4_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x34) |
|
#define | SPIMSP432DMA_P3_4_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x34) |
|
#define | SPIMSP432DMA_P3_4_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x34) |
|
#define | SPIMSP432DMA_P3_4_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x34) |
|
#define | SPIMSP432DMA_P3_4_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x34) |
|
#define | SPIMSP432DMA_P3_4_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x34) |
|
#define | SPIMSP432DMA_P3_4_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x34) |
|
#define | SPIMSP432DMA_P3_4_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x34) |
|
#define | SPIMSP432DMA_P3_4_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x34) |
|
#define | SPIMSP432DMA_P3_4_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x34) |
|
#define | SPIMSP432DMA_P3_4_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x34) |
|
#define | SPIMSP432DMA_P3_4_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x34) |
|
#define | SPIMSP432DMA_P3_4_UCB2STE ((PMAP_UCB2STE << 10) | 0x34) |
|
#define | SPIMSP432DMA_P3_4_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x34) |
|
#define | SPIMSP432DMA_P3_4_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x34) |
|
#define | SPIMSP432DMA_P3_4_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x34) |
|
#define | SPIMSP432DMA_P3_4_UCA1STE ((PMAP_UCA1STE << 10) | 0x34) |
|
#define | SPIMSP432DMA_P3_4_UCA2STE ((PMAP_UCA2STE << 10) | 0x34) |
|
#define | SPIMSP432DMA_P3_5_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x35) |
|
#define | SPIMSP432DMA_P3_5_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x35) |
|
#define | SPIMSP432DMA_P3_5_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x35) |
|
#define | SPIMSP432DMA_P3_5_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x35) |
|
#define | SPIMSP432DMA_P3_5_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x35) |
|
#define | SPIMSP432DMA_P3_5_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x35) |
|
#define | SPIMSP432DMA_P3_5_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x35) |
|
#define | SPIMSP432DMA_P3_5_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x35) |
|
#define | SPIMSP432DMA_P3_5_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x35) |
|
#define | SPIMSP432DMA_P3_5_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x35) |
|
#define | SPIMSP432DMA_P3_5_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x35) |
|
#define | SPIMSP432DMA_P3_5_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x35) |
|
#define | SPIMSP432DMA_P3_5_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x35) |
|
#define | SPIMSP432DMA_P3_5_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x35) |
|
#define | SPIMSP432DMA_P3_5_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x35) |
|
#define | SPIMSP432DMA_P3_5_UCA1STE ((PMAP_UCA1STE << 10) | 0x35) |
|
#define | SPIMSP432DMA_P3_5_UCA2STE ((PMAP_UCA2STE << 10) | 0x35) |
|
#define | SPIMSP432DMA_P3_5_UCB2STE ((PMAP_UCB2STE << 10) | 0x35) |
|
#define | SPIMSP432DMA_P3_6_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x36) |
|
#define | SPIMSP432DMA_P3_6_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x36) |
|
#define | SPIMSP432DMA_P3_6_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x36) |
|
#define | SPIMSP432DMA_P3_6_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x36) |
|
#define | SPIMSP432DMA_P3_6_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x36) |
|
#define | SPIMSP432DMA_P3_6_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x36) |
|
#define | SPIMSP432DMA_P3_6_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x36) |
|
#define | SPIMSP432DMA_P3_6_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x36) |
|
#define | SPIMSP432DMA_P3_6_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x36) |
|
#define | SPIMSP432DMA_P3_6_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x36) |
|
#define | SPIMSP432DMA_P3_6_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x36) |
|
#define | SPIMSP432DMA_P3_6_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x36) |
|
#define | SPIMSP432DMA_P3_6_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x36) |
|
#define | SPIMSP432DMA_P3_6_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x36) |
|
#define | SPIMSP432DMA_P3_6_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x36) |
|
#define | SPIMSP432DMA_P3_6_UCA1STE ((PMAP_UCA1STE << 10) | 0x36) |
|
#define | SPIMSP432DMA_P3_6_UCA2STE ((PMAP_UCA2STE << 10) | 0x36) |
|
#define | SPIMSP432DMA_P3_6_UCB2STE ((PMAP_UCB2STE << 10) | 0x36) |
|
#define | SPIMSP432DMA_P3_7_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x37) |
|
#define | SPIMSP432DMA_P3_7_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x37) |
|
#define | SPIMSP432DMA_P3_7_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x37) |
|
#define | SPIMSP432DMA_P3_7_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x37) |
|
#define | SPIMSP432DMA_P3_7_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x37) |
|
#define | SPIMSP432DMA_P3_7_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x37) |
|
#define | SPIMSP432DMA_P3_7_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x37) |
|
#define | SPIMSP432DMA_P3_7_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x37) |
|
#define | SPIMSP432DMA_P3_7_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x37) |
|
#define | SPIMSP432DMA_P3_7_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x37) |
|
#define | SPIMSP432DMA_P3_7_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x37) |
|
#define | SPIMSP432DMA_P3_7_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x37) |
|
#define | SPIMSP432DMA_P3_7_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x37) |
|
#define | SPIMSP432DMA_P3_7_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x37) |
|
#define | SPIMSP432DMA_P3_7_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x37) |
|
#define | SPIMSP432DMA_P3_7_UCA1STE ((PMAP_UCA1STE << 10) | 0x37) |
|
#define | SPIMSP432DMA_P3_7_UCA2STE ((PMAP_UCA2STE << 10) | 0x37) |
|
#define | SPIMSP432DMA_P3_7_UCB2STE ((PMAP_UCB2STE << 10) | 0x37) |
|
#define | SPIMSP432DMA_P6_2_UCB1STE 0x00000162 /* Primary, port 6, pin 2 */ |
|
#define | SPIMSP432DMA_P6_3_UCB1CLK 0x00000163 /* Primary, port 6, pin 3 */ |
|
#define | SPIMSP432DMA_P6_4_UCB1SIMO 0x00000164 /* Primary, port 6, pin 4 */ |
|
#define | SPIMSP432DMA_P6_5_UCB1SOMI 0x00000165 /* Primary, port 6, pin 5 */ |
|
#define | SPIMSP432DMA_P6_6_UCB3SIMO 0x00000266 /* Secondary, port 6, pin 6 */ |
|
#define | SPIMSP432DMA_P6_7_UCB3SOMI 0x00000267 /* Secondary, port 6, pin 7 */ |
|
#define | SPIMSP432DMA_P7_0_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x70) |
|
#define | SPIMSP432DMA_P7_0_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x70) |
|
#define | SPIMSP432DMA_P7_0_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x70) |
|
#define | SPIMSP432DMA_P7_0_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x70) |
|
#define | SPIMSP432DMA_P7_0_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x70) |
|
#define | SPIMSP432DMA_P7_0_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x70) |
|
#define | SPIMSP432DMA_P7_0_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x70) |
|
#define | SPIMSP432DMA_P7_0_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x70) |
|
#define | SPIMSP432DMA_P7_0_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x70) |
|
#define | SPIMSP432DMA_P7_0_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x70) |
|
#define | SPIMSP432DMA_P7_0_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x70) |
|
#define | SPIMSP432DMA_P7_0_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x70) |
|
#define | SPIMSP432DMA_P7_0_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x70) |
|
#define | SPIMSP432DMA_P7_0_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x70) |
|
#define | SPIMSP432DMA_P7_0_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x70) |
|
#define | SPIMSP432DMA_P7_0_UCA1STE ((PMAP_UCA1STE << 10) | 0x70) |
|
#define | SPIMSP432DMA_P7_0_UCA2STE ((PMAP_UCA2STE << 10) | 0x70) |
|
#define | SPIMSP432DMA_P7_0_UCB2STE ((PMAP_UCB2STE << 10) | 0x70) |
|
#define | SPIMSP432DMA_P7_1_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x71) |
|
#define | SPIMSP432DMA_P7_1_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x71) |
|
#define | SPIMSP432DMA_P7_1_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x71) |
|
#define | SPIMSP432DMA_P7_1_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x71) |
|
#define | SPIMSP432DMA_P7_1_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x71) |
|
#define | SPIMSP432DMA_P7_1_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x71) |
|
#define | SPIMSP432DMA_P7_1_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x71) |
|
#define | SPIMSP432DMA_P7_1_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x71) |
|
#define | SPIMSP432DMA_P7_1_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x71) |
|
#define | SPIMSP432DMA_P7_1_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x71) |
|
#define | SPIMSP432DMA_P7_1_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x71) |
|
#define | SPIMSP432DMA_P7_1_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x71) |
|
#define | SPIMSP432DMA_P7_1_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x71) |
|
#define | SPIMSP432DMA_P7_1_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x71) |
|
#define | SPIMSP432DMA_P7_1_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x71) |
|
#define | SPIMSP432DMA_P7_1_UCA1STE ((PMAP_UCA1STE << 10) | 0x71) |
|
#define | SPIMSP432DMA_P7_1_UCA2STE ((PMAP_UCA2STE << 10) | 0x71) |
|
#define | SPIMSP432DMA_P7_1_UCB2STE ((PMAP_UCB2STE << 10) | 0x71) |
|
#define | SPIMSP432DMA_P7_2_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x72) |
|
#define | SPIMSP432DMA_P7_2_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x72) |
|
#define | SPIMSP432DMA_P7_2_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x72) |
|
#define | SPIMSP432DMA_P7_2_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x72) |
|
#define | SPIMSP432DMA_P7_2_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x72) |
|
#define | SPIMSP432DMA_P7_2_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x72) |
|
#define | SPIMSP432DMA_P7_2_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x72) |
|
#define | SPIMSP432DMA_P7_2_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x72) |
|
#define | SPIMSP432DMA_P7_2_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x72) |
|
#define | SPIMSP432DMA_P7_2_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x72) |
|
#define | SPIMSP432DMA_P7_2_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x72) |
|
#define | SPIMSP432DMA_P7_2_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x72) |
|
#define | SPIMSP432DMA_P7_2_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x72) |
|
#define | SPIMSP432DMA_P7_2_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x72) |
|
#define | SPIMSP432DMA_P7_2_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x72) |
|
#define | SPIMSP432DMA_P7_2_UCA1STE ((PMAP_UCA1STE << 10) | 0x72) |
|
#define | SPIMSP432DMA_P7_2_UCA2STE ((PMAP_UCA2STE << 10) | 0x72) |
|
#define | SPIMSP432DMA_P7_2_UCB2STE ((PMAP_UCB2STE << 10) | 0x72) |
|
#define | SPIMSP432DMA_P7_3_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x73) |
|
#define | SPIMSP432DMA_P7_3_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x73) |
|
#define | SPIMSP432DMA_P7_3_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x73) |
|
#define | SPIMSP432DMA_P7_3_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x73) |
|
#define | SPIMSP432DMA_P7_3_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x73) |
|
#define | SPIMSP432DMA_P7_3_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x73) |
|
#define | SPIMSP432DMA_P7_3_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x73) |
|
#define | SPIMSP432DMA_P7_3_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x73) |
|
#define | SPIMSP432DMA_P7_3_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x73) |
|
#define | SPIMSP432DMA_P7_3_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x73) |
|
#define | SPIMSP432DMA_P7_3_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x73) |
|
#define | SPIMSP432DMA_P7_3_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x73) |
|
#define | SPIMSP432DMA_P7_3_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x73) |
|
#define | SPIMSP432DMA_P7_3_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x73) |
|
#define | SPIMSP432DMA_P7_3_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x73) |
|
#define | SPIMSP432DMA_P7_3_UCA1STE ((PMAP_UCA1STE << 10) | 0x73) |
|
#define | SPIMSP432DMA_P7_3_UCA2STE ((PMAP_UCA2STE << 10) | 0x73) |
|
#define | SPIMSP432DMA_P7_3_UCB2STE ((PMAP_UCB2STE << 10) | 0x73) |
|
#define | SPIMSP432DMA_P7_4_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x74) |
|
#define | SPIMSP432DMA_P7_4_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x74) |
|
#define | SPIMSP432DMA_P7_4_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x74) |
|
#define | SPIMSP432DMA_P7_4_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x74) |
|
#define | SPIMSP432DMA_P7_4_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x74) |
|
#define | SPIMSP432DMA_P7_4_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x74) |
|
#define | SPIMSP432DMA_P7_4_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x74) |
|
#define | SPIMSP432DMA_P7_4_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x74) |
|
#define | SPIMSP432DMA_P7_4_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x74) |
|
#define | SPIMSP432DMA_P7_4_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x74) |
|
#define | SPIMSP432DMA_P7_4_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x74) |
|
#define | SPIMSP432DMA_P7_4_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x74) |
|
#define | SPIMSP432DMA_P7_4_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x74) |
|
#define | SPIMSP432DMA_P7_4_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x74) |
|
#define | SPIMSP432DMA_P7_4_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x74) |
|
#define | SPIMSP432DMA_P7_4_UCA1STE ((PMAP_UCA1STE << 10) | 0x74) |
|
#define | SPIMSP432DMA_P7_4_UCA2STE ((PMAP_UCA2STE << 10) | 0x74) |
|
#define | SPIMSP432DMA_P7_4_UCB2STE ((PMAP_UCB2STE << 10) | 0x74) |
|
#define | SPIMSP432DMA_P7_5_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x75) |
|
#define | SPIMSP432DMA_P7_5_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x75) |
|
#define | SPIMSP432DMA_P7_5_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x75) |
|
#define | SPIMSP432DMA_P7_5_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x75) |
|
#define | SPIMSP432DMA_P7_5_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x75) |
|
#define | SPIMSP432DMA_P7_5_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x75) |
|
#define | SPIMSP432DMA_P7_5_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x75) |
|
#define | SPIMSP432DMA_P7_5_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x75) |
|
#define | SPIMSP432DMA_P7_5_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x75) |
|
#define | SPIMSP432DMA_P7_5_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x75) |
|
#define | SPIMSP432DMA_P7_5_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x75) |
|
#define | SPIMSP432DMA_P7_5_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x75) |
|
#define | SPIMSP432DMA_P7_5_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x75) |
|
#define | SPIMSP432DMA_P7_5_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x75) |
|
#define | SPIMSP432DMA_P7_5_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x75) |
|
#define | SPIMSP432DMA_P7_5_UCA1STE ((PMAP_UCA1STE << 10) | 0x75) |
|
#define | SPIMSP432DMA_P7_5_UCA2STE ((PMAP_UCA2STE << 10) | 0x75) |
|
#define | SPIMSP432DMA_P7_5_UCB2STE ((PMAP_UCB2STE << 10) | 0x75) |
|
#define | SPIMSP432DMA_P7_6_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x76) |
|
#define | SPIMSP432DMA_P7_6_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x76) |
|
#define | SPIMSP432DMA_P7_6_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x76) |
|
#define | SPIMSP432DMA_P7_6_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x76) |
|
#define | SPIMSP432DMA_P7_6_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x76) |
|
#define | SPIMSP432DMA_P7_6_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x76) |
|
#define | SPIMSP432DMA_P7_6_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x76) |
|
#define | SPIMSP432DMA_P7_6_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x76) |
|
#define | SPIMSP432DMA_P7_6_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x76) |
|
#define | SPIMSP432DMA_P7_6_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x76) |
|
#define | SPIMSP432DMA_P7_6_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x76) |
|
#define | SPIMSP432DMA_P7_6_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x76) |
|
#define | SPIMSP432DMA_P7_6_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x76) |
|
#define | SPIMSP432DMA_P7_6_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x76) |
|
#define | SPIMSP432DMA_P7_6_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x76) |
|
#define | SPIMSP432DMA_P7_6_UCA1STE ((PMAP_UCA1STE << 10) | 0x76) |
|
#define | SPIMSP432DMA_P7_6_UCA2STE ((PMAP_UCA2STE << 10) | 0x76) |
|
#define | SPIMSP432DMA_P7_6_UCB2STE ((PMAP_UCB2STE << 10) | 0x76) |
|
#define | SPIMSP432DMA_P7_7_UCA0CLK ((PMAP_UCA0CLK << 10) | 0x77) |
|
#define | SPIMSP432DMA_P7_7_UCA0SIMO ((PMAP_UCA0SIMO << 10) | 0x77) |
|
#define | SPIMSP432DMA_P7_7_UCA0SOMI ((PMAP_UCA0SOMI << 10) | 0x77) |
|
#define | SPIMSP432DMA_P7_7_UCA1CLK ((PMAP_UCA1CLK << 10) | 0x77) |
|
#define | SPIMSP432DMA_P7_7_UCA1SIMO ((PMAP_UCA1SIMO << 10) | 0x77) |
|
#define | SPIMSP432DMA_P7_7_UCA1SOMI ((PMAP_UCA1SOMI << 10) | 0x77) |
|
#define | SPIMSP432DMA_P7_7_UCA2CLK ((PMAP_UCA2CLK << 10) | 0x77) |
|
#define | SPIMSP432DMA_P7_7_UCA2SIMO ((PMAP_UCA2SIMO << 10) | 0x77) |
|
#define | SPIMSP432DMA_P7_7_UCA2SOMI ((PMAP_UCA2SOMI << 10) | 0x77) |
|
#define | SPIMSP432DMA_P7_7_UCB0CLK ((PMAP_UCB0CLK << 10) | 0x77) |
|
#define | SPIMSP432DMA_P7_7_UCB0SIMO ((PMAP_UCB0SIMO << 10) | 0x77) |
|
#define | SPIMSP432DMA_P7_7_UCB0SOMI ((PMAP_UCB0SOMI << 10) | 0x77) |
|
#define | SPIMSP432DMA_P7_7_UCB2CLK ((PMAP_UCB2CLK << 10) | 0x77) |
|
#define | SPIMSP432DMA_P7_7_UCB2SIMO ((PMAP_UCB2SIMO << 10) | 0x77) |
|
#define | SPIMSP432DMA_P7_7_UCB2SOMI ((PMAP_UCB2SOMI << 10) | 0x77) |
|
#define | SPIMSP432DMA_P7_7_UCA1STE ((PMAP_UCA1STE << 10) | 0x77) |
|
#define | SPIMSP432DMA_P7_7_UCA2STE ((PMAP_UCA2STE << 10) | 0x77) |
|
#define | SPIMSP432DMA_P7_7_UCB2STE ((PMAP_UCB2STE << 10) | 0x77) |
|
#define | SPIMSP432DMA_P8_0_UCB3STE 0x00000180 /* Primary, port 8, pin 0 */ |
|
#define | SPIMSP432DMA_P8_1_UCB3CLK 0x00000181 /* Primary, port 8, pin 1 */ |
|
#define | SPIMSP432DMA_P9_4_UCA3STE 0x00000194 /* Primary, port 9, pin 4 */ |
|
#define | SPIMSP432DMA_P9_5_UCA3CLK 0x00000195 /* Primary, port 9, pin 5 */ |
|
#define | SPIMSP432DMA_P9_6_UCA3SOMI 0x00000196 /* Primary, port 9, pin 6 */ |
|
#define | SPIMSP432DMA_P9_7_UCA3SIMO 0x00000197 /* Primary, port 9, pin 7 */ |
|
#define | SPIMSP432DMA_P10_0_UCB3STE 0x000001A0 /* Primary, port 10, pin 0 */ |
|
#define | SPIMSP432DMA_P10_1_UCB3CLK 0x000001A1 /* Primary, port 10, pin 1 */ |
|
#define | SPIMSP432DMA_P10_2_UCB3SIMO 0x000001A2 /* Primary, port 10, pin 2 */ |
|
#define | SPIMSP432DMA_P10_3_UCB3SOMI 0x000001A3 /* Primary, port 10, pin 3 */ |
|