![]() |
![]() |
The following is a reference of all LZ4 compression and decompression API's available for the application to use. More...
Data Structures | |
| struct | LZ4_compressParams |
| Compression parameters for a LZ4 frame. More... | |
| struct | LZ4_compressBlockParams |
| Compression parameters for a single LZ4 block. More... | |
| struct | LZ4_decompressParams |
| Decompression parameters for a LZ4 frame. More... | |
| struct | LZ4_decompressBlockParams |
| Decompression parameters for a single LZ4 block. More... | |
| struct | LZ4_streamDecompressBlockState |
| Decompression state for a streaming LZ4 block. More... | |
| struct | LZ4_streamDecompressBlockParams |
| Decompression parameters for a streaming LZ4 block. More... | |
Macros | |
| #define | LZ4_COMPRESS_MAX_SIZE(n) ((size_t)((float)n * 1.01) + 27) |
| Maximum size of a compressed file, one percent plus 27 bytes larger than uncompressed data. More... | |
| #define | LZ4_MAGIC_NUMBER 0x184d2204 |
| #define | LZ4_MAX_BLOCK_SIZE 0x00100000 |
| #define | LZ4_FLG_VERSION 0x40 |
| #define | LZ4_FLG_BLOCK_INDEP 0x20 |
| #define | LZ4_FLG_BLOCK_CHECKSUM 0x10 |
| #define | LZ4_FLG_CONTENT_SIZE 0x08 |
| #define | LZ4_FLG_CONTENT_CHECKSUM 0x04 |
| #define | LZ4_BD_BYTE 0x70 |
| #define | LZ4_MIN_MATCH 4 |
| #define | LZ4_LAST_MATCH_DIST 12 |
| #define | LZ4_LAST_LITERAL_LENGTH 5 |
| #define | LZ4_TOKEN_LITERAL_MASK 0xf0 |
| #define | LZ4_TOKEN_MATCH_MASK 0x0f |
| #define | LZ4_HASH_VALUE 0x9E3779B1 |
Typedefs | |
| typedef struct LZ4_compressParams | LZ4_compressParams |
| Compression parameters for a LZ4 frame. More... | |
| typedef struct LZ4_compressBlockParams | LZ4_compressBlockParams |
| Compression parameters for a single LZ4 block. More... | |
| typedef struct LZ4_decompressParams | LZ4_decompressParams |
| Decompression parameters for a LZ4 frame. More... | |
| typedef struct LZ4_decompressBlockParams | LZ4_decompressBlockParams |
| Decompression parameters for a single LZ4 block. More... | |
| typedef struct LZ4_streamDecompressBlockState | LZ4_streamDecompressBlockState |
| Decompression state for a streaming LZ4 block. More... | |
| typedef struct LZ4_streamDecompressBlockParams | LZ4_streamDecompressBlockParams |
| Decompression parameters for a streaming LZ4 block. More... | |
Enumerations | |
| enum | LZ4_status { LZ4_SUCCESS, LZ4_PARTIAL_SUCCESS, LZ4_NO_CONTENT_SIZE, LZ4_FRAMING_ERROR, LZ4_BLOCK_CHECKSUM_ERROR, LZ4_CONTENT_CHECKSUM_ERROR } |
| LZ4 status return types. More... | |
| enum | LZ4_streamState { LZ4_BLOCK_SIZE, LZ4_TOKEN, LZ4_LITERAL_LENGTH, LZ4_LITERAL, LZ4_MATCH_LENGTH, LZ4_MATCH_OFFSET_LOW, LZ4_MATCH_OFFSET_HIGH } |
| LZ4 streaming API state. More... | |
Functions | |
| uint32_t | LZ4_compress (const LZ4_compressParams *params, LZ4_status *status) |
| Compress a block of data to a LZ4 frame. More... | |
| uint32_t | LZ4_compressBlock (const LZ4_compressBlockParams *params, LZ4_status *status) |
| Compress a block of data to a single LZ4 block without framing. More... | |
| uint32_t | LZ4_decompress (const LZ4_decompressParams *params, LZ4_status *status) |
| Decompress a LZ4 frame to a block of data. More... | |
| uint32_t | LZ4_decompressBlock (const LZ4_decompressBlockParams *params, LZ4_status *status) |
| Decompress a single LZ4 block without framing to a block of data. More... | |
| uint32_t | LZ4_getContentSize (const uint8_t *src, LZ4_status *status) |
| Get the content size of a compressed LZ4 frame. More... | |
| void | LZ4_streamDecompressBlockInit (const LZ4_streamDecompressBlockParams *params, LZ4_streamDecompressBlockState *state, LZ4_status *status) |
| Initialize LZ4 stream decompression. More... | |
| uint32_t | LZ4_streamDecompressBlock (LZ4_streamDecompressBlockState *state, const void *data, uint16_t length, LZ4_status *status) |
| Decompress a single LZ4 block as a stream of data. More... | |
The following is a reference of all LZ4 compression and decompression API's available for the application to use.
The LZ4 API set includes both compression and decompression APIs that can be called directly from the main application.
| #define LZ4_COMPRESS_MAX_SIZE | ( | n | ) | ((size_t)((float)n * 1.01) + 27) |
Maximum size of a compressed file, one percent plus 27 bytes larger than uncompressed data.
| #define LZ4_MAGIC_NUMBER 0x184d2204 |
| #define LZ4_MAX_BLOCK_SIZE 0x00100000 |
| #define LZ4_FLG_VERSION 0x40 |
| #define LZ4_FLG_BLOCK_INDEP 0x20 |
| #define LZ4_FLG_BLOCK_CHECKSUM 0x10 |
| #define LZ4_FLG_CONTENT_SIZE 0x08 |
| #define LZ4_FLG_CONTENT_CHECKSUM 0x04 |
| #define LZ4_BD_BYTE 0x70 |
| #define LZ4_MIN_MATCH 4 |
Referenced by LZ4_streamDecompressBlock().
| #define LZ4_LAST_MATCH_DIST 12 |
Referenced by LZ4_compressBlock().
| #define LZ4_LAST_LITERAL_LENGTH 5 |
| #define LZ4_TOKEN_LITERAL_MASK 0xf0 |
Referenced by LZ4_streamDecompressBlock().
| #define LZ4_TOKEN_MATCH_MASK 0x0f |
Referenced by LZ4_streamDecompressBlock().
| #define LZ4_HASH_VALUE 0x9E3779B1 |
| typedef struct LZ4_compressParams LZ4_compressParams |
Compression parameters for a LZ4 frame.
| typedef struct LZ4_compressBlockParams LZ4_compressBlockParams |
Compression parameters for a single LZ4 block.
| typedef struct LZ4_decompressParams LZ4_decompressParams |
Decompression parameters for a LZ4 frame.
| typedef struct LZ4_decompressBlockParams LZ4_decompressBlockParams |
Decompression parameters for a single LZ4 block.
| typedef struct LZ4_streamDecompressBlockState LZ4_streamDecompressBlockState |
Decompression state for a streaming LZ4 block.
| typedef struct LZ4_streamDecompressBlockParams LZ4_streamDecompressBlockParams |
Decompression parameters for a streaming LZ4 block.
| enum LZ4_status |
LZ4 status return types.
| enum LZ4_streamState |
LZ4 streaming API state.
| uint32_t LZ4_compress | ( | const LZ4_compressParams * | params, |
| LZ4_status * | status | ||
| ) |
Compress a block of data to a LZ4 frame.
Compress a block of data using LZ4 compression and add LZ4 framing. This API will compress data to a valid LZ4 file and contains several parameters to enable or disable features of the LZ4 framing specification such as content and block checksum using the xxHash algorithm or block size. See the LZ4_compressParams structure documentation for more details about the available parameters.
A block compressed with this method can be saved as a binary .lz4 file and extracted using the LZ4 command line utility.
| params | Pointer to the LZ4 compression parameter structure. |
| status | Pointer to a LZ4 status that will contain the result status. |
References LZ4_compressParams::dst, and LZ4_compressParams::src.
| uint32_t LZ4_compressBlock | ( | const LZ4_compressBlockParams * | params, |
| LZ4_status * | status | ||
| ) |
Compress a block of data to a single LZ4 block without framing.
Compress a block of data using only LZ4 compression and block format. This API can be used to compress data and create a custom framing scheme using an alternative checksum method. The LZ4 block format has a single parameter for enabling block checksum computation with the xxHash algorithm. The block checksum is computed on the compressed data block. See the LZ4_compressBlockParams structure documentation for more details about the available parameters.
| params | Pointer to the LZ4 compression block parameter structure. |
| status | Pointer to a LZ4 status that will contain the result status. |
References LZ4_compressBlockParams::dst, LZ4_compressBlockParams::hashLog2Size, LZ4_compressBlockParams::hashTable, LZ4_compressBlockParams::length, LZ4_LAST_MATCH_DIST, and LZ4_compressBlockParams::src.
| uint32_t LZ4_decompress | ( | const LZ4_decompressParams * | params, |
| LZ4_status * | status | ||
| ) |
Decompress a LZ4 frame to a block of data.
Decompress a LZ4 frame to an uncompressed data block. This API contains parameters to enable checking of content and block checksum. When enabled the xxHash algorithm is used to verify the checksum. While not required it is the application programmers responsibility to determine if validating the checksum is necessary. See the LZ4_decompressParams structure documentation for more details about the available parameters.
A .lz4 file compressed with the LZ4 command line utility can be decompressed using this API.
| params | Pointer to the LZ4 decompression parameter structure. |
| status | Pointer to a LZ4 status that will contain the result status. |
References LZ4_decompressParams::dst, LZ4_decompressParams::dstLength, and LZ4_decompressParams::src.
| uint32_t LZ4_decompressBlock | ( | const LZ4_decompressBlockParams * | params, |
| LZ4_status * | status | ||
| ) |
Decompress a single LZ4 block without framing to a block of data.
Decompress a LZ4 block to an uncompressed data block. This API contains a single parameter to enable checking of the block checksum. When enabled the xxHash algorithm is used to verify the checksum. While not required it is the application programmers responsibility to determine if validating the checksum is necessary. See the LZ4_decompressBlockParams structure documentation for more details about the available parameters.
| params | Pointer to the LZ4 decompression block parameter structure. |
| status | Pointer to a LZ4 status that will contain the result status. |
References LZ4_decompressBlockParams::dst, LZ4_decompressBlockParams::dstLength, and LZ4_decompressBlockParams::src.
| uint32_t LZ4_getContentSize | ( | const uint8_t * | src, |
| LZ4_status * | status | ||
| ) |
Get the content size of a compressed LZ4 frame.
Get the size of the original uncompressed data block if it is present. The content size is an optional parameter when compressing but it is recommended to enable it and verify the uncompressed data block fits in the allocated buffer before decompressing.
| src | Pointer to the LZ4 frame. |
| status | Pointer to a LZ4 status that will contain the result status. |
| void LZ4_streamDecompressBlockInit | ( | const LZ4_streamDecompressBlockParams * | params, |
| LZ4_streamDecompressBlockState * | state, | ||
| LZ4_status * | status | ||
| ) |
Initialize LZ4 stream decompression.
Initialize LZ4 decompression using a stream of data blocks. The streaming API's can be used when data is sent in chunks such as over-the-air or wired serial communication and removes the need to buffer then entire compressed data before running decompression, reducing total system memory used.
This function must be first called to initialize the state before calling LZ4_streamDecompressBlock() to decompress data.
| params | Pointer to the LZ4 decompression strean parameter structure. |
| state | Pointer to the LZ4 decompression stream state. |
| status | Pointer to a LZ4 status that will contain the result status. |
References LZ4_streamDecompressBlockParams::containsBlockSize, LZ4_streamDecompressBlockParams::dst, LZ4_streamDecompressBlockState::dstLength, LZ4_streamDecompressBlockParams::dstLength, LZ4_streamDecompressBlockState::dstOrigin, LZ4_streamDecompressBlockState::dstPtr, LZ4_streamDecompressBlockState::literalLength, LZ4_BLOCK_SIZE, LZ4_SUCCESS, LZ4_TOKEN, LZ4_streamDecompressBlockState::matchLength, LZ4_streamDecompressBlockState::matchOffset, and LZ4_streamDecompressBlockState::state.
| uint32_t LZ4_streamDecompressBlock | ( | LZ4_streamDecompressBlockState * | state, |
| const void * | data, | ||
| uint16_t | length, | ||
| LZ4_status * | status | ||
| ) |
Decompress a single LZ4 block as a stream of data.
Continue decompression using a stream of data blocks. The streaming API's can be used when data is sent in chunks such as over-the-air or wired serial communication and removes the need to buffer then entire compressed data before running decompression, reducing total system memory used.
The LZ4_streamDecompressBlockInit() function must first be called to initialize the state before decompressing data.
| state | Pointer to the LZ4 decompression stream state. |
| data | Pointer to a block of data to continue decompression with. |
| length | Length of data block in bytes. |
| status | Pointer to a LZ4 status that will contain the result status. |
References LZ4_streamDecompressBlockState::dstLength, LZ4_streamDecompressBlockState::dstOrigin, LZ4_streamDecompressBlockState::dstPtr, LZ4_streamDecompressBlockState::literalLength, LZ4_BLOCK_SIZE, LZ4_LITERAL, LZ4_LITERAL_LENGTH, LZ4_MATCH_LENGTH, LZ4_MATCH_OFFSET_HIGH, LZ4_MATCH_OFFSET_LOW, LZ4_MIN_MATCH, LZ4_PARTIAL_SUCCESS, LZ4_SUCCESS, LZ4_TOKEN, LZ4_TOKEN_LITERAL_MASK, LZ4_TOKEN_MATCH_MASK, LZ4_streamDecompressBlockState::matchLength, LZ4_streamDecompressBlockState::matchOffset, and LZ4_streamDecompressBlockState::state.