Logo
MSP Graphics Library
Rectangle_api

Functions

void Graphics_drawRectangle (const Graphics_Context *context, const Graphics_Rectangle *rect)
 
void Graphics_fillRectangle (const Graphics_Context *context, const Graphics_Rectangle *rect)
 
int32_t Graphics_isRectangleOverlap (Graphics_Rectangle *rect1, Graphics_Rectangle *rect2)
 
int32_t Graphics_getRectangleIntersection (Graphics_Rectangle *rect1, Graphics_Rectangle *rect2, Graphics_Rectangle *intersect)
 
bool Graphics_isPointWithinRectangle (const Graphics_Rectangle *rect, uint16_t x, uint16_t y)
 

Detailed Description

Function Documentation

void Graphics_drawRectangle ( const Graphics_Context *  context,
const Graphics_Rectangle *  rect 
)

Draws a rectangle.

Parameters
contextis a pointer to the drawing context to use.
rectis a pointer to the structure containing the extents of the rectangle.

This function draws a rectangle. The rectangle will extend from xMin to xMax and yMin to yMax, inclusive.

Returns
None.
void Graphics_fillRectangle ( const Graphics_Context *  context,
const Graphics_Rectangle *  rect 
)

Draws a filled rectangle.

Parameters
contextis a pointer to the drawing context to use.
rectis a pointer to the structure containing the extents of the rectangle.

This function draws a filled rectangle. The rectangle will extend from xMin to xMax and yMin to yMax, inclusive. The clipping of the rectangle to the clipping rectangle is performed within this routine; the display driver's rectangle fill routine is used to perform the actual rectangle fill.

Returns
None.
int32_t Graphics_getRectangleIntersection ( Graphics_Rectangle *  rect1,
Graphics_Rectangle *  rect2,
Graphics_Rectangle *  intersect 
)

Determines the intersection of two rectangles.

Parameters
rect1is a pointer to the first rectangle.
rect2is a pointer to the second rectangle.
intersectis a pointer to a rectangle which will be written with the intersection of rect1 and rect2.

This function determines if two rectangles overlap and, if they do, calculates the rectangle representing their intersection. If the rectangles do not overlap, 0 is returned and intersect is not written.

Returns
Returns 1 if there is an overlap or 0 if not.
bool Graphics_isPointWithinRectangle ( const Graphics_Rectangle *  rect,
uint16_t  x,
uint16_t  y 
)

Determines if a point lies within a given rectangle.

Parameters
rectis a pointer to the rectangle which the point is to be checked against.
xis the X coordinate of the point to be checked.
yis the Y coordinate of the point to be checked.

This function determines whether point (x, y) lies within the rectangle described by rect.

Returns
Returns 1 if the point is within the rectangle or 0 otherwise.
int32_t Graphics_isRectangleOverlap ( Graphics_Rectangle *  rect1,
Graphics_Rectangle *  rect2 
)

Determines if two rectangles overlap.

Parameters
rect1is a pointer to the first rectangle.
rect2is a pointer to the second rectangle.

This function determines whether two rectangles overlap. It assumes that rectangles rect1 and rect2 are valid with xMin < xMax and yMin < yMax.

Returns
Returns 1 if there is an overlap or 0 if not.