Data Fields
_Timer_A_UpDownModeConfig Struct Reference

Type definition for _Timer_A_UpDownModeConfig structure. More...

#include <timer_a.h>

Data Fields

uint_fast16_t clockSource
 
uint_fast16_t clockSourceDivider
 
uint_fast16_t timerPeriod
 
uint_fast16_t timerInterruptEnable_TAIE
 
uint_fast16_t captureCompareInterruptEnable_CCR0_CCIE
 
uint_fast16_t timerClear
 

Detailed Description

Type definition for _Timer_A_UpDownModeConfig structure.

ypedef Timer_A_UpDownModeConfig

Configuration structure for UpDown mode in the Timer_A module. See Timer_A_configureUpDownMode for parameter documentation.

Field Documentation

uint_fast16_t _Timer_A_UpDownModeConfig::clockSource
uint_fast16_t _Timer_A_UpDownModeConfig::clockSourceDivider
uint_fast16_t _Timer_A_UpDownModeConfig::timerPeriod
uint_fast16_t _Timer_A_UpDownModeConfig::timerInterruptEnable_TAIE
uint_fast16_t _Timer_A_UpDownModeConfig::captureCompareInterruptEnable_CCR0_CCIE
uint_fast16_t _Timer_A_UpDownModeConfig::timerClear

The documentation for this struct was generated from the following file:

Copyright 2017, Texas Instruments Incorporated