Data Structures | Macros | Typedefs | Functions
DMA

Configures and controls MSP432's DMA controller which is built around ARM's uDMA controller. More...

Data Structures

struct  _DMA_ControlTable
 

Macros

#define DMA_TaskStructEntry(transferCount,itemSize,srcIncrement,srcAddr,dstIncrement,dstAddr,arbSize,mode)
 
#define UDMA_ATTR_USEBURST   0x00000001
 
#define UDMA_ATTR_ALTSELECT   0x00000002
 
#define UDMA_ATTR_HIGH_PRIORITY   0x00000004
 
#define UDMA_ATTR_REQMASK   0x00000008
 
#define UDMA_ATTR_ALL   0x0000000F
 
#define UDMA_MODE_STOP   0x00000000
 
#define UDMA_MODE_BASIC   0x00000001
 
#define UDMA_MODE_AUTO   0x00000002
 
#define UDMA_MODE_PINGPONG   0x00000003
 
#define UDMA_MODE_MEM_SCATTER_GATHER   0x00000004
 
#define UDMA_MODE_PER_SCATTER_GATHER   0x00000006
 
#define UDMA_MODE_ALT_SELECT   0x00000001
 
#define UDMA_DST_INC_8   0x00000000
 
#define UDMA_DST_INC_16   0x40000000
 
#define UDMA_DST_INC_32   0x80000000
 
#define UDMA_DST_INC_NONE   0xc0000000
 
#define UDMA_SRC_INC_8   0x00000000
 
#define UDMA_SRC_INC_16   0x04000000
 
#define UDMA_SRC_INC_32   0x08000000
 
#define UDMA_SRC_INC_NONE   0x0c000000
 
#define UDMA_SIZE_8   0x00000000
 
#define UDMA_SIZE_16   0x11000000
 
#define UDMA_SIZE_32   0x22000000
 
#define UDMA_DST_PROT_PRIV   0x00200000
 
#define UDMA_SRC_PROT_PRIV   0x00040000
 
#define UDMA_ARB_1   0x00000000
 
#define UDMA_ARB_2   0x00004000
 
#define UDMA_ARB_4   0x00008000
 
#define UDMA_ARB_8   0x0000c000
 
#define UDMA_ARB_16   0x00010000
 
#define UDMA_ARB_32   0x00014000
 
#define UDMA_ARB_64   0x00018000
 
#define UDMA_ARB_128   0x0001c000
 
#define UDMA_ARB_256   0x00020000
 
#define UDMA_ARB_512   0x00024000
 
#define UDMA_ARB_1024   0x00028000
 
#define UDMA_NEXT_USEBURST   0x00000008
 
#define UDMA_PRI_SELECT   0x00000000
 
#define UDMA_ALT_SELECT   0x00000008
 
#define DMA_CH0_RESERVED0   0x00000000
 
#define DMA_CH0_EUSCIA0TX   0x01000000
 
#define DMA_CH0_EUSCIB0TX0   0x02000000
 
#define DMA_CH0_EUSCIB3TX1   0x03000000
 
#define DMA_CH0_EUSCIB2TX2   0x04000000
 
#define DMA_CH0_EUSCIB1TX3   0x05000000
 
#define DMA_CH0_TIMERA0CCR0   0x06000000
 
#define DMA_CH0_AESTRIGGER0   0x07000000
 
#define DMA_CH1_RESERVED0   0x00000001
 
#define DMA_CH1_EUSCIA0RX   0x01000001
 
#define DMA_CH1_EUSCIB0RX0   0x02000001
 
#define DMA_CH1_EUSCIB3RX1   0x03000001
 
#define DMA_CH1_EUSCIB2RX2   0x04000001
 
#define DMA_CH1_EUSCIB1RX3   0x05000001
 
#define DMA_CH1_TIMERA0CCR2   0x06000001
 
#define DMA_CH1_AESTRIGGER1   0x07000001
 
#define DMA_CH2_RESERVED0   0x00000002
 
#define DMA_CH2_EUSCIA1TX   0x01000002
 
#define DMA_CH2_EUSCIB1TX0   0x02000002
 
#define DMA_CH2_EUSCIB0TX1   0x03000002
 
#define DMA_CH2_EUSCIB3TX2   0x04000002
 
#define DMA_CH2_EUSCIB2TX3   0x05000002
 
#define DMA_CH2_TIMERA1CCR0   0x06000002
 
#define DMA_CH2_AESTRIGGER2   0x07000002
 
#define DMA_CH3_RESERVED0   0x00000003
 
#define DMA_CH3_EUSCIA1RX   0x01000003
 
#define DMA_CH3_EUSCIB1RX0   0x02000003
 
#define DMA_CH3_EUSCIB0RX1   0x03000003
 
#define DMA_CH3_EUSCIB3RX2   0x04000003
 
#define DMA_CH3_EUSCIB2RX3   0x05000003
 
#define DMA_CH3_TIMERA1CCR2   0x06000003
 
#define DMA_CH3_RESERVED1   0x07000003
 
#define DMA_CH4_RESERVED0   0x00000004
 
#define DMA_CH4_EUSCIA2TX   0x01000004
 
#define DMA_CH4_EUSCIB2TX0   0x02000004
 
#define DMA_CH4_EUSCIB1TX1   0x03000004
 
#define DMA_CH4_EUSCIB0TX2   0x04000004
 
#define DMA_CH4_EUSCIB3TX3   0x05000004
 
#define DMA_CH4_TIMERA2CCR0   0x06000004
 
#define DMA_CH4_RESERVED1   0x07000004
 
#define DMA_CH5_RESERVED0   0x00000005
 
#define DMA_CH5_EUSCIA2RX   0x01000005
 
#define DMA_CH5_EUSCIB2RX0   0x02000005
 
#define DMA_CH5_EUSCIB1RX1   0x03000005
 
#define DMA_CH5_EUSCIB0RX2   0x04000005
 
#define DMA_CH5_EUSCIB3RX3   0x05000005
 
#define DMA_CH5_TIMERA2CCR2   0x06000005
 
#define DMA_CH5_RESERVED1   0x07000005
 
#define DMA_CH6_RESERVED0   0x00000006
 
#define DMA_CH6_EUSCIA3TX   0x01000006
 
#define DMA_CH6_EUSCIB3TX0   0x02000006
 
#define DMA_CH6_EUSCIB2TX1   0x03000006
 
#define DMA_CH6_EUSCIB1TX2   0x04000006
 
#define DMA_CH6_EUSCIB0TX3   0x05000006
 
#define DMA_CH6_TIMERA3CCR0   0x06000006
 
#define DMA_CH6_EXTERNALPIN   0x07000006
 
#define DMA_CH7_RESERVED0   0x00000007
 
#define DMA_CH7_EUSCIA3RX   0x01000007
 
#define DMA_CH7_EUSCIB3RX0   0x02000007
 
#define DMA_CH7_EUSCIB2RX1   0x03000007
 
#define DMA_CH7_EUSCIB1RX2   0x04000007
 
#define DMA_CH7_EUSCIB0RX3   0x05000007
 
#define DMA_CH7_TIMERA3CCR2   0x06000007
 
#define DMA_CH7_ADC14   0x07000007
 
#define DMA_INT0   INT_DMA_INT0
 
#define DMA_INT1   INT_DMA_INT1
 
#define DMA_INT2   INT_DMA_INT2
 
#define DMA_INT3   INT_DMA_INT3
 
#define DMA_INTERR   INT_DMA_ERR
 
#define DMA_CHANNEL_0   0
 
#define DMA_CHANNEL_1   1
 
#define DMA_CHANNEL_2   2
 
#define DMA_CHANNEL_3   3
 
#define DMA_CHANNEL_4   4
 
#define DMA_CHANNEL_5   5
 
#define DMA_CHANNEL_6   6
 
#define DMA_CHANNEL_7   7
 

Typedefs

typedef struct _DMA_ControlTable DMA_ControlTable
 

Functions

void DMA_enableModule (void)
 
void DMA_disableModule (void)
 
uint32_t DMA_getErrorStatus (void)
 
void DMA_clearErrorStatus (void)
 
void DMA_enableChannel (uint32_t channelNum)
 
void DMA_disableChannel (uint32_t channelNum)
 
bool DMA_isChannelEnabled (uint32_t channelNum)
 
void DMA_setControlBase (void *controlTable)
 
void * DMA_getControlBase (void)
 
void * DMA_getControlAlternateBase (void)
 
void DMA_requestChannel (uint32_t channelNum)
 
void DMA_enableChannelAttribute (uint32_t channelNum, uint32_t attr)
 
void DMA_disableChannelAttribute (uint32_t channelNum, uint32_t attr)
 
uint32_t DMA_getChannelAttribute (uint32_t channelNum)
 
void DMA_setChannelControl (uint32_t channelStructIndex, uint32_t control)
 
void DMA_setChannelTransfer (uint32_t channelStructIndex, uint32_t mode, void *srcAddr, void *dstAddr, uint32_t transferSize)
 
void DMA_setChannelScatterGather (uint32_t channelNum, uint32_t taskCount, void *taskList, uint32_t isPeriphSG)
 
uint32_t DMA_getChannelSize (uint32_t channelStructIndex)
 
uint32_t DMA_getChannelMode (uint32_t channelStructIndex)
 
void DMA_assignChannel (uint32_t mapping)
 
void DMA_requestSoftwareTransfer (uint32_t channel)
 
void DMA_assignInterrupt (uint32_t interruptNumber, uint32_t channel)
 
void DMA_enableInterrupt (uint32_t interruptNumber)
 
void DMA_disableInterrupt (uint32_t interruptNumber)
 
uint32_t DMA_getInterruptStatus (void)
 
void DMA_clearInterruptFlag (uint32_t channel)
 
void DMA_registerInterrupt (uint32_t interruptNumber, void(*intHandler)(void))
 
void DMA_unregisterInterrupt (uint32_t interruptNumber)
 

Detailed Description

Configures and controls MSP432's DMA controller which is built around ARM's uDMA controller.


Module Operation


The Micro Direct Memory Access (DMA) API provides functions to configure the MSP432 uDMA controller. The DMA controller is designed to work with the ARM Cortex-M processor and provides an efficient and low-overhead means of transferring blocks of data in the system.

The DMA controller has the following features:

The uDMA controller supports several different transfer modes, allowing for complex transfer schemes. The following transfer modes are provided:

Detailed explanation of the various transfer modes is beyond the scope of this document. Please refer to the device data sheet for more information on the operation of the uDMA controller.


Programming Example


The DriverLib package contains a variety of different code examples that demonstrate the usage of the DMA module. These code examples are accessible under the examples/ folder of the SDK release as well as through TI Resource Explorer if using Code Composer Studio. These code examples provide a comprehensive list of use cases as well as practical applications involving each module.

Below is a very brief example of how to configure the DMA controller to transfer from a data array (data_array) to the EUSCI I2C module to be sent over the I2C line. This is useful in the sense that the EUSCI module does not constantly have to wake up the CPU in order to load the next byte into the buffer.

Macro Definition Documentation

#define DMA_TaskStructEntry (   transferCount,
  itemSize,
  srcIncrement,
  srcAddr,
  dstIncrement,
  dstAddr,
  arbSize,
  mode 
)
Value:
{ \
(((srcIncrement) == UDMA_SRC_INC_NONE) ? (void *)(srcAddr) : \
((void *)(&((uint8_t *)(srcAddr))[((transferCount) << \
((srcIncrement) >> 26)) - 1]))), \
(((dstIncrement) == UDMA_DST_INC_NONE) ? (void *)(dstAddr) : \
((void *)(&((uint8_t *)(dstAddr))[((transferCount) << \
((dstIncrement) >> 30)) - 1]))), \
(srcIncrement) | (dstIncrement) | (itemSize) | (arbSize) | \
(((transferCount) - 1) << 4) | \
((((mode) == UDMA_MODE_MEM_SCATTER_GATHER) || \
(mode) | UDMA_MODE_ALT_SELECT : (mode)), 0 \
}
#define UDMA_MODE_MEM_SCATTER_GATHER
Definition: dma.h:200
#define UDMA_SRC_INC_NONE
Definition: dma.h:218
#define UDMA_MODE_PER_SCATTER_GATHER
Definition: dma.h:202
#define UDMA_DST_INC_NONE
Definition: dma.h:214
#define UDMA_MODE_ALT_SELECT
Definition: dma.h:204

A helper macro for building scatter-gather task table entries.

This macro is intended to be used to help populate a table of DMA tasks for a scatter-gather transfer. This macro will calculate the values for the fields of a task structure entry based on the input parameters.

There are specific requirements for the values of each parameter. No checking is done so it is up to the caller to ensure that correct values are used for the parameters.

The transferCount parameter is the number of items that will be transferred by this task. It must be in the range 1-1024.

The itemSize parameter is the bit size of the transfer data. It must be one of UDMA_SIZE_8, UDMA_SIZE_16, or UDMA_SIZE_32.

The srcIncrement parameter is the increment size for the source data. It must be one of UDMA_SRC_INC_8, UDMA_SRC_INC_16, UDMA_SRC_INC_32, or UDMA_SRC_INC_NONE.

The srcAddr parameter is a void pointer to the beginning of the source data.

The dstIncrement parameter is the increment size for the destination data. It must be one of UDMA_DST_INC_8, UDMA_DST_INC_16, UDMA_DST_INC_32, or UDMA_DST_INC_NONE.

The dstAddr parameter is a void pointer to the beginning of the location where the data will be transferred.

The arbSize parameter is the arbitration size for the transfer, and must be one of UDMA_ARB_1, UDMA_ARB_2, UDMA_ARB_4, and so on up to UDMA_ARB_1024. This is used to select the arbitration size in powers of 2, from 1 to 1024.

The mode parameter is the mode to use for this transfer task. It must be one of UDMA_MODE_BASIC, UDMA_MODE_AUTO, UDMA_MODE_MEM_SCATTER_GATHER, or UDMA_MODE_PER_SCATTER_GATHER. Note that normally all tasks will be one of the scatter-gather modes while the last task is a task list will be AUTO or BASIC.

This macro is intended to be used to initialize individual entries of a structure of DMA_ControlTable type, like this:

DMA_ControlTable MyTaskList[] =
{
UDMA_SRC_INC_8, MySourceBuf,
UDMA_DST_INC_8, MyDestBuf,
DMA_TaskStructEntry(Task2Count, ... ),
}
Parameters
transferCountis the count of items to transfer for this task.
itemSizeis the bit size of the items to transfer for this task.
srcIncrementis the bit size increment for source data.
srcAddris the starting address of the data to transfer.
dstIncrementis the bit size increment for destination data.
dstAddris the starting address of the destination data.
arbSizeis the arbitration size to use for the transfer task.
modeis the transfer mode for this task.
Returns
Nothing; this is not a function.
#define UDMA_ATTR_USEBURST   0x00000001
#define UDMA_ATTR_ALTSELECT   0x00000002
#define UDMA_ATTR_HIGH_PRIORITY   0x00000004
#define UDMA_ATTR_REQMASK   0x00000008
#define UDMA_ATTR_ALL   0x0000000F
#define UDMA_MODE_STOP   0x00000000
#define UDMA_MODE_BASIC   0x00000001
#define UDMA_MODE_AUTO   0x00000002
#define UDMA_MODE_PINGPONG   0x00000003
#define UDMA_MODE_MEM_SCATTER_GATHER   0x00000004
#define UDMA_MODE_PER_SCATTER_GATHER   0x00000006
#define UDMA_MODE_ALT_SELECT   0x00000001
#define UDMA_DST_INC_8   0x00000000
#define UDMA_DST_INC_16   0x40000000
#define UDMA_DST_INC_32   0x80000000
#define UDMA_DST_INC_NONE   0xc0000000

Referenced by DMA_setChannelTransfer().

#define UDMA_SRC_INC_8   0x00000000
#define UDMA_SRC_INC_16   0x04000000
#define UDMA_SRC_INC_32   0x08000000
#define UDMA_SRC_INC_NONE   0x0c000000

Referenced by DMA_setChannelTransfer().

#define UDMA_SIZE_8   0x00000000
#define UDMA_SIZE_16   0x11000000
#define UDMA_SIZE_32   0x22000000
#define UDMA_DST_PROT_PRIV   0x00200000
#define UDMA_SRC_PROT_PRIV   0x00040000
#define UDMA_ARB_1   0x00000000
#define UDMA_ARB_2   0x00004000
#define UDMA_ARB_4   0x00008000
#define UDMA_ARB_8   0x0000c000
#define UDMA_ARB_16   0x00010000
#define UDMA_ARB_32   0x00014000
#define UDMA_ARB_64   0x00018000
#define UDMA_ARB_128   0x0001c000
#define UDMA_ARB_256   0x00020000
#define UDMA_ARB_512   0x00024000
#define UDMA_ARB_1024   0x00028000
#define UDMA_NEXT_USEBURST   0x00000008
#define UDMA_PRI_SELECT   0x00000000
#define UDMA_ALT_SELECT   0x00000008
#define DMA_CH0_RESERVED0   0x00000000

Referenced by DMA_assignChannel().

#define DMA_CH0_EUSCIA0TX   0x01000000

Referenced by DMA_assignChannel().

#define DMA_CH0_EUSCIB0TX0   0x02000000

Referenced by DMA_assignChannel().

#define DMA_CH0_EUSCIB3TX1   0x03000000

Referenced by DMA_assignChannel().

#define DMA_CH0_EUSCIB2TX2   0x04000000

Referenced by DMA_assignChannel().

#define DMA_CH0_EUSCIB1TX3   0x05000000

Referenced by DMA_assignChannel().

#define DMA_CH0_TIMERA0CCR0   0x06000000

Referenced by DMA_assignChannel().

#define DMA_CH0_AESTRIGGER0   0x07000000

Referenced by DMA_assignChannel().

#define DMA_CH1_RESERVED0   0x00000001

Referenced by DMA_assignChannel().

#define DMA_CH1_EUSCIA0RX   0x01000001

Referenced by DMA_assignChannel().

#define DMA_CH1_EUSCIB0RX0   0x02000001

Referenced by DMA_assignChannel().

#define DMA_CH1_EUSCIB3RX1   0x03000001

Referenced by DMA_assignChannel().

#define DMA_CH1_EUSCIB2RX2   0x04000001

Referenced by DMA_assignChannel().

#define DMA_CH1_EUSCIB1RX3   0x05000001

Referenced by DMA_assignChannel().

#define DMA_CH1_TIMERA0CCR2   0x06000001

Referenced by DMA_assignChannel().

#define DMA_CH1_AESTRIGGER1   0x07000001

Referenced by DMA_assignChannel().

#define DMA_CH2_RESERVED0   0x00000002

Referenced by DMA_assignChannel().

#define DMA_CH2_EUSCIA1TX   0x01000002

Referenced by DMA_assignChannel().

#define DMA_CH2_EUSCIB1TX0   0x02000002

Referenced by DMA_assignChannel().

#define DMA_CH2_EUSCIB0TX1   0x03000002

Referenced by DMA_assignChannel().

#define DMA_CH2_EUSCIB3TX2   0x04000002

Referenced by DMA_assignChannel().

#define DMA_CH2_EUSCIB2TX3   0x05000002

Referenced by DMA_assignChannel().

#define DMA_CH2_TIMERA1CCR0   0x06000002

Referenced by DMA_assignChannel().

#define DMA_CH2_AESTRIGGER2   0x07000002

Referenced by DMA_assignChannel().

#define DMA_CH3_RESERVED0   0x00000003

Referenced by DMA_assignChannel().

#define DMA_CH3_EUSCIA1RX   0x01000003

Referenced by DMA_assignChannel().

#define DMA_CH3_EUSCIB1RX0   0x02000003

Referenced by DMA_assignChannel().

#define DMA_CH3_EUSCIB0RX1   0x03000003

Referenced by DMA_assignChannel().

#define DMA_CH3_EUSCIB3RX2   0x04000003

Referenced by DMA_assignChannel().

#define DMA_CH3_EUSCIB2RX3   0x05000003

Referenced by DMA_assignChannel().

#define DMA_CH3_TIMERA1CCR2   0x06000003

Referenced by DMA_assignChannel().

#define DMA_CH3_RESERVED1   0x07000003

Referenced by DMA_assignChannel().

#define DMA_CH4_RESERVED0   0x00000004

Referenced by DMA_assignChannel().

#define DMA_CH4_EUSCIA2TX   0x01000004

Referenced by DMA_assignChannel().

#define DMA_CH4_EUSCIB2TX0   0x02000004

Referenced by DMA_assignChannel().

#define DMA_CH4_EUSCIB1TX1   0x03000004

Referenced by DMA_assignChannel().

#define DMA_CH4_EUSCIB0TX2   0x04000004

Referenced by DMA_assignChannel().

#define DMA_CH4_EUSCIB3TX3   0x05000004

Referenced by DMA_assignChannel().

#define DMA_CH4_TIMERA2CCR0   0x06000004

Referenced by DMA_assignChannel().

#define DMA_CH4_RESERVED1   0x07000004

Referenced by DMA_assignChannel().

#define DMA_CH5_RESERVED0   0x00000005

Referenced by DMA_assignChannel().

#define DMA_CH5_EUSCIA2RX   0x01000005

Referenced by DMA_assignChannel().

#define DMA_CH5_EUSCIB2RX0   0x02000005

Referenced by DMA_assignChannel().

#define DMA_CH5_EUSCIB1RX1   0x03000005

Referenced by DMA_assignChannel().

#define DMA_CH5_EUSCIB0RX2   0x04000005

Referenced by DMA_assignChannel().

#define DMA_CH5_EUSCIB3RX3   0x05000005

Referenced by DMA_assignChannel().

#define DMA_CH5_TIMERA2CCR2   0x06000005

Referenced by DMA_assignChannel().

#define DMA_CH5_RESERVED1   0x07000005

Referenced by DMA_assignChannel().

#define DMA_CH6_RESERVED0   0x00000006

Referenced by DMA_assignChannel().

#define DMA_CH6_EUSCIA3TX   0x01000006

Referenced by DMA_assignChannel().

#define DMA_CH6_EUSCIB3TX0   0x02000006

Referenced by DMA_assignChannel().

#define DMA_CH6_EUSCIB2TX1   0x03000006

Referenced by DMA_assignChannel().

#define DMA_CH6_EUSCIB1TX2   0x04000006

Referenced by DMA_assignChannel().

#define DMA_CH6_EUSCIB0TX3   0x05000006

Referenced by DMA_assignChannel().

#define DMA_CH6_TIMERA3CCR0   0x06000006

Referenced by DMA_assignChannel().

#define DMA_CH6_EXTERNALPIN   0x07000006

Referenced by DMA_assignChannel().

#define DMA_CH7_RESERVED0   0x00000007

Referenced by DMA_assignChannel().

#define DMA_CH7_EUSCIA3RX   0x01000007

Referenced by DMA_assignChannel().

#define DMA_CH7_EUSCIB3RX0   0x02000007

Referenced by DMA_assignChannel().

#define DMA_CH7_EUSCIB2RX1   0x03000007

Referenced by DMA_assignChannel().

#define DMA_CH7_EUSCIB1RX2   0x04000007

Referenced by DMA_assignChannel().

#define DMA_CH7_EUSCIB0RX3   0x05000007

Referenced by DMA_assignChannel().

#define DMA_CH7_TIMERA3CCR2   0x06000007

Referenced by DMA_assignChannel().

#define DMA_CH7_ADC14   0x07000007

Referenced by DMA_assignChannel().

#define DMA_INT0   INT_DMA_INT0
#define DMA_INT1   INT_DMA_INT1
#define DMA_INT2   INT_DMA_INT2
#define DMA_INT3   INT_DMA_INT3
#define DMA_INTERR   INT_DMA_ERR
#define DMA_CHANNEL_0   0
#define DMA_CHANNEL_1   1
#define DMA_CHANNEL_2   2
#define DMA_CHANNEL_3   3
#define DMA_CHANNEL_4   4
#define DMA_CHANNEL_5   5
#define DMA_CHANNEL_6   6
#define DMA_CHANNEL_7   7

Typedef Documentation

Function Documentation

void DMA_enableModule ( void  )

Enables the DMA controller for use.

This function enables the DMA controller. The DMA controller must be enabled before it can be configured and used.

Returns
None.
void DMA_disableModule ( void  )

Disables the DMA controller for use.

This function disables the DMA controller. Once disabled, the DMA controller cannot operate until re-enabled with DMA_enableModule().

Returns
None.
uint32_t DMA_getErrorStatus ( void  )

Gets the DMA error status.

This function returns the DMA error status. It should be called from within the DMA error interrupt handler to determine if a DMA error occurred.

Returns
Returns non-zero if a DMA error is pending.
void DMA_clearErrorStatus ( void  )

Clears the DMA error interrupt.

This function clears a pending DMA error interrupt. This function should be called from within the DMA error interrupt handler to clear the interrupt.

Returns
None.
void DMA_enableChannel ( uint32_t  channelNum)

Enables a DMA channel for operation.

Parameters
channelNumis the channel number to enable.

When a DMA transfer is completed, the channel is automatically disabled by the DMA controller. Therefore, this function should be called prior to starting up any new transfer.

Returns
None.

References ASSERT.

void DMA_disableChannel ( uint32_t  channelNum)

Disables a DMA channel for operation.

Parameters
channelNumis the channel number to disable.

This function disables a specific DMA channel. Once disabled, a channel cannot respond to DMA transfer requests until re-enabled via DMA_enableChannel().

Returns
None.

References ASSERT.

bool DMA_isChannelEnabled ( uint32_t  channelNum)

Checks if a DMA channel is enabled for operation.

Parameters
channelNumis the channel number to check.

This function checks to see if a specific DMA channel is enabled. This function can be used to check the status of a transfer, as the channel is automatically disabled at the end of a transfer.

Returns
Returns true if the channel is enabled, false if disabled.

References ASSERT.

void DMA_setControlBase ( void *  controlTable)

Sets the base address for the channel control table.

Parameters
controlTableis a pointer to the 1024-byte-aligned base address of the DMA channel control table.

This function configures the base address of the channel control table. This table resides in system memory and holds control information for each DMA channel. The table must be aligned on a 1024-byte boundary. The base address must be configured before any of the channel functions can be used.

The size of the channel control table depends on the number of DMA channels and the transfer modes that are used. Refer to the introductory text and the microcontroller datasheet for more information about the channel control table.

Returns
None.

References ASSERT.

void* DMA_getControlBase ( void  )

Gets the base address for the channel control table.

This function gets the base address of the channel control table. This table resides in system memory and holds control information for each DMA channel.

Returns
Returns a pointer to the base address of the channel control table.
void* DMA_getControlAlternateBase ( void  )

Gets the base address for the channel control table alternate structures.

This function gets the base address of the second half of the channel control table that holds the alternate control structures for each channel.

Returns
Returns a pointer to the base address of the second half of the channel control table.
void DMA_requestChannel ( uint32_t  channelNum)

Requests a DMA channel to start a transfer.

Parameters
channelNumis the channel number on which to request a DMA transfer.

This function allows software to request a DMA channel to begin a transfer. This function could be used for performing a memory-to-memory transfer, or if for some reason a transfer needs to be initiated by software instead of the peripheral associated with that channel.

Returns
None.

References ASSERT.

void DMA_enableChannelAttribute ( uint32_t  channelNum,
uint32_t  attr 
)

Enables attributes of a DMA channel.

Parameters
channelNumis the channel to configure.
attris a combination of attributes for the channel.

This function is used to enable attributes of a DMA channel.

The attr parameter is the logical OR of any of the following:

  • UDMA_ATTR_USEBURST is used to restrict transfers to use only burst mode.
  • UDMA_ATTR_ALTSELECT is used to select the alternate control structure for this channel (it is very unlikely that this flag should be used).
  • UDMA_ATTR_HIGH_PRIORITY is used to set this channel to high priority.
  • UDMA_ATTR_REQMASK is used to mask the hardware request signal from the peripheral for this channel.
Returns
None.

References ASSERT, UDMA_ATTR_ALTSELECT, UDMA_ATTR_HIGH_PRIORITY, UDMA_ATTR_REQMASK, and UDMA_ATTR_USEBURST.

void DMA_disableChannelAttribute ( uint32_t  channelNum,
uint32_t  attr 
)

Disables attributes of a DMA channel.

Parameters
channelNumis the channel to configure.
attris a combination of attributes for the channel.

This function is used to disable attributes of a DMA channel.

The attr parameter is the logical OR of any of the following:

  • UDMA_ATTR_USEBURST is used to restrict transfers to use only burst mode.
  • UDMA_ATTR_ALTSELECT is used to select the alternate control structure for this channel.
  • UDMA_ATTR_HIGH_PRIORITY is used to set this channel to high priority.
  • UDMA_ATTR_REQMASK is used to mask the hardware request signal from the peripheral for this channel.
Returns
None.

References ASSERT, UDMA_ATTR_ALTSELECT, UDMA_ATTR_HIGH_PRIORITY, UDMA_ATTR_REQMASK, and UDMA_ATTR_USEBURST.

uint32_t DMA_getChannelAttribute ( uint32_t  channelNum)

Gets the enabled attributes of a DMA channel.

Parameters
channelNumis the channel to configure.

This function returns a combination of flags representing the attributes of the DMA channel.

Returns
Returns the logical OR of the attributes of the DMA channel, which can be any of the following:
  • UDMA_ATTR_USEBURST is used to restrict transfers to use only burst mode.
  • UDMA_ATTR_ALTSELECT is used to select the alternate control structure for this channel.
  • UDMA_ATTR_HIGH_PRIORITY is used to set this channel to high priority.
  • UDMA_ATTR_REQMASK is used to mask the hardware request signal from the peripheral for this channel.

References ASSERT, UDMA_ATTR_ALTSELECT, UDMA_ATTR_HIGH_PRIORITY, UDMA_ATTR_REQMASK, and UDMA_ATTR_USEBURST.

void DMA_setChannelControl ( uint32_t  channelStructIndex,
uint32_t  control 
)

Sets the control parameters for a DMA channel control structure.

Parameters
channelStructIndexis the logical OR of the DMA channel number with UDMA_PRI_SELECT or UDMA_ALT_SELECT.
controlis logical OR of several control values to set the control parameters for the channel.

This function is used to set control parameters for a DMA transfer. These parameters are typically not changed often.

The channelStructIndex parameter should be the logical OR of the channel number with one of UDMA_PRI_SELECT or UDMA_ALT_SELECT to choose whether the primary or alternate data structure is used.

The control parameter is the logical OR of five values: the data size, the source address increment, the destination address increment, the arbitration size, and the use burst flag. The choices available for each of these values is described below.

Choose the data size from one of UDMA_SIZE_8, UDMA_SIZE_16, or UDMA_SIZE_32 to select a data size of 8, 16, or 32 bits.

Choose the source address increment from one of UDMA_SRC_INC_8, UDMA_SRC_INC_16, UDMA_SRC_INC_32, or UDMA_SRC_INC_NONE to select an address increment of 8-bit bytes, 16-bit half-words, 32-bit words, or to select non-incrementing.

Choose the destination address increment from one of UDMA_DST_INC_8, UDMA_DST_INC_16, UDMA_DST_INC_32, or UDMA_SRC_INC_8 to select an address increment of 8-bit bytes, 16-bit half-words, 32-bit words, or to select non-incrementing.

The arbitration size determines how many items are transferred before the DMA controller re-arbitrates for the bus. Choose the arbitration size from one of UDMA_ARB_1, UDMA_ARB_2, UDMA_ARB_4, UDMA_ARB_8, through UDMA_ARB_1024 to select the arbitration size from 1 to 1024 items, in powers of 2.

The value UDMA_NEXT_USEBURST is used to force the channel to only respond to burst requests at the tail end of a scatter-gather transfer.

Note
The address increment cannot be smaller than the data size.
Returns
None.

References ASSERT, and _DMA_ControlTable::control.

void DMA_setChannelTransfer ( uint32_t  channelStructIndex,
uint32_t  mode,
void *  srcAddr,
void *  dstAddr,
uint32_t  transferSize 
)

Sets the transfer parameters for a DMA channel control structure.

Parameters
channelStructIndexis the logical OR of the DMA channel number with either UDMA_PRI_SELECT or UDMA_ALT_SELECT.
modeis the type of DMA transfer.
srcAddris the source address for the transfer.
dstAddris the destination address for the transfer.
transferSizeis the number of data items to transfer.

This function is used to configure the parameters for a DMA transfer. These parameters are typically changed often. The function DMA_setChannelControl() MUST be called at least once for this channel prior to calling this function.

The channelStructIndex parameter should be the logical OR of the channel number with one of UDMA_PRI_SELECT or UDMA_ALT_SELECT to choose whether the primary or alternate data structure is used.

The mode parameter should be one of the following values:

  • UDMA_MODE_STOP stops the DMA transfer. The controller sets the mode to this value at the end of a transfer.
  • UDMA_MODE_BASIC to perform a basic transfer based on request.
  • UDMA_MODE_AUTO to perform a transfer that always completes once started even if the request is removed.
  • UDMA_MODE_PINGPONG to set up a transfer that switches between the primary and alternate control structures for the channel. This mode allows use of ping-pong buffering for DMA transfers.
  • UDMA_MODE_MEM_SCATTER_GATHER to set up a memory scatter-gather transfer.
  • UDMA_MODE_PER_SCATTER_GATHER to set up a peripheral scatter-gather transfer.

The srcAddr and dstAddr parameters are pointers to the first location of the data to be transferred. These addresses should be aligned according to the item size. The compiler takes care of this alignment if the pointers are pointing to storage of the appropriate data type.

The transferSize parameter is the number of data items, not the number of bytes.

The two scatter-gather modes, memory and peripheral, are actually different depending on whether the primary or alternate control structure is selected. This function looks for the UDMA_PRI_SELECT and UDMA_ALT_SELECT flag along with the channel number and sets the scatter-gather mode as appropriate for the primary or alternate control structure.

The channel must also be enabled using DMA_enableChannel() after calling this function. The transfer does not begin until the channel has been configured and enabled. Note that the channel is automatically disabled after the transfer is completed, meaning that DMA_enableChannel() must be called again after setting up the next transfer.

Note
Great care must be taken to not modify a channel control structure that is in use or else the results are unpredictable, including the possibility of undesired data transfers to or from memory or peripherals. For BASIC and AUTO modes, it is safe to make changes when the channel is disabled, or the DMA_getChannelMode() returns UDMA_MODE_STOP. For PINGPONG or one of the SCATTER_GATHER modes, it is safe to modify the primary or alternate control structure only when the other is being used. The DMA_getChannelMode() function returns UDMA_MODE_STOP when a channel control structure is inactive and safe to modify.
Returns
None.

References ASSERT, _DMA_ControlTable::control, _DMA_ControlTable::dstEndAddr, _DMA_ControlTable::srcEndAddr, UDMA_ALT_SELECT, UDMA_DST_INC_NONE, UDMA_MODE_ALT_SELECT, UDMA_MODE_MEM_SCATTER_GATHER, UDMA_MODE_PER_SCATTER_GATHER, and UDMA_SRC_INC_NONE.

void DMA_setChannelScatterGather ( uint32_t  channelNum,
uint32_t  taskCount,
void *  taskList,
uint32_t  isPeriphSG 
)

Configures a DMA channel for scatter-gather mode.

Parameters
channelNumis the DMA channel number.
taskCountis the number of scatter-gather tasks to execute.
taskListis a pointer to the beginning of the scatter-gather task list.
isPeriphSGis a flag to indicate it is a peripheral scatter-gather transfer (else it is memory scatter-gather transfer)

This function is used to configure a channel for scatter-gather mode. The caller must have already set up a task list and must pass a pointer to the start of the task list as the taskList parameter. The taskCount parameter is the count of tasks in the task list, not the size of the task list. The flag bIsPeriphSG should be used to indicate if scatter-gather should be configured for peripheral or memory operation.

See Also
DMA_TaskStructEntry
Returns
None.

References ASSERT, _DMA_ControlTable::control, _DMA_ControlTable::dstEndAddr, _DMA_ControlTable::spare, _DMA_ControlTable::srcEndAddr, and UDMA_ALT_SELECT.

uint32_t DMA_getChannelSize ( uint32_t  channelStructIndex)

Gets the current transfer size for a DMA channel control structure.

Parameters
channelStructIndexis the logical OR of the DMA channel number with either UDMA_PRI_SELECT or UDMA_ALT_SELECT.

This function is used to get the DMA transfer size for a channel. The transfer size is the number of items to transfer, where the size of an item might be 8, 16, or 32 bits. If a partial transfer has already occurred, then the number of remaining items is returned. If the transfer is complete, then 0 is returned.

Returns
Returns the number of items remaining to transfer.

References ASSERT, and _DMA_ControlTable::control.

uint32_t DMA_getChannelMode ( uint32_t  channelStructIndex)

Gets the transfer mode for a DMA channel control structure.

Parameters
channelStructIndexis the logical OR of the DMA channel number with either UDMA_PRI_SELECT or UDMA_ALT_SELECT.

This function is used to get the transfer mode for the DMA channel and to query the status of a transfer on a channel. When the transfer is complete the mode is UDMA_MODE_STOP.

Returns
Returns the transfer mode of the specified channel and control structure, which is one of the following values: UDMA_MODE_STOP, UDMA_MODE_BASIC, UDMA_MODE_AUTO, UDMA_MODE_PINGPONG, UDMA_MODE_MEM_SCATTER_GATHER, or UDMA_MODE_PER_SCATTER_GATHER.

References ASSERT, _DMA_ControlTable::control, UDMA_MODE_ALT_SELECT, UDMA_MODE_MEM_SCATTER_GATHER, and UDMA_MODE_PER_SCATTER_GATHER.

void DMA_assignChannel ( uint32_t  mapping)

Assigns a peripheral mapping for a DMA channel.

Parameters
mappingis a macro specifying the peripheral assignment for a channel.

This function assigns a peripheral mapping to a DMA channel. It is used to select which peripheral is used for a DMA channel. The parameter mapping should be one of the macros named UDMA_CHn_tttt from the header file dma.h. For example, to assign DMA channel 0 to the eUSCI AO RX channel, the parameter should be the macro UDMA_CH1_EUSCIA0RX.

Please consult the data sheet for a table showing all the possible peripheral assignments for the DMA channels for a particular device.

Returns
None.

References ASSERT, DMA_CH0_AESTRIGGER0, DMA_CH0_EUSCIA0TX, DMA_CH0_EUSCIB0TX0, DMA_CH0_EUSCIB1TX3, DMA_CH0_EUSCIB2TX2, DMA_CH0_EUSCIB3TX1, DMA_CH0_RESERVED0, DMA_CH0_TIMERA0CCR0, DMA_CH1_AESTRIGGER1, DMA_CH1_EUSCIA0RX, DMA_CH1_EUSCIB0RX0, DMA_CH1_EUSCIB1RX3, DMA_CH1_EUSCIB2RX2, DMA_CH1_EUSCIB3RX1, DMA_CH1_RESERVED0, DMA_CH1_TIMERA0CCR2, DMA_CH2_AESTRIGGER2, DMA_CH2_EUSCIA1TX, DMA_CH2_EUSCIB0TX1, DMA_CH2_EUSCIB1TX0, DMA_CH2_EUSCIB2TX3, DMA_CH2_EUSCIB3TX2, DMA_CH2_RESERVED0, DMA_CH2_TIMERA1CCR0, DMA_CH3_EUSCIA1RX, DMA_CH3_EUSCIB0RX1, DMA_CH3_EUSCIB1RX0, DMA_CH3_EUSCIB2RX3, DMA_CH3_EUSCIB3RX2, DMA_CH3_RESERVED0, DMA_CH3_RESERVED1, DMA_CH3_TIMERA1CCR2, DMA_CH4_EUSCIA2TX, DMA_CH4_EUSCIB0TX2, DMA_CH4_EUSCIB1TX1, DMA_CH4_EUSCIB2TX0, DMA_CH4_EUSCIB3TX3, DMA_CH4_RESERVED0, DMA_CH4_RESERVED1, DMA_CH4_TIMERA2CCR0, DMA_CH5_EUSCIA2RX, DMA_CH5_EUSCIB0RX2, DMA_CH5_EUSCIB1RX1, DMA_CH5_EUSCIB2RX0, DMA_CH5_EUSCIB3RX3, DMA_CH5_RESERVED0, DMA_CH5_RESERVED1, DMA_CH5_TIMERA2CCR2, DMA_CH6_EUSCIA3TX, DMA_CH6_EUSCIB0TX3, DMA_CH6_EUSCIB1TX2, DMA_CH6_EUSCIB2TX1, DMA_CH6_EUSCIB3TX0, DMA_CH6_EXTERNALPIN, DMA_CH6_RESERVED0, DMA_CH6_TIMERA3CCR0, DMA_CH7_ADC14, DMA_CH7_EUSCIA3RX, DMA_CH7_EUSCIB0RX3, DMA_CH7_EUSCIB1RX2, DMA_CH7_EUSCIB2RX1, DMA_CH7_EUSCIB3RX0, DMA_CH7_RESERVED0, and DMA_CH7_TIMERA3CCR2.

void DMA_requestSoftwareTransfer ( uint32_t  channel)

Initializes a software transfer of the corresponding DMA channel. This is done if the user wants to force a DMA on the specified channel without the hardware precondition. Specific channels can be configured using the DMA_assignChannel function.

Parameters
channelis the channel to trigger the interrupt
Returns
None
void DMA_assignInterrupt ( uint32_t  interruptNumber,
uint32_t  channel 
)

Assigns a specific DMA channel to the corresponding interrupt handler. For MSP432 devices, there are three configurable interrupts, and one master interrupt. This function will assign a specific DMA channel to the provided configurable DMA interrupt.

Note that once a channel is assigned to a configurable interrupt, it will be masked in hardware from the master DMA interrupt (interruptNumber zero). This function can also be used in conjunction with the DMAIntTrigger function to provide the feature to software trigger specific channel interrupts.

Parameters
interruptNumberis the configurable interrupt to assign the given channel. Valid values are:
  • DMA_INT1 the first configurable DMA interrupt handler
  • DMA_INT2 the second configurable DMA interrupt handler
  • DMA_INT3 the third configurable DMA interrupt handler
channelis the channel to assign the interrupt
Returns
None.

References ASSERT, DMA_enableInterrupt(), DMA_INT1, DMA_INT2, and DMA_INT3.

void DMA_enableInterrupt ( uint32_t  interruptNumber)

Enables the specified interrupt for the DMA controller. Note for interrupts one through three, specific channels have to be mapped to the interrupt using the DMA_assignInterrupt function.

Parameters
interruptNumberidentifies which DMA interrupt is to be enabled. This interrupt should be one of the following:
  • DMA_INT1 the first configurable DMA interrupt handler
  • DMA_INT2 the second configurable DMA interrupt handler
  • DMA_INT3 the third configurable DMA interrupt handler
Returns
None.

References ASSERT, DMA_INT1, DMA_INT2, and DMA_INT3.

Referenced by DMA_assignInterrupt().

void DMA_disableInterrupt ( uint32_t  interruptNumber)

Disables the specified interrupt for the DMA controller.

Parameters
interruptNumberidentifies which DMA interrupt is to be disabled. This interrupt should be one of the following:
  • DMA_INT1 the first configurable DMA interrupt handler
  • DMA_INT2 the second configurable DMA interrupt handler
  • DMA_INT3 the third configurable DMA interrupt handler

    Note for interrupts that are associated with a specific DMA channel (DMA_INT1 - DMA_INT3), this function will also enable that specific channel for interrupts.

Returns
None.

References ASSERT, DMA_INT1, DMA_INT2, and DMA_INT3.

uint32_t DMA_getInterruptStatus ( void  )

Gets the DMA controller channel interrupt status for interrupt zero.

This function is used to get the interrupt status of the DMA controller. The returned value is a 32-bit bit mask that indicates which channels are requesting an interrupt. This function can be used from within an interrupt handler to determine or confirm which DMA channel has requested an interrupt.

Note that this will only apply to interrupt zero for the DMA controller as only one interrupt can be associated with interrupts one through three. If an interrupt is assigned to an interrupt other than interrupt zero, it will be masked by this function.

Returns
Returns a 32-bit mask which indicates requesting DMA channels. There is a bit for each channel and a 1 indicates that the channel is requesting an interrupt. Multiple bits can be set.
void DMA_clearInterruptFlag ( uint32_t  channel)

Clears the DMA controller channel interrupt mask for interrupt zero.

Parameters
channelis the channel interrupt to clear.

This function is used to clear the interrupt status of the DMA controller. Note that only interrupts that weren't assigned to DMA interrupts one through three using the DMA_assignInterrupt function will be affected by this function. For other DMA interrupts, only one channel can be associated and therefore clearing is unnecessary.

Returns
None
void DMA_registerInterrupt ( uint32_t  interruptNumber,
void(*)(void)  intHandler 
)

Registers an interrupt handler for the DMA controller.

Parameters
interruptNumberidentifies which DMA interrupt is to be registered.
intHandleris a pointer to the function to be called when the interrupt is called.

This function registers and enables the handler to be called when the DMA controller generates an interrupt. The interrupt parameter should be one of the following:

  • DMA_INT0 the master DMA interrupt handler
  • DMA_INT1 the first configurable DMA interrupt handler
  • DMA_INT2 the second configurable DMA interrupt handler
  • DMA_INT3 the third configurable DMA interrupt handler
  • DMA_INTERR the DMA error interrupt handler
See Also
Interrupt_registerInterrupt() for important information about registering interrupt handlers.
Returns
None.

References ASSERT, DMA_INT0, DMA_INT1, DMA_INT2, DMA_INT3, DMA_INTERR, Interrupt_enableInterrupt(), and Interrupt_registerInterrupt().

void DMA_unregisterInterrupt ( uint32_t  interruptNumber)

Unregisters an interrupt handler for the DMA controller.

Parameters
interruptNumberidentifies which DMA interrupt to unregister.

This function disables and unregisters the handler to be called for the specified DMA interrupt. The interrupt parameter should be one of the parameters as documented for the function DMA_registerInterrupt().

Note for interrupts that are associated with a specific DMA channel (DMA_INT1 - DMA_INT3), this function will also disable that specific channel for interrupts.

See Also
Interrupt_registerInterrupt() for important information about registering interrupt handlers.
Returns
None.

References ASSERT, DMA_INT0, DMA_INT1, DMA_INT2, DMA_INT3, DMA_INTERR, Interrupt_disableInterrupt(), and Interrupt_unregisterInterrupt().


Copyright 2017, Texas Instruments Incorporated