![]() |
![]() |
Macros | |
#define | AESCCM_STATUS_SUCCESS (0) |
Successful status code. More... | |
#define | AESCCM_STATUS_ERROR (-1) |
Generic error status code. More... | |
#define | AESCCM_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by AESCCM_control() for undefined command codes. More... | |
#define | AESCCM_STATUS_RESOURCE_UNAVAILABLE (-3) |
An error status code returned if the hardware or software resource is currently unavailable. More... | |
#define | AESCCM_STATUS_MAC_INVALID (-4) |
An error status code returned if the MAC provided by the application for a decryption operation does not match the one calculated during the operation. More... | |
AESCCM_STATUS_* macros are general status codes returned by AESCCM functions
#define AESCCM_STATUS_SUCCESS (0) |
Successful status code.
Function return AESCCM_STATUS_SUCCESS if the control code was executed successfully.
#define AESCCM_STATUS_ERROR (-1) |
Generic error status code.
Functions return AESCCM_STATUS_ERROR if the control code was not executed successfully.
#define AESCCM_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by AESCCM_control() for undefined command codes.
AESCCM_control() returns AESCCM_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.
#define AESCCM_STATUS_RESOURCE_UNAVAILABLE (-3) |
An error status code returned if the hardware or software resource is currently unavailable.
AESCCM driver implementations may have hardware or software limitations on how many clients can simultaneously perform operations. This status code is returned if the mutual exclusion mechanism signals that an operation cannot currently be performed.
#define AESCCM_STATUS_MAC_INVALID (-4) |
An error status code returned if the MAC provided by the application for a decryption operation does not match the one calculated during the operation.
This code is returned by AESCCM_oneStepDecrypt() and AESCCM_verifyMAC() if the verification of the MAC fails.