Modules | |
Status Codes | |
Command Codes | |
Macros | |
#define | I2C_CMD_RESERVED (32) |
#define | I2C_STATUS_RESERVED (-32) |
These I2C macros are reservations for I2C.h
#define I2C_CMD_RESERVED (32) |
Common I2C_control command code reservation offset. I2C driver implementations should offset command codes with I2C_CMD_RESERVED growing positively
Example implementation specific command codes:
#define I2C_STATUS_RESERVED (-32) |
Common I2C_control status code reservation offset. I2C driver implementations should offset status codes with I2C_STATUS_RESERVED growing negatively.
Example implementation specific status codes: