![]() |
![]() |
TimerMSP432 Object Driver specific structure that takes care of various driver parameters such as hardware interrupts and callbacks. The application should not modify any members of this structure. More...
#include <TimerMSP432.h>
Data Fields | |
bool | resourceAvailable |
Timer_Config * | config |
HwiP_Params | hwiParams |
HwiP_Handle | hwiHandle |
Timer_CallBackFxn | callBack |
SemaphoreP_Handle | timerSem |
Timer_Mode | timerMode |
bool | isRunning |
uint32_t | timerPeriod |
TimerMSP432 Object Driver specific structure that takes care of various driver parameters such as hardware interrupts and callbacks. The application should not modify any members of this structure.
bool TimerMSP432_Object::resourceAvailable |
Timer_Config* TimerMSP432_Object::config |
HwiP_Params TimerMSP432_Object::hwiParams |
HwiP_Handle TimerMSP432_Object::hwiHandle |
Timer_CallBackFxn TimerMSP432_Object::callBack |
SemaphoreP_Handle TimerMSP432_Object::timerSem |
Timer_Mode TimerMSP432_Object::timerMode |
bool TimerMSP432_Object::isRunning |
uint32_t TimerMSP432_Object::timerPeriod |