![]() |
![]() |
SPIMSP432DMA Hardware attributes These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP432 driverlib these definitions are found in: More...
#include <SPIMSP432DMA.h>
Data Fields | |
uint32_t | baseAddr |
uint16_t | bitOrder |
uint8_t | clockSource |
uint8_t | defaultTxBufValue |
uint8_t | dmaIntNum |
uint32_t | intPriority |
uint32_t | rxDMAChannelIndex |
uint32_t | txDMAChannelIndex |
uint16_t | simoPin |
uint16_t | somiPin |
uint16_t | clkPin |
uint16_t | stePin |
uint16_t | pinMode |
SPIMSP432DMA Hardware attributes These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP432 driverlib these definitions are found in:
intPriority is the SPI peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.dpl interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().
A sample structure is shown below:
uint32_t SPIMSP432DMA_HWAttrsV1::baseAddr |
EUSCI_B_SPI Peripheral's base address
uint16_t SPIMSP432DMA_HWAttrsV1::bitOrder |
EUSCI_B_SPI Bit order
uint8_t SPIMSP432DMA_HWAttrsV1::clockSource |
EUSCI_B_SPI Clock source
uint8_t SPIMSP432DMA_HWAttrsV1::defaultTxBufValue |
uint8_t SPIMSP432DMA_HWAttrsV1::dmaIntNum |
Default TX value if txBuf == NULL DMA interrupt number
uint32_t SPIMSP432DMA_HWAttrsV1::intPriority |
DMA interrupt priority
uint32_t SPIMSP432DMA_HWAttrsV1::rxDMAChannelIndex |
DMA rxDMAChannel for Rx data
uint32_t SPIMSP432DMA_HWAttrsV1::txDMAChannelIndex |
DMA txDMAChannel for Tx data
uint16_t SPIMSP432DMA_HWAttrsV1::simoPin |
Port/pin for SIMO (MOSI)
uint16_t SPIMSP432DMA_HWAttrsV1::somiPin |
Port/pin for SOMI (MISO)
uint16_t SPIMSP432DMA_HWAttrsV1::clkPin |
Port/pin for SPI CLK
uint16_t SPIMSP432DMA_HWAttrsV1::stePin |
Port/pin for STE
uint16_t SPIMSP432DMA_HWAttrsV1::pinMode |
3-pin or 4-pin mode