#include <SDSPIMSP432.h>
§ baseAddr
uint32_t SDSPIMSP432_HWAttrsV1::baseAddr |
SPI Peripheral's base address
§ clockSource
uint8_t SDSPIMSP432_HWAttrsV1::clockSource |
§ sckPin
uint16_t SDSPIMSP432_HWAttrsV1::sckPin |
Pin configuration for SPI SCK
§ somiPin
uint16_t SDSPIMSP432_HWAttrsV1::somiPin |
Pin configuration for the MISO pin
§ simoPin
uint16_t SDSPIMSP432_HWAttrsV1::simoPin |
Pin configuration for the MOSI pin
§ csPin
uint16_t SDSPIMSP432_HWAttrsV1::csPin |
Pin configuration for chip select
The documentation for this struct was generated from the following file: