Data Fields
ADCBufMSP432_ParamsExtension Struct Reference

MSP432 specfic extension to ADCBuf_Params. More...

#include <ADCBufMSP432.h>

Data Fields

ADCBufMSP432_Sampling_Duration samplingDuration
 

Detailed Description

MSP432 specfic extension to ADCBuf_Params.

To use non-default MSP432 specific parameters when calling ADCBuf_open(), a pointer to an instance of this struct must be specified in ADCBuf_Params::custom. Alternatively, these values can be set using the control function after calling ADCBuf_open().

Field Documentation

§ samplingDuration

ADCBufMSP432_Sampling_Duration ADCBufMSP432_ParamsExtension::samplingDuration

The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated