![]() |
![]() |
Macros | |
#define | CAMERA_STATUS_SUCCESS (0) |
Successful status code returned by Camera_control(). More... | |
#define | CAMERA_STATUS_ERROR (-1) |
Generic error status code returned by Camera_control(). More... | |
#define | CAMERA_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by Camera_control() for undefined command codes. More... | |
Camera_STATUS_* macros are general status codes returned by Camera_control()
#define CAMERA_STATUS_SUCCESS (0) |
Successful status code returned by Camera_control().
Camera_control() returns CAMERA_STATUS_SUCCESS if the control code was executed successfully.
#define CAMERA_STATUS_ERROR (-1) |
Generic error status code returned by Camera_control().
Camera_control() returns CAMERA_STATUS_ERROR if the control code was not executed successfully.
#define CAMERA_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by Camera_control() for undefined command codes.
Camera_control() returns CAMERA_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.